Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Testcard generator revisted
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 1 Mar 2025 5:58 PM Date Created
  • Views 1350 views
  • Likes 7 likes
  • Comments 3 comments
  • hdmi
  • test tool
  • raspberry pi
Related
Recommended

Testcard generator revisted

Workshopshed
Workshopshed
1 Mar 2025

Back in 2016 I created a test card generator to help check a small composite monitor that wasn't working.

For an upcoming project I need to test a HDMI monitor so I thought I could just use that again. But when I came to dig it out the SDCard was nowhere to be found. And checking the links the old software RPi-ATV I'd used was also no longer there.

So I needed to start from scratch. After quickly identifying the PI, I downloaded the PIImager and selected the right image. After a quick head scratch where I realised the wifi dongle I was using was actually a Zigbee dongle, I had it up and running.

Next thing to do was to configure the Pi to boot into console mode which can be done with the raspi-config tool.

And to replace the ATV software I installed a tool called FBI or Framebuffer Imaging. And I created the image for the testcard by downloading the PM5544 card from Wikipedia which was recreated by Zacabeb

By default FBI seems to have a menu so to turn this off you can use -noverbose and the -a option autozooms the image to match the display.

The last step was create a little shell script to run the fbi command in a loop with a little delay. This was needed as I found that if you boot up without the cable plugged in then fbi errors. The was run by adding to the end of the .bashrc file.

A monitor with a testcard on it

Future enhancements

  • Reduce the boot time by using something like DietPi
  • Work out how to switch it between Composite and HDMI without needing to plug in a mouse and keyboard
  • Sign in to reply
Parents
  • DAB
    DAB over 1 year ago

    I like it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 1 year ago

    I like it.