Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs 3D Printing
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 29 Mar 2015 1:08 AM Date Created
  • Views 2323 views
  • Likes 2 likes
  • Comments 8 comments
  • 3d_printing
Related
Recommended

3D Printing

e14 Contributor
e14 Contributor
29 Mar 2015

    You walk up to the washing machine. You turn a knob, and it breaks off. Now you have to call the manufacturers and order an expensive new knob. Or do you?

    Printing started with ink splashing into sections of paper, creating words and things 2D, for you to look at and create plans. As time went on, another dimension was taken over and used to make 3D printed objects. Objects would start to pop out of your printer bed. Suddenly, everything changed. The world was a more automatic. Cases were made. And that time, is now.

    The knob you previously had purchased now can appear on a bed where plastic is extruded. The 3D printing world is actually a lot simpler than most would expect. A circuit board, such as an Arduino, has a connection adapter to connect to various electronics. The circuit board tells the three motors to go to a position. 0,0,0 is commonly known as home. The circuit board is told to go to a position, then another position, one after another, layer by layer. The 3D printer will print a layer, then move up, and then another layer is printed. Continuously this happens, making a final 3D object. The printer will also have to let filament come out and melt, so the extruder was created. The extruder is also a very simple component. The extruder has a motor to push the filament into the hot end, which will heat the filament, and places it on the bed. The filament then dries and gets covered by the next layer of the 3D print.

     Suprisingly, this is all that is to a 3D printer. So now that you know all how a 3D printer works, you can get one for yourself. Now talking about costs, they can vary from as little as $200 (for a kit to make one), up to thousands of dollars, depending on quality and size, choose the printer that is right for you, or maybe even make one.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 11 years ago +1
    The problem is that the replacement knob that a low cost 3D printer can make is no substitute for the real thing - which will have been injection molded in a engineering type plastic to quite high precision…
  • DAB
    DAB over 11 years ago +1
    You could also make a mold out of clay and use a plastic resin to cast a new part. Much less expensive than a 3D printer and once you have a mold, you can make as many as you need. DAB
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    The problem is that the replacement knob that a low cost 3D printer can make is no substitute for the real thing - which will have been injection molded in a engineering type plastic to quite high precision, and then silk screened or otherwise embellished. It will have  smooth or even tactile finish. The very best 3D printers (which don't use extrusion) can come quite close but you still need the design.

    Then there is all the messing about, dealing with chemicals, reels of filament or boxes of dust.

    In just the same way as people don't print newspapers or books I don't expect them to print replacement parts for their washing machines.

    It's just possible that the spare parts suppliers might.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 11 years ago

    The problem is that the replacement knob that a low cost 3D printer can make is no substitute for the real thing - which will have been injection molded in a engineering type plastic to quite high precision, and then silk screened or otherwise embellished. It will have  smooth or even tactile finish. The very best 3D printers (which don't use extrusion) can come quite close but you still need the design.

    Then there is all the messing about, dealing with chemicals, reels of filament or boxes of dust.

    In just the same way as people don't print newspapers or books I don't expect them to print replacement parts for their washing machines.

    It's just possible that the spare parts suppliers might.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • D_Hersey
    D_Hersey over 11 years ago in reply to michaelkellett

    Hi MK, spookily, I find myself in agreement with you.  My washing machine has a touchpad.  My stove has knobs made of phenolic bakelite.  I have a set of spares in my junk drawer that I got in a surplus store for a buck and a quarter, IIRC.  The control shafts are standard.  Thermoset bakelite easily lasts a century.  The supports for the third-rail of el' train track are made of it.  Well, a bakelite, glass-mat composite, anyway.

     

    Generally, my stuff is not breaking all around me.  I generally buy good stuff because the ground it sits upon is more burdensome to acquire and hold than the stuff itself.  I'm not seeing this as a problem.  In some senses I wish I was wrong about this.  There might be more centralization for me it stuff did break.

     

    Anyway, the mechanical properties of a three-dee printed object seem to be inferior to stuff made through traditional methods, usually, and at greater cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    Well, even though that is true, it was just an example. There are actually many other things you can do with a 3D printer. You can print toys, small board games, or even circuit boards. Now filaments have come to the point where some can stretch (like rubber), some can glow in the dark, some are clear, some have wood qualities, and even some are conductive!(for 3D printed circuits)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor

    Please be so kind as to tell us what kind of circuit board you can 3D print - AFAIK it is not possible to achieve typical prototype board design rules (4 layers, 0.15mm track and gap, 0.2mm holes) or even anywhere close.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    Well, the size of the extruded filament is as small as you get, maybe check this out to read more about conductive filament.

    And here is where you can buy some if you are interested. http://www.makergeeks.com/coabs3dfi10.html

    I hope this answers your question and I am always glad to help!