Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs CPLD Controlled Door Lock - Soldering the CPLD
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oldmanraskers
  • Date Created: 24 May 2015 2:49 PM Date Created
  • Views 887 views
  • Likes 0 likes
  • Comments 4 comments
  • max
  • max_v_cpld
Related
Recommended

CPLD Controlled Door Lock - Soldering the CPLD

oldmanraskers
oldmanraskers
24 May 2015

I am now in the process of redesigning the circuit to accommodate a larger pin pitch CPLD, since soldering the 100 pin package proved very difficult image and I trashed three of them - admittedly I was better each time but I still ripped up tracks, moved pads, etc. etc. So... back to the drawing board.

  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago +1
    I would definitely look into SchmartBoard for a 100-pin TQFP: http://schmartboard.com/index.asp?page=products_qfp&id=68 However, see if you can get away with a Xilinx XC9536XL or XC9572XL in a 44-pin PLCC…
  • johnbeetem
    johnbeetem over 11 years ago

    I would definitely look into SchmartBoard for a 100-pin TQFP: http://schmartboard.com/index.asp?page=products_qfp&id=68

     

    However, see if you can get away with a Xilinx XC9536XL or XC9572XL in a 44-pin PLCC.  You can even socket those with 0.1" through-hole pins.

     

    Or find a cheap CPLD module that already has the CPLD soldered on and has 0.1" connectors you can adapt, or has room for prototyping the rest of your circuitry.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to oldmanraskers

    From what I see, liberal use of paste and heat with gun or oven until the paste separates. Solder should never be used on the BGA unless you have a rock solid hand (which I do not).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oldmanraskers
    oldmanraskers over 11 years ago in reply to clem57

    image I did use solder paste and a heat gun... and soldering iron... I just kept getting bridges and in the end I snapped the legs etc.. I need to experiment some more I think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    are you really soldier these? Look at Schmart boards or use soidler paste instead. Then use heat to reflow the paste.