Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Current Sensor 1. Introduction.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: peterjcs23
  • Date Created: 21 Feb 2015 5:26 PM Date Created
  • Views 3899 views
  • Likes 7 likes
  • Comments 18 comments
  • rogowski
  • current
  • hall-effect
  • know-how
  • shunt
  • hall
  • electronics
  • analog
  • sensor
Related
Recommended

Current Sensor 1. Introduction.

peterjcs23
peterjcs23
21 Feb 2015

Current Sensor 1. Introduction.

 

19 Feb 2015

 

Voltage and current sensing are fundamental to electrical and electronic circuits. Pretty much all analogue parametric sensors have a voltage output that is going to be compatible with the input of some measuring device, for example an ADC or the input to an amplifier. Current sensors must in some way convert the current to voltage for measurement and in general there are 2 methods, either a resistor is in the current path and the voltage across the resistor is measured, or the magnetic field around the current path is detected and converted to voltage for measurement. In the photograph at the heading of this blog both types of current sensor are represented.

 

Current sensing is required in a wide range of electrical and electronic applications. For example:

  • Battery life indicators and chargers
  • Over-current protection
  • Current and voltage  regulators
  • Power supply controllers
  • Current control in solenoids
  • Motor torque control
  • Heater controls
  • And so on

 

The current may range from milliamps to thousands of amps, it may be DC or AC, it may be steady or transient.


Direct current sensing – resistive - invasive.

 

Direct resistive current sensing is based on Ohm’s Law, by placing a resistor (perhaps referred to as a current shunt) in series with a load, a voltage is generated that is proportional to the current. The voltage may be scaled by an amplifier before it is passed to the measurement circuit. The amplifier may be a specialist current shunt monitor, an operational amplifier, a difference amplifier or an instrumentation amplifier. This method of measurement is referred to as invasive, there is no galvanic isolation, as the current shunt resistor and measurement circuit are connected to the circuit whose parameters are being measured; so grounding and common mode voltage must be considered when such a measurement is made. If galvanic isolation is required with a current shunt then an isolation amplifier must be used. The current shunt resistor will dissipate heat as I2R and the value of R used will be determined by the allowed heating effect traded off with the sensing voltage range and the amplifier gain.


Indirect current sensing – magnetic field – isolated.

 

Indirect current sensing is based on Ampere’s and Faraday’s laws of magnetism. There are a number of configurations for the sensing element relative to the current carrying conductor. If a toroid magnetic material is wrapped around the conductor and a slot is cut in it, then the magnetic field in the resulting air gap is proportional to the current in the conductor. The magnetic field must be converted to a voltage in order to measure it and a Hall Effect sensor is often used. This type of sensor has no direct connection to the circuit that carries the current and is therefore isolated or non-invasive. In a variant of this method, the toroid may have a secondary coil wound onto it and a current passed through the coil such that it opposes the field of the conductor we wish to measure. In this case, a closed loop circuit sets the secondary current to achieve zero field in the air gap; the secondary current is proportional to the primary current and can be measured by a current shunt; galvanic isolation still exists between the primary and secondary circuits.

Current transformers work with AC current by winding a large number of turns onto the secondary of the transformer core and the primary is a single turn passing through the core. The current in the secondary is measured by generating a voltage across a resistor but galvanic isolation is maintained between the measurement and primary circuits.

A Rogowski current sensor is an air cored coil where the coil is wrapped around the conductor. The voltage output of such a coil is proportional to the rate of change of current so an integrator is used to generate a voltage for the measurement circuit.

 

image

 

Types of current sensor:

  1. Typical current shunt resistor, 200A generates 50mV output.
  2. Current measurement resistor, 0.05R.
  3. Toroid made of silicon steel with a Hall Sensor in an air gap.
  4. Closed loop Hall Sensor, the secondary coil is wound on a ferrite core and potted.
  5. Current Transformer
  6. Rogowski coil made on a PCB with integrator and amplifier.
  7. These sensors all use a toroid, air gap and Hall sensor.
  8. These sensors use a magnetic core and Hall sensor miniaturised into a package with an amplifier.
  9. 20A current shunt in a DC electrical meter.

Also available at https://electronicsknowhowblog.wordpress.com/

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor +2
    You can automate anything w.r.t. PCB designs. Write your code to generate a script file (.scr) which EAGLE can read, and it can contain any arbitrary lines with any arbitrary co-ordinates. Basically, express…
  • COMPACT
    COMPACT over 9 years ago

    This makes me potentially loopy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    Ultra-sensitive current measuring has its applications in physics and astrophysics, but, lest we forget, also in biological research, in studying the nervous system particularly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    Now I feel like a pedantry Olympian!

     

    The very definition of current is in flux:

     

    Ampere

    The definition of the ampere is undergoing a major overhaul—the current definition, which is difficult to realise with high precision in practice, is being replaced by a definition that is more intuitive and that is easier to realise.

    Current definition: The ampere is that constant current which, if maintained in two straight parallel conductors of infinite length, of negligible circular cross-section, and placed 1 m apart in vacuum, would produce between these conductors a force equal to 2×10−7 newton per metre of length.
    Proposed definition: The ampere, A, is the unit of electric current; its magnitude is set by fixing the numerical value of the elementary charge to be equal to exactly 1.60217X×10−19 when it is expressed in the unit A·s, which is equal to C.

    Since the current definition contains a reference to force which has the dimensions MLT−2 it follows that in SI the kilogram, metre and second, the base units representing these dimensions, must be defined before the ampere can be defined. Other consequences of this definition are that in SI the value of vacuum permeability (μ0) is fixed at exactly 4π×10−7 H·m−1.[34] Since the speed of light in vacuum (c) is also fixed, it follows from the relationship

    image

    that the vacuum permittivity (ε0) has a fixed value and from

    image

    that the impedance of free space (Z0) likewise has a fixed value.[35]

    One consequence of the proposed changes to the definition of the ampere is that the definition will no longer be dependent on the definitions of the kilogram and the metre, but will still be dependent on the definition of the second. In addition the vacuum permeability, vacuum permittivity and impedance of free space, which, in the current definition have exact values will, in the future, be subject to experimental error.[36]

    from WIKI:

    https://en.wikipedia.org/wiki/Proposed_redefinition_of_SI_base_units#Ampere

     


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • peterjcs23
    peterjcs23 over 10 years ago in reply to D_Hersey

    If ever I need to detect gravitational waves, I'll remember your post, thanks! Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    If ya' need ultra-sensitivity, you can use a SQUID

     

    An Ultra High Sensitive Current Sensor based on Superconducting Quantum Interference Device

     

    Now, I feel like a pedant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>