Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DAC8775 Quad-Channel DAC EVM - part 5: HART Interface
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 3 Aug 2018 8:54 PM Date Created
  • Views 4939 views
  • Likes 8 likes
  • Comments 21 comments
  • firmware
  • industrial
  • dac8775
  • hart_network_connectivity
  • ti_rt
Related
Recommended

DAC8775 Quad-Channel DAC EVM - part 5: HART Interface

Jan Cumps
Jan Cumps
3 Aug 2018

For the Instrumentation, Automation and Industrial Application fanboys.

And for anyone interested in communication protocols that are widely used but not commonly known.

 

I'm checking the Highway Addressable Remote Transducer Protocol interface on the DAC8775.

image

 

 

HART Protocol

 

The HART protocol communicates info on a current loop by adding a small AC component to the current loop.

The frequency of that component defines that you're sending a mark (1200 Hz) or space (2200 Hz).

That's all I'll tell about the protocol. The blog is not about how it works, but how to use it with the DAC8775.

Secretly I hope this gets you interested in a widely used industrial communication protocol,

 

DAC8775 and HART

 

From the DAC8775 datasheet:

DAC8775 is also implemented with a Highway Addressable Remote Transducer (HART) Signal Interface to superimpose an external HART signal on the current output.

 

The HART peripheral is only useful in current mode. The HART signal is a communication component added to the current output that DAC is set to.

The DAC8775 implements the physical layer. It doesn't know HART protocol or data handling, but can generate the compliant signal on its output.

In essence, it accepts a sinusoidal signal of 0.5 Vpp, either 1200 or 2200 Hz, and translates that in an AC current component on the output of 1 mA

image

The image above, from the DAC8775 datasheet, shows how the DAC, when set to a  6 mA DC output current, mixes a HART signal of 0.5 mApp to it.

 

EVM Board Modification

 

The evaluation kit used in the element14 Road Test has no breakout point for the HART inputs. On each of the 4 DAC channels, that pin is coupled to ground via a capacitor.

image

I'm using channel A, so I have removed the capacitor for that module's HART input - C58, and soldered a patch wire to the PCB.

imageimage
imageimage

 

 

The HART input signal has to be capactive coupled. The HART pins on the DAC8775 have a DC bias. I used a 0.470 µF capacitor.

According to the data sheet, a value between 10 and 20 nF is recommended. I wasn't in the mood to go look for one.

 

 

Testing the HART Interface

 

There are two things you have to do:

  • enable the HART interface on the DAC in your firmware
  • provide the HART input signal. A sinus of 0.5Vpp, with 1200 or 2200 Hz frequency.

 

To enable the HART interface, you need to set bit 13 of the DAC Config register 0x04.

 

image

In our initial example, we were setting the bit 12 high, because we enabled the DAC output.

So we only have to change that part of the code, and instead of sending 00010000b (0x10), we send 00110000b (0x30).

 

    TX_Data_Master[0] = 0x04;
//    TX_Data_Master[1] = 0x10; // output on, default slew rate without HART
    TX_Data_Master[1] = 0x30; // output on, default slew rate with HART
    TX_Data_Master[2] = 0x05; // slew rate off, 0 - 20 mA mode
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

We're setting an output current of 10 mA. Or range is from 0 to 20 mA, so we need to set the half of 0xffff: 0x07ff.

 

    TX_Data_Master[0] = 0x05;
    TX_Data_Master[1] = 0x7f;
    TX_Data_Master[2] = 0xff;
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

That's all for the firmware. If you run it, the HART intrface for Channel A is enabled.

 

I simulate the HART signals with a generic function generator. I set it to sinus 1200 and 2200 Hz. I used my oscilloscope to set up a 500 mVpp output after the coupling capacitor of 0.470 µF.

Then I inserted the signal into the DAC and checked the output. Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage.

I attached channel 2 of my oscilloscope to the output of the µCurrent.

 

 

image

 

The yellow signal is the HART input, generated by the function generator. It's 500 mV, 1.2 kHz.

The blue signal represents the DAC's output current. Each mA is a mV on the Oscilloscope display.

You see the DC component of 10 mA, and the 0.5 mVpp AC component superposed by the HART interface.

 

For the reader, this isn't spectacular. But in industrial installations, this can be used (and is regularly used) as a digital communication path over the commonly used analog instrumentation current loops.

 

 

 

Related Blog
DAC8775 Quad-Channel DAC EVM - unlicensed roadtest part 1: Raw SPI
DAC8775 Quad-Channel DAC EVM - part 2: Firmware
DAC8775 Quad-Channel DAC EVM - part 3: Slew Rate Control
DAC8775 Quad-Channel DAC EVM - part 4: Current Mode
DAC8775 Quad-Channel DAC EVM - part 5: HART Interface
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +2
    jc2048 wrote: ... Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage. Why not just use a resistor to convert the current to a voltage…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +2
    jc2048 wrote: This HART stuff is interesting. Wonder why they chose a modem standard from 1960-something? ... I can only guess. The 1200 - 2200 Hz standard (imposed on a current) has proven to be reliable…
  • DAB
    DAB over 8 years ago +2
    Nice update Jan. Thanks for showing how to use this embedded communications port. DAB
Parents
  • jc2048
    jc2048 over 8 years ago

    This HART stuff is interesting. Wonder why they chose a modem standard from 1960-something?

     

    Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage.

    Why not just use a resistor to convert the current to a voltage?

     

    If you used a 500R resistor (quarter watt or better - a pair of 1k resistors in parallel, maybe?), you could use a voltage probe and you'd see a voltage signal the same size as the one you're feeding in.

     

    I'm presuming here that the output is floating and the current is sourced rather than sunk, so it doesn't matter if you have the grounds on both the input side and the current output side connected to your 'scope ground (but you're now the expert on this chip, so you decide if that's correct or not).

     

    That way you'll probably see a better signal and can properly measure the current amplitude (if you have a reasonably accurate resistor); you'll be able to measure the delay; and, if your generator has a sweep capability, you can see what the frequency response is like (not essential, but what kind of engineer are you if you're not curious about these kind of things?)

     

    Forgot, we're meant to be doing [+] as well as [-]. Really good 'not a Road Test' you're doing here. Keep up the good work. Have a star.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    ...

     

    Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage.

    Why not just use a resistor to convert the current to a voltage?

     

    If you used a 500R resistor (quarter watt or better - a pair of 1k resistors in parallel, maybe?), you could use a voltage probe and you'd see a voltage signal the same size as the one you're feeding in.

     

    ...

    Mainly because I have a µCurrent. No need to think, just plug it in as the DAC's load. The A to V conversion is printed on the front panel so the brain does not have to come into action.

    It also has convenient banana plug inputs and outputs. It allows me to make my setup a little easier. And with its internal amp it lifts the signal a little more above the noise.

    I don't always use it. Most of the times when playing with the DAC's current mode, I just used my DMM in mA or µA mode directly as a load across the DAC output.

     

     

    I'm presuming here that the output is floating and the current is sourced rather than sunk, so it doesn't matter if you have the grounds on both the input side and the current output side connected to your 'scope ground (but you're now the expert on this chip, so you decide if that's correct or not).

     

    The input signal is capacitive coupled. My generator shares the same ground as the whole circuit.

    Here's the internal Current Output driver of a DAC8775 channel: It can source and sink.

    image

     

     

     

     

    That way you'll probably see a better signal and can properly measure the current amplitude (if you have a reasonably accurate resistor); you'll be able to measure the delay; and, if your generator has a sweep capability, you can see what the frequency response is like (not essential, but what kind of engineer are you if you're not curious about these kind of things?)

     

    My function generator has a built-in sweep option. It's very basic though - I can only sweep from DC to a set frequency. Not a subrange (here 1200 - 2200 Hz range would be nice).

    It does have an external input though where you can control frequency with a voltage. I have an instrument here that I can program to ramp between two voltages.

    I could even use that same ramp voltage as the Y signal for the scope in XY-mode and have some frequency chart.

     

    A few years ago, I probed the function generator to find the signals related to the ramp functionality.

    image

    I found both the sweep start trigger and the sweep sawtooth signal.

    I made a little buffer for both signals so that I could use them as either Y axis for my scope (in XY mode) or as trigger signal in normal mode.

    I still have the little device, but have removed it from the function generator when I blew up its output stage.

     

    image

    image

    21/04/2014. Go figure ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    ...

     

    Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage.

    Why not just use a resistor to convert the current to a voltage?

     

    If you used a 500R resistor (quarter watt or better - a pair of 1k resistors in parallel, maybe?), you could use a voltage probe and you'd see a voltage signal the same size as the one you're feeding in.

     

    ...

    Mainly because I have a µCurrent. No need to think, just plug it in as the DAC's load. The A to V conversion is printed on the front panel so the brain does not have to come into action.

    It also has convenient banana plug inputs and outputs. It allows me to make my setup a little easier. And with its internal amp it lifts the signal a little more above the noise.

    I don't always use it. Most of the times when playing with the DAC's current mode, I just used my DMM in mA or µA mode directly as a load across the DAC output.

     

     

    I'm presuming here that the output is floating and the current is sourced rather than sunk, so it doesn't matter if you have the grounds on both the input side and the current output side connected to your 'scope ground (but you're now the expert on this chip, so you decide if that's correct or not).

     

    The input signal is capacitive coupled. My generator shares the same ground as the whole circuit.

    Here's the internal Current Output driver of a DAC8775 channel: It can source and sink.

    image

     

     

     

     

    That way you'll probably see a better signal and can properly measure the current amplitude (if you have a reasonably accurate resistor); you'll be able to measure the delay; and, if your generator has a sweep capability, you can see what the frequency response is like (not essential, but what kind of engineer are you if you're not curious about these kind of things?)

     

    My function generator has a built-in sweep option. It's very basic though - I can only sweep from DC to a set frequency. Not a subrange (here 1200 - 2200 Hz range would be nice).

    It does have an external input though where you can control frequency with a voltage. I have an instrument here that I can program to ramp between two voltages.

    I could even use that same ramp voltage as the Y signal for the scope in XY-mode and have some frequency chart.

     

    A few years ago, I probed the function generator to find the signals related to the ramp functionality.

    image

    I found both the sweep start trigger and the sweep sawtooth signal.

    I made a little buffer for both signals so that I could use them as either Y axis for my scope (in XY mode) or as trigger signal in normal mode.

    I still have the little device, but have removed it from the function generator when I blew up its output stage.

     

    image

    image

    21/04/2014. Go figure ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    My function generator has a built-in sweep option. It's very basic though - I can only sweep from DC to a set frequency. Not a subrange (here 1200 - 2200 Hz range would be nice).

    I was interested in what happens outside the 1200-2200 range. I think we can assume TI has managed a fairly level response over that range. I wondered if the modulation could be higher in frequency? The high-end response might just be that of the current drive circuit (whatever that is).

     

    On the low side, the response may well be what you get from the coupling capacitor working into the input resistance.

     

    Anyway, I think you're over-thinking things. Set it to sweep to 10kHz, plug it in and see what you get out on the current-loop side. The input is AC coupled, so you're not going to upset the chip. If you're really nervous, include a series resistor of a few hundred ohms on the input.