Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DIY Soldering Station Part 3
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adsicks
  • Date Created: 16 Mar 2017 3:53 PM Date Created
  • Views 2525 views
  • Likes 4 likes
  • Comments 15 comments
  • diy rework station
  • openscad
  • carpentry
Related
Recommended

DIY Soldering Station Part 3

adsicks
adsicks
16 Mar 2017

I made the clamp to hold my extra pair of hands in place yesterday. It took about an hour.

 

I started out measuring the base of my hands and making a 3D model in OpenScad.

 

image

To start my cuts I set my blade to take out approximately half of the height of the base of the hands. I put a mark on a scrap board and used it to set my saw.

image

Then a marked two scraps the same width as one of the legs...

image

And cross cut them at the set depth (mindful of my thumb. I didn't want to chop it off today).

image

 

Then I checked my depth against the base of my extra hands.

image

I made adjustments to my saw depth and cut it until I got it flush. Next, I went back to my model and looked at the cut lay out.

image

 

 

 

And marked my wood.

 

image

 

I did the cross cut first. I used a long piece of wood because I like my thumbs.

 

image

 

I went a little past the line to make sure my channels were deep enough. It is alright if they aren't as deep towards the line as I am about to cut the channel along the grain of the wood.

 

To mark the channel for the back of the base I line the back of my extra hands with the line, put a mark and marked it with a speed square.

 

image

image

 

Then I cut the channel to my marks. It is important to have a square edge to work with for this step.

 

image

 

I used one of the scraps from my first steps to check my depth with the extra hands.

 

image

I cut out the top part from the edge. I turned it around and marked the hole for the neck. I adjusted the saw to the table for a full cut and notched out the neck hole. I used the full board to make this safer.

 

image

 

I used a jig saw to finish out the notch. Then I cut my pieces out of the larger board and dry fitted it.

image

 

It also helps to put the hands in it at this point to see if it fits the way you want it.

 

When I was satisfied I started the gluing process. First I glued the risers on the base with Gorilla Glue...

image

 

And clamped.

image

 

I only left it clamped for 30 minutes since I was clamping the top part along the same axis. Then I glued the top part with more Gorilla Glue and clamped.

 

image

 

Then I drilled the hole to hold the front clamp on. The finished product holding the hands should look like this:

 

image

 

Here is the open scad code for the exploded view:

 

//Base

rotate([180,0,180])

translate([-4,0,0])

difference(){

cube([4,2,0.75]);

translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

translate([-0.05,1,-0.00005]) cube([4.1,1.1,0.375]);

    translate([2,0.5,0]) cylinder(r=0.1875);

    

}

 

 

// Front clamp

 

 

translate([0,-1,0])

difference(){

    cube([4,1,0.75]);

    translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.3751]);

    translate([2,0.5,0]) cylinder(r=0.1875);

  }

 

 

// Back clamp

 

translate([0,2,1])

difference(){

    cube([4,1,0.75]);

    translate([-0.05,-0.05,-0.0001]) cube([4.1,1.1,0.375]);

    translate([1.5,0,0]) cube([1,0.5,0.75]);

  

}

 

 

translate([0,1.25,.5]) cube([1,1,0.75]);

 

 

translate([3,1.25,.5]) cube([1,1,0.75]);

 

 

Thanks to my helper, Paul, who took the action shots....

  • Sign in to reply
Parents
  • COMPACT
    COMPACT over 9 years ago

    A FRIENDLY NOTE

    Be aware that your ESD mat is not a compliant ESD mat!

    I've just found out that the JAKEMY JM-Z16 is just a silicone mat with a very thin ESD coating that is very easily damaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    The mat has:

    Three-tier structure: upper layer: antistatic layer; middle layer: shock

    absorption layer, electronic components protector; lower layer:

    conductive layer

     

    Plus, I'm going to tie all of my clips and extra set of hands to ground

    and a ground clip for my wrist strap. I guess if you need more paths to

    ground or are hard on your workspace use a different mat....

     

    What I am worred about is making sure I turn the ESD lines off if I

    bring something up live....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to adsicks

    I suggest finding someone with the proper ESD measuring tools to validate your mat.

     

    Something like element14's bench mat is a winner!

    069-0024 - MULTICOMP - EU ESD WORK STATION KIT | element14 Australia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    Or just build it in a later project....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    Or just build it in a later project....