Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DIY Soldering Station Part 3
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adsicks
  • Date Created: 16 Mar 2017 3:53 PM Date Created
  • Views 2538 views
  • Likes 4 likes
  • Comments 15 comments
  • diy rework station
  • openscad
  • carpentry
Related
Recommended

DIY Soldering Station Part 3

adsicks
adsicks
16 Mar 2017

I made the clamp to hold my extra pair of hands in place yesterday. It took about an hour.

 

I started out measuring the base of my hands and making a 3D model in OpenScad.

 

image

To start my cuts I set my blade to take out approximately half of the height of the base of the hands. I put a mark on a scrap board and used it to set my saw.

image

Then a marked two scraps the same width as one of the legs...

image

And cross cut them at the set depth (mindful of my thumb. I didn't want to chop it off today).

image

 

Then I checked my depth against the base of my extra hands.

image

I made adjustments to my saw depth and cut it until I got it flush. Next, I went back to my model and looked at the cut lay out.

image

 

 

 

And marked my wood.

 

image

 

I did the cross cut first. I used a long piece of wood because I like my thumbs.

 

image

 

I went a little past the line to make sure my channels were deep enough. It is alright if they aren't as deep towards the line as I am about to cut the channel along the grain of the wood.

 

To mark the channel for the back of the base I line the back of my extra hands with the line, put a mark and marked it with a speed square.

 

image

image

 

Then I cut the channel to my marks. It is important to have a square edge to work with for this step.

 

image

 

I used one of the scraps from my first steps to check my depth with the extra hands.

 

image

I cut out the top part from the edge. I turned it around and marked the hole for the neck. I adjusted the saw to the table for a full cut and notched out the neck hole. I used the full board to make this safer.

 

image

 

I used a jig saw to finish out the notch. Then I cut my pieces out of the larger board and dry fitted it.

image

 

It also helps to put the hands in it at this point to see if it fits the way you want it.

 

When I was satisfied I started the gluing process. First I glued the risers on the base with Gorilla Glue...

image

 

And clamped.

image

 

I only left it clamped for 30 minutes since I was clamping the top part along the same axis. Then I glued the top part with more Gorilla Glue and clamped.

 

image

 

Then I drilled the hole to hold the front clamp on. The finished product holding the hands should look like this:

 

image

 

Here is the open scad code for the exploded view:

 

//Base

rotate([180,0,180])

translate([-4,0,0])

difference(){

cube([4,2,0.75]);

translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

translate([-0.05,1,-0.00005]) cube([4.1,1.1,0.375]);

    translate([2,0.5,0]) cylinder(r=0.1875);

    

}

 

 

// Front clamp

 

 

translate([0,-1,0])

difference(){

    cube([4,1,0.75]);

    translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.3751]);

    translate([2,0.5,0]) cylinder(r=0.1875);

  }

 

 

// Back clamp

 

translate([0,2,1])

difference(){

    cube([4,1,0.75]);

    translate([-0.05,-0.05,-0.0001]) cube([4.1,1.1,0.375]);

    translate([1.5,0,0]) cube([1,0.5,0.75]);

  

}

 

 

translate([0,1.25,.5]) cube([1,1,0.75]);

 

 

translate([3,1.25,.5]) cube([1,1,0.75]);

 

 

Thanks to my helper, Paul, who took the action shots....

  • Sign in to reply
Parents
  • COMPACT
    COMPACT over 9 years ago

    A FRIENDLY NOTE

    Be aware that your ESD mat is not a compliant ESD mat!

    I've just found out that the JAKEMY JM-Z16 is just a silicone mat with a very thin ESD coating that is very easily damaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    The mat has:

    Three-tier structure: upper layer: antistatic layer; middle layer: shock

    absorption layer, electronic components protector; lower layer:

    conductive layer

     

    Plus, I'm going to tie all of my clips and extra set of hands to ground

    and a ground clip for my wrist strap. I guess if you need more paths to

    ground or are hard on your workspace use a different mat....

     

    What I am worred about is making sure I turn the ESD lines off if I

    bring something up live....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    The mat has:

    Three-tier structure: upper layer: antistatic layer; middle layer: shock

    absorption layer, electronic components protector; lower layer:

    conductive layer

     

    Plus, I'm going to tie all of my clips and extra set of hands to ground

    and a ground clip for my wrist strap. I guess if you need more paths to

    ground or are hard on your workspace use a different mat....

     

    What I am worred about is making sure I turn the ESD lines off if I

    bring something up live....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • COMPACT
    COMPACT over 9 years ago in reply to adsicks

    I suggest finding someone with the proper ESD measuring tools to validate your mat.

     

    Something like element14's bench mat is a winner!

    069-0024 - MULTICOMP - EU ESD WORK STATION KIT | element14 Australia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    Or just build it in a later project....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    Our motto is "fOcUs on the Solution" If you have another mat this size

    to to suggest, please do so (and send me one to do a comparison report)

    if you are honestly trying to be helpful (as I believe you ARE honestly

    trying to be). It seems to everyone sitting here that hung up on a mat

    that isn't even a permanent part of this project.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to adsicks

    I've seen far too much damage to electronic equipment due to uncontrolled ESD and I don't want to see you go through so much effort and risk damage to your projects.

    Compliant ESD bench matting is often available as cheap EOR (END OF ROLL) specials. And whilst you're at it purchase some ESD mat cleanser (apparently it is different to normal cleanser).

    Here's photo of some small mats that I use as ESD bench toppers.

    They're the perfect size!

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to COMPACT

    For one, where can I get this?

    For two, can you post a link to an actual test of the mat I have? I've seen the claims that this particular pad is not actually an ESD pad, but the manufacturer says otherwise.

    For three, If a component is placed on a surface by a technician wearing a wrist strap, how likely is a high amp ESD strike from the surface to the component to the hand to the 1 megaohm impedance to the ground?

     

    I mean, yeah, I could get so paranoid I paint this and my floors with ESD paint and wear ESD shoes like I did when we were working on Disc Drives and such, but $800 worth of paint to save what now amounts to 30 or 40 dollars worth of components. I can buy a large bottle of fabric softener and a bottle of Isopropyl Alcohol  for a couple of dollars and keep it sprayed down and it will do basically the same thing.

     

    Plus, I have this StarTech mat for staging and assembly.
    image

     

    But it is about 24"X 24", doesn't have trays and doesn't have the heat tolerance I'm looking for.

     

    That all being said, it would be nice to incorporate an ESD test circuit in this project. It was part of the brainstorming, but I decided it would be a better add on later part. (I should build the workstation so I can better build the protection curcuit kind of thing).....

     

     

    But, heck, what I am doing in this post is open source. I don't have some paramilitary force that is going to come to your house and beat you into using a specific mat, design or saw, or wear special clothes or anything like that....