Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Fluke PRV240FS Proving Unit Battery Consumption
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 11 Apr 2018 8:35 PM Date Created
  • Views 4885 views
  • Likes 8 likes
  • Comments 23 comments
  • proving unit
  • fluke prv240fs
  • battery life
Related
Recommended

Fluke PRV240FS Proving Unit Battery Consumption

three-phase
three-phase
11 Apr 2018

I purchased the PRV240FS proving unit around seven weeks ago now to go with the Fluke T110 voltage tester that replaced my old Kewtech unit that decided to exit the tool bag in two halves detailed in a previous blog;

 

My new voltage probe has arrived

 

Up until last week, both Fluke units have been working fine, but last week when I went to test for dead, the proving unit did not work. This was quickly diagnosed as a set of flat batteries and the issue was solved by installing a new set. A seven week battery life though seemed a little short. The instruction leaflet that comes with the proving unit details a battery life of 1100 tests of a 10 second duration, and it certainly hasn't done that much work, closer to 200 tests as an estimate. My old Kewtech proving unit was seven years old, and has only had two sets of batteries over that time period.

 

image

 

The batteries supplied with the proving unit were four Toshiba AA Alkaline batteries, so they are form a renowned battery manufacturer. Each battery measured in the region of 1.030V on no load using a DC voltmeter, so it looks like the whole pack has been drained and not just an individual weakened battery.

 

For a little further investigation, I hooked the proving unit up to a 6V DC power supply to measure the current drawn.

 

                                             1) On initial power up the unit draws circa 16nA

                                             2) Using the finger test button test draws around 105mA

                                             3) Testing the T110 on the proving draws around 160mA

                                             4) After the first test, the unit drops back down to 16nA

                                             5) After a second test, the unit drops back down to 4.5mA

 

{gallery} PRV240FS Current Tests

image

image

image

image

 

The Toshiba batteries don't have an Ah rating on them, but an internet search suggests that AA Alkaline batteries have a rating between 1700mAh and 3000mAh. The intermittent 4.5mA drain observed would therefore fit in with draining the AA batteries over a seven week period.

 

Proving unit power consumption tests video

 

As a proving unit, this isn't much use to me and I will look for a more reliable unit to replace it with, or stick with my old Kewtech proving unit that I used with the old probe, although this only puts out DC, so does not work with non-contact voltage pens that I desired.

 

I would be interested to hear from anyone else who has purchased one of these units, if they have had any issues with battery life.

 

Update 12/04/2018

 

Working with the idea from Gene in the comments below, I have dismantled the proving unit to see what the possibility would be of adding in a small switch. Mechanically, as the pictures show, there would be space at either end, to add in a small switch. Electrically, there are some issues with interrupting the power.

 

 

{gallery} PRV240FS Dismantled

image

PRV240FS opened up

image

Board in top part of enclosure with base removed

image

Component side of board

image

Underside of board showing battery connections

image

Field sense end of case

image

Transformer end of case

image

Case Length

image

Bottom case height

image

Battery positive terminal

image

Component side of battery positive terminal

image

Battery negative terminal

image

Component side of battery negative terminal

From the photos, it can be seen that the battery terminals are soldered directly to the PCB and make electrical connections on both sides of the board. However, I believe that the positive terminal just goes to a test point pad on one side and then SNBL1 component on the other side.

 

It may be possible to cut the track to the SNBL1 component and wire the switch in-between that and the battery connection.

 

A little bit more investigation required to find a suitable switch and identify the SNBL1 component.

 

Update 17/04/2018

 

Following on from the useful comments made by members of the element14 community, I had a go at installing a switch into the proving unit that broke the battery circuit and stopped the current drain.

 

I don't have a huge stock of electronic parts as I am more electrically biased, but managed to find a suitable slide switch that could be mounted in the front case. There is a thin internal web that I drilled to provide the mounting of the switch as seen in the first photo. The switch was a little wide, so I had to carefully cut back a small piece of the ridge, seen in the second photo, to enable the switch to sit correctly and go through the front case enough to allow it to be operated. The cut out can be seen from the front in the third photo and is reasonably unobtrusive, but hopefully prominent enough that I don't forget to use it.

 

imageimageimage

 

I only had veroboard which seemed to be to thick to put between the one of the batteries and its terminal. I eventually settled on a small plastic piece cut from an old credit card that had just expired. It pushed neatly into the clips that hold the battery terminal in place. It did bend them slightly, but nothing to excessive as seen in the photo below on the left. This held the first wire in place behind the battery contact. The second wire for the switch was held in place using some aluminium foil tape seen in the second photo. I then trimmed down the aluminium foil with a craft knife.

 

imageimageimage

The board sits very close to the back of the battery case, so I had to cut out a small section of the case to allow the wires to pass out of the battery case as seen in the third picture above. I then secure the wires with a little hot glue in the cut out and along the inside of the case to the switch.

 

The switch was successfully mounted and secured with two screws into the internal web. A slight downside is that the wire crossover form the bottom half of the case to the top half now, so the unit does not dismantle as easy as it did before as seen below.

 

image

The case was then reassembled and then using my current favourite insulation tester, I conducted a 20V insulation test with the switch open, which gave a 4GOhm reading and then a 200mA resistance test with the switch closed, which gave a 0.1Ohm reading.

 

imageimage

I have a Brother P-touch printer, so made a little label up to finish off the modification shown in the first photo below. The work went reasonably well, the opposite battery terminal is now pretty much crushed up in comparison to the other terminals as can be seen in the second photo, the top battery contains the switch circuit, where as the battery below is unmodified. This may mean that the foil tape is damaged when the batteries are replaced, but with the wires glued into position, it should just mean stick on a new piece of tape when required.

 

imageimage

 

Many thanks to genebren, mcb1 and jw0752 for their suggestions and comments for ideas to resolve this, much appreciated.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +4
    Donald, That is clearly sub-standard performance for a tool battery pack. I guess the manual could be right if you just ran 1100 test right out of the box before the batteries drained due to storage. Is…
  • shabaz
    shabaz over 8 years ago +4
    That really sucks when manufacturers put so little effort into reducing the off/standby power. I have a portable ham receiver that does that, and the manufacturer states that's the way it is - and they…
  • genebren
    genebren over 8 years ago in reply to three-phase +4
    Donald, Looking at the pictures, there appears to be small surface mount switches under the two lower contact points. I assume that the probe insertion causes those switches to be pressed. Is it possible…
Parents
  • genebren
    genebren over 8 years ago

    Donald,

     

    That is clearly sub-standard performance for a tool battery pack.  I guess the manual could be right if you just ran 1100 test right out of the box before the batteries drained due to storage.  Is there any convenient way to add a power switch to disconnect that batteries during storage?

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 8 years ago in reply to genebren

    I have updated the blog to include some photos of the proving unit dismantled. There does seem to be a bit of room to physically mount a small slide switch. Connecting in electrically may be a bit awkward and I will need to ensure what PCB tracks I will need to break to wire it in.

     

    Many thanks for the idea.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to three-phase

    Donald,

    Looking at the pictures, there appears to be small surface mount switches under the two lower contact points.  I assume that the probe insertion causes those switches to be pressed.  Is it possible to adjust those switches (shave down their buttons), such that they disconnect when the probes are removed?  I don't think that bending the contacts would be a good idea.

    Just a thought.

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to three-phase

    I'd be looking at isolating the negative connection.

    It seems there are 4 small connections from the battery terminal to the ground plane, that seem to be easily isolated.

     

    The other option I use is a piece of mylar or simialr plastic slipped between one battery and the terminal.

    Yes you have to undo it, but it beats taking out batteries or flat batteries.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago in reply to three-phase

    I'd be looking at isolating the negative connection.

    It seems there are 4 small connections from the battery terminal to the ground plane, that seem to be easily isolated.

     

    The other option I use is a piece of mylar or simialr plastic slipped between one battery and the terminal.

    Yes you have to undo it, but it beats taking out batteries or flat batteries.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • three-phase
    three-phase over 8 years ago in reply to mcb1

    Yes, the negative pad on each side of the board appears to have connections to the ground plane, so I would have to do both sides. I presume you have suggested that method to avoid soldering onto the passive component and possibly causing heat damage.

     

    I must admit that I hadn't thought of that and just went for the least amount of soldering method!

     

    I did think about popping the batteries out, which is ok for short term, but the battery compartment securing is only a plastic quarter turn fastener, so I was a bit concerned that clumsy thumbs here would damage it sooner or later with repeated use.

     

    Thanks for the suggestion.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to three-phase

    Afterwards I had a sudden thought.

    The board isn't 4 layers with a ground plane in the middle is it.?

     

    The negative terminal suggestion was because it looked like the easiest solution and very easily put back if you wanted to.

     

     

    The other crude way is double side pcb between the batteries and a cable with switch wired across the side.

    You could possibly add the switch neatly inside with no modifications to the circuitry.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 8 years ago in reply to mcb1

    I believe it is a standard double layer PCB, I can see a torch shine through from one side of the board to the other and I cannot see any ground plane at any of the edges or at the through holes for the PCB mounts.

     

    The PCB option may be crude, but may be an easy option for me.

     

    Kind regards