Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Getting up and running with Arm Design Start, Generating the SW
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adamtaylorcengfiet
  • Date Created: 19 Dec 2018 2:50 PM Date Created
  • Views 4345 views
  • Likes 4 likes
  • Comments 3 comments
  • cortex®
  • xilinx_explore
  • arm m3
  • fpga
  • xilinx;
  • arm m1
Related
Recommended

Getting up and running with Arm Design Start, Generating the SW

adamtaylorcengfiet
adamtaylorcengfiet
19 Dec 2018

In my last blog we examined how we could get the Arm Design Start Cortex M3 up and running on out Arty A7-35T board using the example SW application provided. In this blog we are going to look at how we can create our own application software.

 

To do this we are going to use the following tools

  • Xilinx Vivado
  • Xilinx SDK
  • Arm KEIL
  • Terminal program such as PuTTY

 

For this example we will look at how we can build the M3 example on the Arty A7, although the process for a M1 is also the same.

 

The program for both the Cortex M3 and M1 is stored within the FPGA block RAM as such the outcome of this process will be an updated FPGA bit file.

 

Lets take a walk through how we create this bit file.

 

Following completion of the build (shown in the previous blog) we will be in a position to export the hardware description file.

 

image

We do this by selecting File->Project-> Export->Export Hardware

image

 

We need to export the hardware design to the root of the software directory, this is achieved by selecting the directory in the export hardware dialog as shown below. Note we should map the project directory to the V drive. As we will be coming back to Vivado to update the bit file we do not need to include this in our export.

 

 

image

 

With the design exported, the next step is to use Vivado to open Xilinx SDK. Again we can do this using File->Launch SDK

 

 

image

 

To correctly build the application, we need to tell SDK where the exported hardware location and the SDK workspace are located, these are not located locally to the project.

 

Point the Exported location to the location we have just exported the hardware

 

image

 

The workspace can be found in the path below.

 

image

 

With both of these correctly set, clicking OK will result in Xilinx SDK being opened, within this workspace you will see the hardware definition that was just exported

 

At this stage we should also check the SDK repositories are as expected, this should point to the following directory V:\vivado\Arm_sw_repository. We can check the repository is correct by selecting Xilinx->Repositories

 

image

Note the Global Repository

image

 

Just like we do for MicroBlaze and Arm A9, A53 and R5 developments, we need to create a Board Support Package. We can do this selecting File->New->Board Support Package

image

 

This will open the BSP creation dialog, leave the project name as the automatic name and click finish.

image

 

Clicking finish will open a BSP configuration dialog, double check on the standalone tab the stdin and stdout are connected to the AXI Uart Lite.

 

image

Clicking OK will now build the BSP, you may see some warning but if done correctly you will see no errors. The next stage is to generate the ELF file which includes this BSP and the Application. However to do so we will not be using Xilinx SDK.

 

Instead we will be using Arm KEIL however, before we do we need to copy two files into the BSP include directory.

 

These files are the xpseudo_asm_rvct.c and xpseudo_asm_rvct.h which are located within Arm SW Repository.

 

image

These files should be copied in to the BSP include directory

image

 

Before we start with the Arm KEIL software development, we need to ensure we have the following paths mapped correctly in our operating system Path

 

  • C:\Keil_v5\ARM\ARMCC\bin
  • C:\Xilinx\Vivado\2018.2\bin

 

With that completed, we are ready to open up the Arm KEIL software. We can find an Arm KEIL project under the directory software/m(3/1)_for_Arty_a7/Build_Keil double click on the m(3/1)_for_arty_a7.uvprojx and the program will open.

 

image

Once Arm KEIL is open, you will be able to see the files in the BSP under the Standalone folder and the main application under the Main folder.

image

To build the executable select the rebuild option.

 

This will generate a new elf and hex file, which will be seen under the Build_Keil directory names bram_a7.elf / hex these files are also copied over to our Vivado directory which is where we need to go back to now to generate the FPGA bit file.

 

 

image

Open a windows command terminal in the directory V:\hardware\m3_for_arty_a7\m3_for_arty_a7

 

You will notice the BRAM files are also under this directory as well

 

Within the command prompt run the script make_prog_files.bat this will run Vivado and update the contents of the BRAM which contain the Cortex application. This is a much faster process than rebuilding the entire bit file from scratch.

 

image

We are now ready to test our application, to do this we need to use Vivado and the hardware manager in Vivado.

 

Once the hardware manager is open select the Open Target -> Auto Connect option this will connect to the Arty A7

 

image

 

We can then select the bit file we just generated and program the FPGA, ensure you double check the timestamp on the file to ensure it is the latest one.

 

image

 

Once this bit file is downloaded you will see the in a terminal window the application start running on the Arty A7.

 

image

We are now ready to start adding in our own SW functionality and creating our own application, that is over to you!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Nice detailed update. DAB
Parents
  • jlbrian
    jlbrian over 7 years ago

    I followed the first tutorial, and that seems to be working.  I got the following in the putty terminal:

     

    image

     

    and all of the buttons and switches seem to be responding appropriately, however, when I go to export hardware I get the following dialog:

     

    image

     

    Did I miss a step?

     

    This is the console output:

     

    start_gui

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    INFO: [Project 1-313] Project file moved from 'V:/hardware/m3_for_arty_a7/m3_for_arty_a7' since last save.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v'.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v'.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/sfdp.vmf', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/sfdp.vmf'.

    Scanning sources...

    Finished scanning sources

    WARNING: [Project 1-509] GeneratedRun file for 'synth_1' not found

    WARNING: [Project 1-509] GeneratedRun file for 'impl_1' not found

    WARNING: [filemgmt 56-2] IPUserFilesDir: Could not find the directory 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files', nor could it be found using path 'V:/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files'.

    CRITICAL WARNING: [Board 49-67] The board_part definition was not found for digilentinc.com:arty:part0:1.1. This can happen sometimes when you use custom board part. You can resolve this issue by setting 'board.repoPaths' parameter, pointing to the location of custom board files. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command.

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_project: Time (s): cpu = 00:00:20 ; elapsed = 00:00:29 . Memory (MB): peak = 800.305 ; gain = 105.840

    update_compile_order -fileset sources_1

    close_project

    open_hw

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1704] No user IP repositories specified

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_hw: Time (s): cpu = 00:00:09 ; elapsed = 00:00:06 . Memory (MB): peak = 851.555 ; gain = 0.000

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v'.

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v'.

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/sfdp.vmf'.

    Scanning sources...

    Finished scanning sources

    WARNING: [filemgmt 56-3] IPUserFilesDir: Could not find the directory 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files'.

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_project: Time (s): cpu = 00:00:11 ; elapsed = 00:00:08 . Memory (MB): peak = 859.746 ; gain = 8.191

    current_project {New Project}

    close_project

    ****** Webtalk v2018.2.2 (64-bit)

      **** SW Build 2348494 on Mon Oct  1 18:25:44 MDT 2018

      **** IP Build 2318053 on Mon Oct  1 21:44:26 MDT 2018

        ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved.

     

     

    source C:/Users/Jeramy/AppData/Roaming/Xilinx/Vivado/.Xil/Vivado-17340-DESKTOP-90VHBE3/webtalk/labtool_webtalk.tcl -notrace

    INFO: [Common 17-206] Exiting Webtalk at Sun Mar 17 08:59:15 2019...

    update_compile_order -fileset sources_1

    open_bd_design {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd}

    Adding cell -- xilinx.com:ip:axi_bram_ctrl:4.0 - axi_bram_ctrl_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_bram_ctrl_0_0

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-2] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, please note that memory depth value gets calculated based on the Data Width of the IP and Address range selected in the Address Editor.Incase a validation error occured on the range of this parameter, please check if the selected Data width and the Address Range are valid. For valid Data width and memory depth values, please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-1] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, The Maximum address range supported is 2G. Selecting the address range more than 2G in the address editor may resets the value of Memory depth to default value (1024). please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-2] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, please note that memory depth value gets calculated based on the Data Width of the IP and Address range selected in the Address Editor.Incase a validation error occured on the range of this parameter, please check if the selected Data width and the Address Range are valid. For valid Data width and memory depth values, please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-1] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, The Maximum address range supported is 2G. Selecting the address range more than 2G in the address editor may resets the value of Memory depth to default value (1024). please refer to the AXI BRAM Controller Product Guide.

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_0_0

    ERROR: [IP_Flow 19-3461] Value 'dip_switches_4bits' is out of the range for parameter 'GPIO2 BOARD INTERFACE(GPIO2_BOARD_INTERFACE)' for BD Cell 'axi_gpio_0' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'led_4bits' is out of the range for parameter 'GPIO BOARD INTERFACE(GPIO_BOARD_INTERFACE)' for BD Cell 'axi_gpio_0' . Valid values are - Custom

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_1_0

    ERROR: [IP_Flow 19-3461] Value 'rgb_led' is out of the range for parameter 'GPIO BOARD INTERFACE(GPIO_BOARD_INTERFACE)' for BD Cell 'axi_gpio_1' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'push_buttons_4bits' is out of the range for parameter 'GPIO2 BOARD INTERFACE(GPIO2_BOARD_INTERFACE)' for BD Cell 'axi_gpio_1' . Valid values are - Custom

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_interconnect_0_0

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_quad_spi_0_0

    ERROR: [IP_Flow 19-3461] Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    INFO: [IP_Flow 19-3438] Customization errors found on 'axi_quad_spi_0'. Restoring to previous valid configuration.

    ERROR: [IP_Flow 19-3439] Failed to restore IP 'axi_quad_spi_0' customization to its previous valid configuration.

    ERROR: [BD 41-245] set_property error - Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    Customization errors found on 'axi_quad_spi_0'. Restoring to previous valid configuration.

    Failed to restore IP 'axi_quad_spi_0' customization to its previous valid configuration.

     

     

    ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

    ERROR: [BD 41-1273] Error running init TCL procedure: ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

        ::xilinx.com_ip_axi_quad_spi_3.2::init Line 8

    Adding cell -- xilinx.com:ip:axi_uartlite:2.0 - axi_uartlite_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_uartlite_0_0

    Adding cell -- xilinx.com:ip:blk_mem_gen:8.4 - blk_mem_gen_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_blk_mem_gen_0_0

    INFO: [Device 21-403] Loading part xc7a35ticsg324-1L

    Adding cell -- xilinx.com:module_ref:tri_io_buf:1.0 - tri_io_buf_0

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [BD 41-1728] Could not find a module with name: m3_for_arty_a7_tri_io_buf_0_0

    Adding cell -- xilinx.com:ip:xlconcat:2.1 - xlconcat_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconcat_0_0

    Adding cell -- xilinx.com:ip:xlconcat:2.1 - xlconcat_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconcat_1_0

    Adding cell -- xilinx.com:ip:xlconstant:1.1 - xlconstant_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconstant_1_0

    Adding cell -- Arm.com:CortexM:CORTEXM3_AXI:1.0 - Cortex_M3_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_Cortex_M3_0_0

    cell handle is /Cortex_M3_0

    CRITICAL WARNING: [BD 41-5] axi_gpio_0 does not have a bus interface called GPIO2

    CRITICAL WARNING: [BD 41-5] axi_gpio_1 does not have a bus interface called GPIO2

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_interconnect_0_1

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_single_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_single_spi_0_0

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_quad_spi_0_1

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_xip_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_xip_quad_spi_0_0

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_0_1

    Adding cell -- xilinx.com:ip:axi_protocol_converter:2.1 - axi_protocol_convert_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_protocol_convert_0_0

    Adding cell -- Arm.com:user:DAPLink_to_Arty_shield:1.0 - DAPLink_to_Arty_shield_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_DAPLink_to_Arty_shield_0_0

    Adding cell -- xilinx.com:ip:axi_crossbar:2.1 - xbar

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xbar_0

    Adding cell -- xilinx.com:ip:axi_crossbar:2.1 - xbar

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xbar_1

    Adding cell -- xilinx.com:ip:axi_protocol_converter:2.1 - auto_pc

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_auto_pc_0

    Adding cell -- xilinx.com:ip:proc_sys_reset:5.0 - proc_sys_reset_DAPLink

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_proc_sys_reset_DAPLink_0

    Adding cell -- xilinx.com:ip:proc_sys_reset:5.0 - proc_sys_reset_base

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_proc_sys_reset_base_0

    ERROR: [IP_Flow 19-3461] Value 'reset' is out of the range for parameter 'RESET BOARD INTERFACE(RESET_BOARD_INTERFACE)' for BD Cell 'proc_sys_reset_base' . Valid values are - Custom

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_interconnect_aresetn

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_interconnect_aresetn_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_peripheral_aresetn1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_peripheral_aresetn1_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_sysresetn_or

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_sysresetn_or_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_inv_dbgresetn

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_inv_dbgresetn_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_inv_sysresetn1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_inv_sysresetn1_0

    Adding cell -- xilinx.com:ip:clk_wiz:6.0 - clk_wiz_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_clk_wiz_0_0

    Adding cell -- xilinx.com:ip:xlconstant:1.1 - xlconstant_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconstant_1_1

    Successfully read diagram <m3_for_arty_a7> from BD file <C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd>

    INFO: [BD 41-433]

    Design successfully migrated to use XCI files...

    Wrote  : <C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/ui/bd_a2e86b50.ui>

    open_bd_design: Time (s): cpu = 00:00:32 ; elapsed = 00:00:51 . Memory (MB): peak = 1200.547 ; gain = 331.961

    ERROR: [Common 17-39] 'open_bd_design' failed due to earlier errors.

    update_compile_order -fileset sources_1

    open_hw

    connect_hw_server

    INFO: [Labtools 27-2285] Connecting to hw_server url TCP:localhost:3121

    INFO: [Labtools 27-2222] Launching hw_server...

    INFO: [Labtools 27-2221] Launch Output:

     

     

    ****** Xilinx hw_server v2018.2.2

      **** Build date : Oct  1 2018-20:15:45

        ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved.

     

     

     

     

    connect_hw_server: Time (s): cpu = 00:00:01 ; elapsed = 00:00:06 . Memory (MB): peak = 1218.250 ; gain = 0.000

    open_hw_target

    INFO: [Labtoolstcl 44-466] Opening hw_target localhost:3121/xilinx_tcf/Digilent/210319A7667FA

    open_hw_target: Time (s): cpu = 00:00:04 ; elapsed = 00:00:06 . Memory (MB): peak = 1876.188 ; gain = 657.938

    current_hw_device [get_hw_devices xc7a35t_0]

    refresh_hw_device -update_hw_probes false [lindex [get_hw_devices xc7a35t_0] 0]

    INFO: [Labtools 27-1435] Device xc7a35t (JTAG device index = 0) is not programmed (DONE status = 0).

    set_property PROBES.FILE {} [get_hw_devices xc7a35t_0]

    set_property FULL_PROBES.FILE {} [get_hw_devices xc7a35t_0]

    set_property PROGRAM.FILE {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7_reference.bit} [get_hw_devices xc7a35t_0]

    program_hw_devices [get_hw_devices xc7a35t_0]

    INFO: [Labtools 27-3164] End of startup status: HIGH

    refresh_hw_device [lindex [get_hw_devices xc7a35t_0] 0]

    INFO: [Labtools 27-1434] Device xc7a35t (JTAG device index = 0) is programmed with a design that has no supported debug core(s) in it.

    WARNING: [Labtools 27-3361] The debug hub core was not detected.

    Resolution:

    1. Make sure the clock connected to the debug hub (dbg_hub) core is a free running clock and is active.

    2. Make sure the BSCAN_SWITCH_USER_MASK device property in Vivado Hardware Manager reflects the user scan chain setting in the design and refresh the device.  To determine the user scan chain setting in the design, open the implemented design and use 'get_property C_USER_SCAN_CHAIN [get_debug_cores dbg_hub]'.

    For more details on setting the scan chain property, consult the Vivado Debug and Programming User Guide (UG908).

    open_bd_design {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd}

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jlbrian
    jlbrian over 7 years ago

    I followed the first tutorial, and that seems to be working.  I got the following in the putty terminal:

     

    image

     

    and all of the buttons and switches seem to be responding appropriately, however, when I go to export hardware I get the following dialog:

     

    image

     

    Did I miss a step?

     

    This is the console output:

     

    start_gui

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    INFO: [Project 1-313] Project file moved from 'V:/hardware/m3_for_arty_a7/m3_for_arty_a7' since last save.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v'.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v'.

    CRITICAL WARNING: [Project 1-311] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/sfdp.vmf', nor could it be found using path 'V:/hardware/m3_for_arty_a7/testbench/sfdp.vmf'.

    Scanning sources...

    Finished scanning sources

    WARNING: [Project 1-509] GeneratedRun file for 'synth_1' not found

    WARNING: [Project 1-509] GeneratedRun file for 'impl_1' not found

    WARNING: [filemgmt 56-2] IPUserFilesDir: Could not find the directory 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files', nor could it be found using path 'V:/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files'.

    CRITICAL WARNING: [Board 49-67] The board_part definition was not found for digilentinc.com:arty:part0:1.1. This can happen sometimes when you use custom board part. You can resolve this issue by setting 'board.repoPaths' parameter, pointing to the location of custom board files. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command.

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_project: Time (s): cpu = 00:00:20 ; elapsed = 00:00:29 . Memory (MB): peak = 800.305 ; gain = 105.840

    update_compile_order -fileset sources_1

    close_project

    open_hw

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1704] No user IP repositories specified

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_hw: Time (s): cpu = 00:00:09 ; elapsed = 00:00:06 . Memory (MB): peak = 851.555 ; gain = 0.000

    open_project C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.xpr

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7'

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/Micron_N25Q128A13E/code/N25Qxxx.v'.

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/S25fl128s/model/s25fl128s.v'.

    CRITICAL WARNING: [Project 1-19] Could not find the file 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/testbench/sfdp.vmf'.

    Scanning sources...

    Finished scanning sources

    WARNING: [filemgmt 56-3] IPUserFilesDir: Could not find the directory 'C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7.ip_user_files'.

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2018.2/data/ip'.

    open_project: Time (s): cpu = 00:00:11 ; elapsed = 00:00:08 . Memory (MB): peak = 859.746 ; gain = 8.191

    current_project {New Project}

    close_project

    ****** Webtalk v2018.2.2 (64-bit)

      **** SW Build 2348494 on Mon Oct  1 18:25:44 MDT 2018

      **** IP Build 2318053 on Mon Oct  1 21:44:26 MDT 2018

        ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved.

     

     

    source C:/Users/Jeramy/AppData/Roaming/Xilinx/Vivado/.Xil/Vivado-17340-DESKTOP-90VHBE3/webtalk/labtool_webtalk.tcl -notrace

    INFO: [Common 17-206] Exiting Webtalk at Sun Mar 17 08:59:15 2019...

    update_compile_order -fileset sources_1

    open_bd_design {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd}

    Adding cell -- xilinx.com:ip:axi_bram_ctrl:4.0 - axi_bram_ctrl_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_bram_ctrl_0_0

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-2] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, please note that memory depth value gets calculated based on the Data Width of the IP and Address range selected in the Address Editor.Incase a validation error occured on the range of this parameter, please check if the selected Data width and the Address Range are valid. For valid Data width and memory depth values, please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-1] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, The Maximum address range supported is 2G. Selecting the address range more than 2G in the address editor may resets the value of Memory depth to default value (1024). please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-2] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, please note that memory depth value gets calculated based on the Data Width of the IP and Address range selected in the Address Editor.Incase a validation error occured on the range of this parameter, please check if the selected Data width and the Address Range are valid. For valid Data width and memory depth values, please refer to the AXI BRAM Controller Product Guide.

    INFO: [xilinx.com:ip:axi_bram_ctrl:4.0-1] m3_for_arty_a7_axi_bram_ctrl_0_0: In IP Integrator, The Maximum address range supported is 2G. Selecting the address range more than 2G in the address editor may resets the value of Memory depth to default value (1024). please refer to the AXI BRAM Controller Product Guide.

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_0_0

    ERROR: [IP_Flow 19-3461] Value 'dip_switches_4bits' is out of the range for parameter 'GPIO2 BOARD INTERFACE(GPIO2_BOARD_INTERFACE)' for BD Cell 'axi_gpio_0' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'led_4bits' is out of the range for parameter 'GPIO BOARD INTERFACE(GPIO_BOARD_INTERFACE)' for BD Cell 'axi_gpio_0' . Valid values are - Custom

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_1_0

    ERROR: [IP_Flow 19-3461] Value 'rgb_led' is out of the range for parameter 'GPIO BOARD INTERFACE(GPIO_BOARD_INTERFACE)' for BD Cell 'axi_gpio_1' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'push_buttons_4bits' is out of the range for parameter 'GPIO2 BOARD INTERFACE(GPIO2_BOARD_INTERFACE)' for BD Cell 'axi_gpio_1' . Valid values are - Custom

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_interconnect_0_0

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_quad_spi_0_0

    ERROR: [IP_Flow 19-3461] Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    ERROR: [IP_Flow 19-3461] Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    INFO: [IP_Flow 19-3438] Customization errors found on 'axi_quad_spi_0'. Restoring to previous valid configuration.

    ERROR: [IP_Flow 19-3439] Failed to restore IP 'axi_quad_spi_0' customization to its previous valid configuration.

    ERROR: [BD 41-245] set_property error - Value 'qspi_flash' is out of the range for parameter 'QSPI Board Interface(QSPI_BOARD_INTERFACE)' for BD Cell 'axi_quad_spi_0' . Valid values are - Custom

    Customization errors found on 'axi_quad_spi_0'. Restoring to previous valid configuration.

    Failed to restore IP 'axi_quad_spi_0' customization to its previous valid configuration.

     

     

    ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

    ERROR: [BD 41-1273] Error running init TCL procedure: ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

        ::xilinx.com_ip_axi_quad_spi_3.2::init Line 8

    Adding cell -- xilinx.com:ip:axi_uartlite:2.0 - axi_uartlite_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_uartlite_0_0

    Adding cell -- xilinx.com:ip:blk_mem_gen:8.4 - blk_mem_gen_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_blk_mem_gen_0_0

    INFO: [Device 21-403] Loading part xc7a35ticsg324-1L

    Adding cell -- xilinx.com:module_ref:tri_io_buf:1.0 - tri_io_buf_0

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1700] Loaded user IP repository 'c:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/vivado/Arm_ipi_repository'.

    INFO: [BD 41-1728] Could not find a module with name: m3_for_arty_a7_tri_io_buf_0_0

    Adding cell -- xilinx.com:ip:xlconcat:2.1 - xlconcat_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconcat_0_0

    Adding cell -- xilinx.com:ip:xlconcat:2.1 - xlconcat_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconcat_1_0

    Adding cell -- xilinx.com:ip:xlconstant:1.1 - xlconstant_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconstant_1_0

    Adding cell -- Arm.com:CortexM:CORTEXM3_AXI:1.0 - Cortex_M3_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_Cortex_M3_0_0

    cell handle is /Cortex_M3_0

    CRITICAL WARNING: [BD 41-5] axi_gpio_0 does not have a bus interface called GPIO2

    CRITICAL WARNING: [BD 41-5] axi_gpio_1 does not have a bus interface called GPIO2

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_interconnect_0_1

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_single_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_single_spi_0_0

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_quad_spi_0_1

    Adding cell -- xilinx.com:ip:axi_quad_spi:3.2 - axi_xip_quad_spi_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_xip_quad_spi_0_0

    Adding cell -- xilinx.com:ip:axi_gpio:2.0 - axi_gpio_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_gpio_0_1

    Adding cell -- xilinx.com:ip:axi_protocol_converter:2.1 - axi_protocol_convert_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_axi_protocol_convert_0_0

    Adding cell -- Arm.com:user:DAPLink_to_Arty_shield:1.0 - DAPLink_to_Arty_shield_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_DAPLink_to_Arty_shield_0_0

    Adding cell -- xilinx.com:ip:axi_crossbar:2.1 - xbar

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xbar_0

    Adding cell -- xilinx.com:ip:axi_crossbar:2.1 - xbar

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xbar_1

    Adding cell -- xilinx.com:ip:axi_protocol_converter:2.1 - auto_pc

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_auto_pc_0

    Adding cell -- xilinx.com:ip:proc_sys_reset:5.0 - proc_sys_reset_DAPLink

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_proc_sys_reset_DAPLink_0

    Adding cell -- xilinx.com:ip:proc_sys_reset:5.0 - proc_sys_reset_base

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_proc_sys_reset_base_0

    ERROR: [IP_Flow 19-3461] Value 'reset' is out of the range for parameter 'RESET BOARD INTERFACE(RESET_BOARD_INTERFACE)' for BD Cell 'proc_sys_reset_base' . Valid values are - Custom

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_interconnect_aresetn

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_interconnect_aresetn_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_peripheral_aresetn1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_peripheral_aresetn1_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_sysresetn_or

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_sysresetn_or_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_inv_dbgresetn

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_inv_dbgresetn_0

    Adding cell -- xilinx.com:ip:util_vector_logic:2.0 - i_inv_sysresetn1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_i_inv_sysresetn1_0

    Adding cell -- xilinx.com:ip:clk_wiz:6.0 - clk_wiz_0

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_clk_wiz_0_0

    Adding cell -- xilinx.com:ip:xlconstant:1.1 - xlconstant_1

    INFO: [BD 41-434] Could not find an IP with XCI file by name: m3_for_arty_a7_xlconstant_1_1

    Successfully read diagram <m3_for_arty_a7> from BD file <C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd>

    INFO: [BD 41-433]

    Design successfully migrated to use XCI files...

    Wrote  : <C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/ui/bd_a2e86b50.ui>

    open_bd_design: Time (s): cpu = 00:00:32 ; elapsed = 00:00:51 . Memory (MB): peak = 1200.547 ; gain = 331.961

    ERROR: [Common 17-39] 'open_bd_design' failed due to earlier errors.

    update_compile_order -fileset sources_1

    open_hw

    connect_hw_server

    INFO: [Labtools 27-2285] Connecting to hw_server url TCP:localhost:3121

    INFO: [Labtools 27-2222] Launching hw_server...

    INFO: [Labtools 27-2221] Launch Output:

     

     

    ****** Xilinx hw_server v2018.2.2

      **** Build date : Oct  1 2018-20:15:45

        ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved.

     

     

     

     

    connect_hw_server: Time (s): cpu = 00:00:01 ; elapsed = 00:00:06 . Memory (MB): peak = 1218.250 ; gain = 0.000

    open_hw_target

    INFO: [Labtoolstcl 44-466] Opening hw_target localhost:3121/xilinx_tcf/Digilent/210319A7667FA

    open_hw_target: Time (s): cpu = 00:00:04 ; elapsed = 00:00:06 . Memory (MB): peak = 1876.188 ; gain = 657.938

    current_hw_device [get_hw_devices xc7a35t_0]

    refresh_hw_device -update_hw_probes false [lindex [get_hw_devices xc7a35t_0] 0]

    INFO: [Labtools 27-1435] Device xc7a35t (JTAG device index = 0) is not programmed (DONE status = 0).

    set_property PROBES.FILE {} [get_hw_devices xc7a35t_0]

    set_property FULL_PROBES.FILE {} [get_hw_devices xc7a35t_0]

    set_property PROGRAM.FILE {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/m3_for_arty_a7/m3_for_arty_a7_reference.bit} [get_hw_devices xc7a35t_0]

    program_hw_devices [get_hw_devices xc7a35t_0]

    INFO: [Labtools 27-3164] End of startup status: HIGH

    refresh_hw_device [lindex [get_hw_devices xc7a35t_0] 0]

    INFO: [Labtools 27-1434] Device xc7a35t (JTAG device index = 0) is programmed with a design that has no supported debug core(s) in it.

    WARNING: [Labtools 27-3361] The debug hub core was not detected.

    Resolution:

    1. Make sure the clock connected to the debug hub (dbg_hub) core is a free running clock and is active.

    2. Make sure the BSCAN_SWITCH_USER_MASK device property in Vivado Hardware Manager reflects the user scan chain setting in the design and refresh the device.  To determine the user scan chain setting in the design, open the implemented design and use 'get_property C_USER_SCAN_CHAIN [get_debug_cores dbg_hub]'.

    For more details on setting the scan chain property, consult the Vivado Debug and Programming User Guide (UG908).

    open_bd_design {C:/Users/Jeramy/Documents/XILINX/AT426-BU-98000-r0p0-00rel0/hardware/m3_for_arty_a7/block_diagram/m3_for_arty_a7.bd}

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jlbrian
    jlbrian over 7 years ago in reply to jlbrian

    I believe I was able to answer my own question.

     

    1) Read the Doc's

    2) Install board files.

        -- This cleared the errors I got when opening the block diagram and allowed me to proceed to the next step.

    3) Generate Block Design

    4) Export Hardware