Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Hercules LaunchPad and GaN FETs - Part 2: Make a BoosterPack
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 12 Sep 2016 11:55 AM Date Created
  • Views 4774 views
  • Likes 11 likes
  • Comments 19 comments
  • gallium_nitride
  • smart_instrument
  • boosterpack
  • lmg5200
  • texas_instruments
  • labview
  • gan
  • hercules
  • launchpad
  • test_automation
Related
Recommended

Hercules LaunchPad and GaN FETs - Part 2: Make a BoosterPack

Jan Cumps
Jan Cumps
12 Sep 2016

I'm designing a BoosterPack to evaluate GaN devices with the help of a microcontroller.

 

             image

 

The kit will have a GaN half-bridge that can control an output of 20V and 10A.

Currently the prototype can control switching frequency and duty cycle.

I'm also planning a stretch goal to integrate the design with LabView. You can then use this as a part of a test setup.

 

 

 

The Design Exists

 

I have a working prototype. I modded an existing LMG5200 evaluation kit a while ago.

I removed the discrete PWM generator and replaced it with microcontroller managed signals.

image

 

This proof of concept works, both electronics and firmware. I can make a more sturdy version now.

The switching layout is fully based on the design guidelines and the evaluation kit's PCB.

Because of the high switching frequencies and high currents, that part of the design is critical.

I'm trying to place all components similar to the application notes. This will be my first 4-layer PCB design.

 

Status

 

I have the schematic ready.

I had to create a few components and footprints (both for LMG5200 and rotary encoder, footprint only for the inductor).

image

For the PCB, I have a provisional layout. I haven't routed a single trace yet.

But I have uploaded that intermediate status to OSHPark to get an idea of how this device will look like.

Before doing that routing, I first have to verify if I can source all the components that I'm planning to use.

In particular the SMD 360° rotary encoder may be a tricky purchase.

 

image

 

image

 

To be continued...

 

Related Blogs
Hercules LaunchPad and GaN FETs - Part 1: Control Big Power with a Flimsy Mouse Scroll Wheel
Hercules LaunchPad and GaN FETs - Part 2: Make a BoosterPack
Hercules LaunchPad and GaN FETs - Part 3a: BoosterPack Layout - Reference Design
Hercules LaunchPad and GaN FETs - Part 3b: BoosterPack Layout - my version
Hercules LaunchPad and GaN FETs - Side Note A: BoosterPack Layout - Custom KiCad Parts
Hercules LaunchPad and GaN FETs - Side Note B: Look at the PCB
Rotary Encoders - Part 1: Electronics
Checking Out GaN Half-Bridge Power Stage: Texas Instruments LMG5200 - Part 1: Preview
Rotary Encoders - Part 4: Capturing Input on a Texas Instruments Hercules LaunchPad with eQEP
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958 - part 4 - Hercules LaunchPad Enhanced PWM try-out
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 10 years ago in reply to Jan Cumps +2
    Right. I've read the datasheet. Should have done that first. How many times in my life have I said "Don't guess - read the datasheet"? Firstly, I'm not an expert. I don't have direct experience of switching…
  • DAB
    DAB over 10 years ago +1
    Nice update. I like the idea of using a SBC to provide your PWM signals. That approach should give you solid control over the waveforms so that you can explore the reactions of the devices to various stimuli…
  • jc2048
    jc2048 over 10 years ago +1
    A PCB! And it's a Boosterpack (whatever that is)! I don't know what you intend for the tracking (please don't say it's going to be a job for an autorouter, entertaining though that might be), but wouldn…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to jc2048

    I'm using the layout advice in  the 'Layout Considerations for LMG5200 GaN Power Stage' appnote from the manufacturer.

    They have a proposal for a double layer pcb in the datasheet with this remark:

    To maximize the efficiency benefits of fast switching, its extremely important to optimize the board layout such

    that the power loop impedance is minimum. When using a multilayer board (more than 2 layers), power loop

    parasitic impedance is minimized by having the return path to the input capacitor (between VIN and PGND) small

    and directly underneath the first layer

     

    [...]

     

    Two-layer boards are not recommended for use with LMG5200 device due to the larger power loop inductance.

    However, if design considerations allow only two board layers, place the input decoupling capacitors immediately

    behind the device on the back-side of the board to minimize loop inductance.

     

     

    Four layer layout:

    image

     

    Two layer layout:

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago

    A PCB! And it's a Boosterpack (whatever that is)!

     

    I don't know what you intend for the tracking (please don't say it's going to be a job for an autorouter, entertaining though that might be), but wouldn't it work better if you rotated P3 (the output connector) by 180 degrees. It would then allow you to have the power ground (input gnd - GaN - output gnd) as copper on the top layer. Since all the power tracking could then be copper on the top, you might consider whether it would work well enough as a 2-layer board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to DAB

    I'm trying to control a few key things from hardware:

    - PWM Duty cycle via a rotary encoder

    - Frequency via LaunchPad buttons

     

    If I still have energy after that (and if I don't goof up my design - this is rather expensive both for PCB and components) , then also these two parameters and deadband programmable via LabWare and Serial over USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Nice update.

     

    I like the idea of using a SBC to provide your PWM signals.

     

    That approach should give you solid control over the waveforms so that you can explore the reactions of the devices to various stimuli.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<