Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Renesas Synergy AE-Cloud1 for IoT and IIoT #1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: weiwei2
  • Date Created: 7 Jul 2019 10:45 AM Date Created
  • Views 989 views
  • Likes 4 likes
  • Comments 2 comments
  • iiot
  • iot
Related
Recommended

Renesas Synergy AE-Cloud1 for IoT and IIoT #1

weiwei2
weiwei2
7 Jul 2019

This is my first attempt to use the Renesas AE-CLOUD1

It is based on S5D9

 

Installation

this applies to my Windows 10 64 bit

i originally face some problem booting the board properly. It helps to refer to https://renesasrulz.com/renesas-synergy-enterprise-cloud-toolbox/f/synergy-enterprise-cloud-toolbox---forum/9981/ae-clou…

as the quick start guide PDF is somewhat misleading and confusing.

 

first, we need some drivers:

Download location of drivers

https://cloud.renesassynergy.com/app/index.html#/device/development-kit --> download the binary firmware for kit, extract it and run the batch file. This is after we have connect the board

https://www.renesas.com/us/en/products/synergy/software/add-ons/usb-cdc-drivers.html

 

 

Jumper

J6: please choose between 5V or 3V, But for setting up, we set to 3V

 

upon plug in with 2 USB cable, it is detected as portable device, which is wrong. by right it needs to be detected as port

image

In order to do that, need run the segger installation as mentioned above (run the batch file)

image

The driver is updated by selecting serial port (COM21 in my case) and update driver. point to the USB CDC folder

 

image

post installation, the port will look like this

image

The last step is to restart the board by power cycling it.

 

Using the Board

after restarting, it will light up a green and an orange LED. We then use terminal program to connect to it, press any key

and we will get to the screen below. the LEDs are now not lighten up

image

type ktid to get the device ID and register it with the Renesas Synergy. Following the video is easiest way https://renesasrulz.com/renesas-synergy-enterprise-cloud-toolbox/f/synergy-enterprise-cloud-toolbox---forum/9981/ae-clou…

 

we then need to register this device to synergy sect with add device

on the terminal, we then need to set the username and password with command user <user name> <password>

we then issue the boot command

after that, we run turb start

it will start sending data

image

on the synergy dashboard we will see this

image

 

conclusion

the documentation is a bit confusing but once you get it running, the board is good. It has wifi as a module via PMOD, and ethernet on board. This is very suitable for prototyping IIoT as it provide both ethernet and wifi

with the 5V option, many boards and components can be run easier compared with 3.3V (although the wifi module only can work with 3V)>> i subsequently discovered that the 5V/3V option only apply to the PMOD

 

Next part of this blog is at

Renesas Synergy AE-Cloud1 for IoT and IIoT #2

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 7 years ago +1
    Nice! I bought one of the AE-CLOUD1 kits last year when the 50% coupon was posted but it is still sitting waiting for my attention. I had worked with the RX62N Dev Kit and the HEW IDE a few years back…
Parents
  • jomoenginer
    jomoenginer over 7 years ago

    Nice!  I bought one of the AE-CLOUD1 kits last year when the 50% coupon was posted but it is still sitting waiting for my attention.  I had worked with the RX62N Dev Kit and the HEW IDE a few years back which was my intro to the cloud with Exocite and I was looking to see how the new tools from Renesas faired.

     

    After seeing this, the kit has certainly moved up the list of boards to work with.

     

    Thanks for posting this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 7 years ago

    Nice!  I bought one of the AE-CLOUD1 kits last year when the 50% coupon was posted but it is still sitting waiting for my attention.  I had worked with the RX62N Dev Kit and the HEW IDE a few years back which was my intro to the cloud with Exocite and I was looking to see how the new tools from Renesas faired.

     

    After seeing this, the kit has certainly moved up the list of boards to work with.

     

    Thanks for posting this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • weiwei2
    weiwei2 over 7 years ago in reply to jomoenginer

    I am continuing my journey to Renesas Synergy AE-Cloud1 for IoT and IIoT #2 image