Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Talk SPI to EEPROM with Hercules Launchpad  Hero
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 30 Aug 2015 12:55 AM Date Created
  • Views 3661 views
  • Likes 4 likes
  • Comments 7 comments
  • hercules_launchpad
  • rm46
  • microchip
  • spi
  • serial
  • protocol
  • sp:texas_instruments
Related
Recommended

Talk SPI to EEPROM with Hercules Launchpad  Hero

martinvalencia
martinvalencia
30 Aug 2015
Related posts by Jan Cumps
part 1: from Zero to Hero
part 2: Circuit and Test Bed
part 3: Testing SPI Protocol with Bus Pirate
Talk SPI to EEPROM with Hercules Launchpad - part 4: First Trial on the RM46

 

 

Our plan was to get them working with the Texas Instruments Hercules LaunchPad MK II.

That was back in January. And then we stalled.

This blog is our path from Zero to Hero.

25LC256 connection pins to Hercules Launchpad (@Jan Cumps)
image

 

 

Details SPI communication

 

When configuring the SPI Bus HalCoGen, you have SPI_CS0 settings such as automatic so that the internal MCU module generates the control signal CS0 for enabling the external memory module 25LC256 (Microchip).

image

The result of this configuration, gives a signal CS, which changes state whenever the SPI (Hercules RMx) module finishes sending a byte by its bus.

 

in other words, send 1 byte and CS value change, this is what creates compatibility problems of Texas Instruments with Microchip series.

 

image

image

 

In the following Link my partner Jan Cumps explains how the SPI module is configured HalcoGen

Talk SPI to EEPROM with Hercules Launchpad - part 4: First Trial on the RM46

 

I make some changes to the configuration of the output pins, thus allowing me to my control signal CS, manually by program.

image

need change the configuration of CS [0], to work as a GIO

image

Extras configuration for the SPI module:

image

And

image

Codes for controlling the memory 25LC256 (Microchip)

 

As you can in the following example code, the control to the state of CS, and programming is not automatically generated by the internal SPI module.

 

Memory Status

int Ready_25LC(void) {

 

 

  uint16 buffer_status[2]={0x05,0x00};                  // Initial Instruction

 

 

  gioSetBit(spiPORT3, SPI3_CS0, LOW);

 

 

  spiTransmitData(spiREG3, &dataconfig1_t, 1, (uint16*) buffer_status);

  spiReceiveData(spiREG3, &dataconfig1_t, 1, (uint16*) buffer_status);

 

 

gioSetBit(spiPORT3, SPI3_CS0, HIGH);

 

 

  return (!bit_test(buffer_status[0], 0));

}

#define bit_test(byte,bit) (byte & (1 << bit)) // test for bit set

 

Memory read

 

 

uint16 Read_25LC(int address) {

  uint16 read_data[2];

  uint16 buffer_read[4];

 

 

  while (!Ready_25LC());

  /*Load Instruction and address and data*/

  buffer_read[0] = (uint16) 0x03;

  buffer_read[1] = (uint16) address >> 8;

  buffer_read[2] = (uint16) address;

 

 

gioSetBit(spiPORT3, SPI3_CS0, LOW);

  spiTransmitData(spiREG3, &dataconfig1_t, 3, buffer_read);

  spiReceiveData(spiREG3, &dataconfig1_t, 1, (uint16*) read_data);

  gioSetBit(spiPORT3, SPI3_CS0, HIGH);

 

 

  return (read_data[0]);

}

 

Memory Write

void Write_25LC(int address, uint8 write_data) {

  uint16 buffer_write[4]={0x06,0x00,0x00,0x00}; // Initial Instruction

  while (!Ready_25LC());

 

 

  gioSetBit(spiPORT3, SPI3_CS0, LOW);

 

 

  spiTransmitData(spiREG3, &dataconfig1_t, 1, buffer_write);

 

 

gioSetBit(spiPORT3, SPI3_CS0, HIGH);

 

 

  /*Load Instruction and address and data*/

  buffer_write[0] = (uint16) 0x02;

  buffer_write[1] = (uint16) address >> 8;

  buffer_write[2] = (uint16) address;

  buffer_write[3] = (uint16) write_data;

 

 

  /*Low CS0 and Transmit Data SPI to 25LC256 and High CS0*/

  gioSetBit(spiPORT3, SPI3_CS0, LOW);

 

 

  spiTransmitData(spiREG3, &dataconfig1_t, 4, buffer_write);

 

 

  gioSetBit(spiPORT3, SPI3_CS0, HIGH);

}

 

 

Resulting Waveform

 

image

image

 

waveform 25LC256 Datasheet (Microchip)


For the sequence of reading and writing, the state of CS remains low.

even after full 1Byte transmitted.

 

image

image

 

Program execution and memory read successfully!

image

 

 

Source Code:

Hercules RM46x SPI MEMORY 25LC256 (Microchip)

 

 

Muchas gracias Jan Cumps (Spanish)
Desde Inicios del año 2015, yo he tenido la curiosidad de poder usar los modulos de comunicacion SPI del Hercules RMx, pero siempre lo note algo dificil; pero gracias a la ayuda de usted Jan Cumps, yo he podido comprender el uso de este modulo y poder terminar el trabajo que iniciamos a principios de año, Muchos Saludos desde Peru / Arequipa.
  • Sign in to reply

Top Comments

  • terabyte21
    terabyte21 over 11 years ago +2
    Excelente Martin y Jan Cumps, sigan adelante.
  • martinvalencia
    martinvalencia over 11 years ago in reply to terabyte21 +1
    Muchas gracias por tus palabras, espero podamos mejorar aun mas el bus y llevarlo a un nuevo nivel que es el MibSPI :-)
  • DAB
    DAB over 11 years ago +1
    Very good detailed post. Well done. DAB
Parents
  • DAB
    DAB over 11 years ago

    Very good detailed post.

     

    Well done.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    Thank you very much for your feedback, communication protocols is complicated with processors that working in 32 bits, I had much trouble to declare the correct data type.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    Thank you very much for your feedback, communication protocols is complicated with processors that working in 32 bits, I had much trouble to declare the correct data type.