Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Art of Noise
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 22 May 2021 10:41 AM Date Created
  • Views 8493 views
  • Likes 14 likes
  • Comments 36 comments
  • transistor
  • 2n3904
  • noise
  • analog
Related
Recommended

The Art of Noise

jc2048
jc2048
22 May 2021

22nd May 2021

 

image

 

I've just been playing with a very simple noise generator and that's the result.

The digital phosphor of the oscilloscope presents multiple traces of the waveform as though it were sketched with a pencil or crayon.

 

In case it's of any interest, here's the circuit:

 

image

 

The internet is full of variations, with either a Zener, reverse-biased LED, or reverse-biased base-emitter junction as the avalanche 'noise diode'.

 

image

 

 

For these traces I used a reverse-biased base-emitter junction (the transistor on the left with two pins connected - the other transistor is working as a common-emitter amplifier)

and it produced a very good level of noise out on a 12V supply.

 

At lower frequencies (the scope is AC-coupled for these), the noise looks quite noise-like. Like this:

 

image

 

but if I go back to the start and show you a single trace of the first waveform, we see this

 

image

 

so we're now looking at a time scale where we can see the avalanching stopping and starting.

 

Update 4th June 2021

 

What started as a throwaway blog about an interesting/amusing waveform seems to have taken on a life of its own.

 

Thanks for all the useful comments below. They've had the useful effect of forcing me to rethink some of this.

 

1. The original circuit that I copied had an integrator (low-pass filter) in the feedback of the common-emitter stage

[the 27k and the 10uF] to set the DC bias voltage. That means that the resulting overall transfer characteristic will

be high-pass [the inverse]. I should have considered that a bit more at the time. If I simulate it with this following

circuit (I've substituted a simple signal generator, with an 8V DC offset on it, for the 'noise diode' which is the input to the circuit)

 

image

I get this for the response

 

image

That won't be entirely right - the simulation is small-signal and the generator is working large-signal - but it lets us

see in a rough way what's happening and understand it in general terms. It falls off from a few hundred Hertz downwards.

That means I'm going to see very little of the low frequency noise as the circuit will integrate it away. Indeed, if I had wanted

to use the generator circuit for audio, it would probably have been better if I had moved the low end cut-off down by

another decade [100uF might do instead of the 10uF].

 

At the top end, that plot shows quite nicely that the response is determined largely by the amplifier transistor running

out of steam and that will depend to some extent on the individual transistor.

 

2. In my reply to Shabaz in the comments, I suggested that seeing the noise decline as I filtered it with the 'scopes

noise filtering meant that it wasn't white noise. That is quite wrong and I need to correct it. Since random noise level

is a function of bandwidth, if I restrict the bandwith, I lessen the noise seen. That doesn't mean that it's necessarily

'white' noise [equal power per unit of bandwidth], but it most certainly doesn't mean the opposite [that it's not].

 

In Motchenbacher and Fitchen, they suggest that avalanche noise is white but that there is also excess noise

in the form of multistate noise that is predominently l/f. This is in a section comparing the noise performance

of zener and avalanche diodes, though I presume a reverse-biased base-emitter junction is similar.

  • Sign in to reply

Top Comments

  • geralds
    geralds over 5 years ago in reply to shabaz +6
    shabaz wrote: Hi Jon, Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit! Yes, that's an age-old way of creating noise. Simply operate a transistor…
  • fmilburn
    fmilburn over 5 years ago +5
    By coincidence I became interested in these circuits recently, mostly with the idea of making a random number generator. Horowitz and Hill have one in the Art of Electronics but I also found a good article…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to shabaz +5
    My Tektronic TBS2xxx scope had a reasonable spectrum display. Not magic, but (almost) workable in that frequency range. I gave it away to a makerspace here in Belgium, so that avenue is closed. A SA is…
Parents
  • fmilburn
    fmilburn over 5 years ago

    By coincidence I became interested in these circuits recently, mostly with the idea of making a random number generator.  Horowitz and Hill have one in the Art of Electronics but I also found a good article on the internet:  Really, Really Random Number Generator | Make: (makezine.com).  They present an algorithm by John von Neumann and a circuit that can be added to remove weighting away from the center for a binary RNG.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to fmilburn

    Thanks for the link.

     

    I've never owned a copy of 'The Art of Electronics'.  Do they give any other uses for the noise circuit? The only time I've noticed it used in actual circuits is with RNG and with analog [music] sythesizers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to jc2048

    The following condenses something I don't understand down into a few sentences and a short list.

     

    Horowitz and Hill have a chapter on noise and its analog sources (useful on where it comes from and maybe how to avoid it) as well as a section on pseudorandom noise generated digitally.  They also discuss programmable pseudorandom noise using shift registers which allows band limited white noise.  Most of the application seems to be around random number generation and audio application such as testing audio or music synthesizers.  But on page 975 of section 13.14 they also give the following for pseudorandom bit sequences:

    • pattern generation in serial link testing
    • bit scrambling in serial network protocols like Ethernet
    • sequences for error checking codes
    • radar-ranging codes
    • use as compact modulo-n dividers

    I have no idea what most of that means to be honest.  For domestic use I have seen "white" or more accurately "pink" noise used to soothe babies.  My daughter used one with my youngest grandson.  Supposedly it can help with tinnitus (which I have) and as an aid to concentration. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to jc2048

    This application note by Maxim is interesting: Building a Low-Cost White-Noise Generator (maximintegrated.com).  He uses a spectrum analyzer to show the energy across the spectrum.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to fmilburn

    I was thinking more of where genuine randomness would be advantageous.

     

    Pseudo-random sequences are popular because the sequence is actually deterministic, even though it might have statistical properties that make it look similar to random noise. That allows it to be recognised, followed, and removed, or just confirmed it has been correctly received, in the case of the link test.

     

    You might add to their uses for pseudo-random sequences:

    - dither in data conversion

    - evenly spreading energy across a band for a modulated signal

     

    One thing to be cautious of is that pseudo-random sequences [of ones and zeroes] don't necessarily make for good pseudo-random numbers if you take a run of the bits coming out.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to fmilburn

    I was thinking more of where genuine randomness would be advantageous.

     

    Pseudo-random sequences are popular because the sequence is actually deterministic, even though it might have statistical properties that make it look similar to random noise. That allows it to be recognised, followed, and removed, or just confirmed it has been correctly received, in the case of the link test.

     

    You might add to their uses for pseudo-random sequences:

    - dither in data conversion

    - evenly spreading energy across a band for a modulated signal

     

    One thing to be cautious of is that pseudo-random sequences [of ones and zeroes] don't necessarily make for good pseudo-random numbers if you take a run of the bits coming out.