Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Transistors: Saturation Part 2 and Inverse Mode
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 12 Feb 2019 9:17 AM Date Created
  • Views 1916 views
  • Likes 7 likes
  • Comments 1 comment
  • analog design
  • saturation
  • inverse mode
  • transistors
Related
Recommended

Transistors: Saturation Part 2 and Inverse Mode

jc2048
jc2048
12 Feb 2019

This is another exploratory blog relating to bipolar junction transistors (BJTs). It follows on from a previous blog which

can be found here Transistors: Saturation

 

Be aware that I'm not an expert in all this: I'm studying it and you're looking over my shoulder as I experiment and explore

the subject. So this is not a tutorial and it's possible that some of my explanations may, at times, be wrong.

  

Introduction

  

In the previous blog I looked at the collector and base saturation voltages of small bipolar junction transistors at moderately

high collector currents in the range up to 200mA. I took my cue for that from the kind of figures seen in datasheets. It gives

a sensible idea of the kind of collector saturation voltage that might be encountered when using the transistor to switch a

load of some sort.

  

Something that was evident from doing that experiment was that there was a fair amount of variation in saturation voltage

over the range of currents I looked at.

 

I became curious to see in more detail what happens at lower currents; whether the saturation voltage would keep going down

or level out. I also wanted to try out a technique (inverse mode operation) that is sometimes suggested in old books on transistor

design for reducing saturation voltage in circumstances where it might be quite critical; I was curious to see if it would work with

modern transistors.

  

The current source I used in part 1, with a differential amplifier to amplify the voltage from a current-sense resistor and a second

op amp to compare that to an input voltage and run a control loop with the help of an output transistor, wasn't particularly stable

and had particular difficulty with the 2N3904 part. For this blog I decided that as the currents involved could be delivered directly

by an op-amp output I'd try something like a pair of Howland current regulators, one for the collector and one for the base.

  

Saturation voltage at lower currents

  

To start with, I'm going to stick with the ten-to-one ratio between collector current and base current and have the collector current

in the range 0-10mA and the base current as 0-1mA. Here is the circuit

 

 image

  

and here it is built on a breadboard (the transistor under test in that shot is the 2N30532N3053 which is housed in a TO39 can)

 

image

  

Note that the circuit inverts, so I had to arrange for the ramp from the generator to go from 0V to -1V to sweep from 0mA to 10mA

for the collector and 0mA to 1mA for the base.

  

To test that the currents were correct, I placed 100R resistors to ground instead of connecting to the transistor and quickly checked

that the traces were linear ramps and had the correct voltages to correspond to the currents, which they did. It isn't amazingly precise,

but it's good enough for this blog and to get a feel for how the transistors behave [I can see myself automating this at some point with

processor-controlled voltage and current sources].

  

I'm going to test again the three transistor types I tried previously.

 

image

 

Here are the traces (the yellow trace is the base voltage, the blue trace is the collector voltage):

  

2N3904:

 

 image

  

BC548:

  

image

  

2N30532N3053:

 

image

 

There's quite a variation between the devices. All in all, the 2N3904 looks quite poor compared to the others. The BC548 has a higher

gain than the other two, so that would perhaps suggest that the rise again in the saturation voltage at low currents with the other two

may come from the device starting to come out of saturation as the gain falls off.

  

The current sources now work a lot better, though the somewhat imprecise tracking between the two is messing things up a little on

the lefthand side where the base current is only a few tens of uA.

  

Inverse mode operation

  

This sounds very technical but simply means using the transistor upside down, so that we're swapping the emitter and collector over.

The transistor is very inefficient operated like this and will have hardly any gain, but it might have a lower saturation voltage. Old books

used to suggest this a way of getting a very low saturation voltage for switches used in chopper amplifiers but I suspect that with

efficient modern transistors the benefits might not be so great.

  

To make this work, I'm going to have the base current the same as the collector current so that I'm not asking for any current gain at all

from the transistor; that gives it a good chance to bottom and get to the saturation point. For a fair comparison, I'll test the transistor

both ways round because the saturation voltage one-to-one will probably be different to what I measured before.

  

Here are the curves. For each transistor type, the first screen capture is for the normal mode and the second one is inverse mode.

  

2N3904:

 

 image

image

  

BC548:

 

image

 

image

  

2N30532N3053:

 

image

 

image

  

Conclusion from that I think is that there is value in driving the base harder in the normal mode but that the benefit of inverse mode is

only a slight improvement (possibly a mere 10% or 20% reduction in the saturation voltage). [On a practical note, something to watch

out for if you were tempted to use a transistor in inverse mode is the breakdown voltages - the reverse breakdown voltage of the

base-emitter junction is normally something like 8V or 9V (it usually gets specified as either 5V or 6V on a datasheet). In inverse mode that

then determines how far above the base you can have the emitter that is now pretending to be the collector.]

  

So, beware of what you read in 50-year-old books. Caveat scholaris! (or whatever the Latin would be).

  

What I have shown, though, is that if the saturation voltage is important to you then choice of device makes a considerable difference,

as does how hard you drive the base (but keep in mind it will slow further the turn-off time and add to the dissipation) and also the

collector current you work at (if you happen to have a choice in that).

  

Bear in mind that these aren't precision measurements and if you wanted to apply this in some way you'd need to do some experimenting

of your own. In particular, I've avoided any mention of how the voltage varies with temperature (it does) and that then means that device

dissipation will be an issue, particularly at the higher currents [when manufacturers do these tests, they do them with a pulse test where

the device is on for just 2% of the time to avoid the temperature effects].

 

If you found this interesting and would like to see more of the blogs I've written, a list can be found here: jc2048 Blog Index

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago +2
    [I can see myself automating this at some point with processor-controlled voltage and current sources] The DAC / ADC board that we made could be used to deliver the voltages (positive only though). Peter…
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    [I can see myself automating this at some point with processor-controlled voltage and current sources]

    The DAC / ADC board that we made could be used to deliver the voltages (positive only though).

    Peter Oakes' GUI (or any program that can shoot SCPI commands to a COM port) and the default firmware for the eload support this.

    There are low level ADC and DAC commands.

    note: Currently that firmware is not polling ADC 4 because it's not used in the design.

    You'd have to change this define to 4 to get ADC 4 polled too:

     

    // adc 4 is not used. Sample 3 channels
    #define ADC_ACTIVE_INPUTS 3

     

     

    (in adc_impl.c. recompilation is needed).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago

    [I can see myself automating this at some point with processor-controlled voltage and current sources]

    The DAC / ADC board that we made could be used to deliver the voltages (positive only though).

    Peter Oakes' GUI (or any program that can shoot SCPI commands to a COM port) and the default firmware for the eload support this.

    There are low level ADC and DAC commands.

    note: Currently that firmware is not polling ADC 4 because it's not used in the design.

    You'd have to change this define to 4 to get ADC 4 polled too:

     

    // adc 4 is not used. Sample 3 channels
    #define ADC_ACTIVE_INPUTS 3

     

     

    (in adc_impl.c. recompilation is needed).