Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Z probe for the CNC machine [part 2]
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 6 Mar 2021 4:26 PM Date Created
  • Views 2372 views
  • Likes 2 likes
  • Comments 2 comments
  • arduino based
  • cnc
  • pcb mil
  • digispark
  • pcb milling
Related
Recommended

Z probe for the CNC machine [part 2]

kk99
kk99
6 Mar 2021

image

In this part I focused on creating of the simple script which allows to execute g-code created by Autoleveller application to collect information about thickness of the PCB in different measurement points and use it to generate corrected g-code. The connection with the devices is as at following diagram:

image

The script is written in bash and setups serial connection with CNC machine and Z axis probe. One of connectors of Z axis probe is connected to PCB plate and second to the spindle. Below there is diagram of script flow:

image

At the beginning of script are few basic checks of required arguments and connections (I need add more in final solution). The flow is following:
- setup the custom descriptors for read/write for each device: CNC and Z-probe,

- read one line of source g-code,

- if it is not a z axis leveling command then this line is redirected to CNC machine (In my machine is required to send additional "M105" command to establish and keep connection due the firmware is mainly for 3D printer),

- otherwise is started Z-axis probing procedure which has following steps:
     - read the status of Z-axis probe circuit,
     - if it is open then switch to relative positioning and perform one step down by 0.01 mm in Z axis,

     - if we hit the PCB plate the read the values of positions and switch back to absolute positioning,

     - positions are stored in file and next line of g-code is performed.

 

Here is the source code:

#!/bin/bash

if [ $# -ne 2 ]; then
    echo "Usage: zProbe.sh input.gcode probes.txt"
    exit 1
fi

PROBETTY=`ls -l /dev/serial/by-id/ | grep "Digispark_Serial" | grep -o "tty.*"`
if [ -z "${PROBETTY}" ]; then
    echo "There is no Z axis probe attached."
    exit 1;
fi
exec 4</dev/${PROBETTY} 5>/dev/${PROBETTY}
stty -F /dev/${PROBETTY} 115200 raw -echo

PRINTTTY=`ls -l /dev/serial/by-id/ | grep "1a86_USB2.0-Serial" | grep -o "tty.*"`
if [ -z "${PRINTTTY}" ]; then
    echo "There is no printer attached."
    exit 1;
fi
exec 6</dev/${PRINTTTY} 7>/dev/${PRINTTTY}
stty -F /dev/${PRINTTTY} 115200 raw -echo

sendCommand() {
    local COMMAND="$1"
    local TIMEOUT="$2"
    if [ -z ${TIMEOUT} ]; then
        TIMEOUT=0.4
    fi
    echo "${COMMAND}" >&7
    while read -n 100 -t ${TIMEOUT} VALUE <&6; do
        echo ${VALUE}
    done
    echo "M400" >&7
    while read -n 100 VALUE <&6; do
        echo ${VALUE} | grep -q "ok"
        if [ $? -eq 0 ]; then
            break;
        fi
    done
}

probe_zlevel() {
    echo "P" >&5
    read -n 10 -t 5 VALUE <&4
    if [ "${VALUE}" == "O" ]; then
        sendCommand "G0 Z-0.01" "0.005" > /dev/null
        return 1;
    elif [ "${VALUE}" == "C" ]; then
        return 0;
    else
        echo "ERROR"
        return -1;
    fi
}

sendCommand "M105" > /dev/null
while read line; do
    echo ${line} | grep -q "G31 Z-1 F100"
    if [ $? -eq 0 ]; then
        STATUS=1
        sendCommand "M105" > /dev/null
        sendCommand "G91" > /dev/null
        while [ ${STATUS} -ne 0 ]; do
            probe_zlevel
            STATUS=`echo $?`
            if [ ${STATUS} -eq 0 ]; then
                POSITION=`sendCommand "M114"`
                echo "${POSITION}" | grep -o "X:.* Y:.* Z:.* " >> $2
                sendCommand "G90" > /dev/null
                break
            elif [ ${STATUS} -eq  -1 ]; then
                echo "ERROR"
                sendCommand "G28" > /dev/null
                exit 1
            fi
        done
    else
        sendCommand "${line}" > /dev/null
    fi
done < $1

 

I have performed before few tests without leveling and there were difference in cutting of copper layer. I have created a simple schematic which uses 12 mils width paths.
image

I have used FlatCAM to configure milling with V shape 30 degrees 0.1 mm spindle. The finale g-code is configured to cut with 0.1mm thin.

image

Then I used the Autoleveller to generate g-code for collect the information about the PCB plate.

image

Here is output from Autoleveller with collected probes from my PCB plate.

image

With this information I was able to generate corrected g-code and perform milling. From my initial observations it looks like that I need to spend now more time on finding proper settings e.g. cut depth to get best results. Additionally it will be nice to rewrite this script to other language code e.g. C/C++ with adding more strict checks during performing. Below sample results and video (was speed up 4 times) from probing and milling.

image

image

image

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +1
    Nice implementation. DAB
  • kk99
    kk99 over 5 years ago +1
    Here is one more example of made PCB:
Parents
  • kk99
    kk99 over 5 years ago

    Here is one more example of made PCB:
    image


    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kk99
    kk99 over 5 years ago

    Here is one more example of made PCB:
    image


    imageimage