Browse By Tags

  • Wireless IoT device

    Some time ago Erik created the Digispark, and then went on to create a few more projects. News - Digistump I've backed each of his projects and been more than impressed over the kickstarter and more importantly the support during and even after the kickstarter…
  • Code that will turn off my Iron

    Hello, my mom asked me for a circuit that will turn her iron off when she's not using it and maybe check the water level. I came up with two contacts on the iron "parking" pad and classic BC547 circuit for water level sensing. Now I need to develop the…
  • digispark

    Hello ... my question is about digispark (I think that it's close enought to arduino ) I have trouble installing drivers for digispark on my laptop (Win7 64bit) using this tutorial https://www.youtube.com/watch?v=MmDBvgrYGZs . Everything works until I…
  • Z probe for the CNC machine [part 2]

    In this part I focused on creating of the simple script which allows to execute g-code created by Autoleveller application to collect information about thickness of the PCB in different measurement points and use it to generate corrected g-code. The connection…
  • Z probe for the CNC machine [part 1]

    I few weeks ago I bought convertible 3 in 1 device (DOBOT Mooz-2 Plus) which allow 3D printing, laser engraving and CNC. After initial testing of each module I decided to try the CNC module in PCB engraving. Initial tests showed me that is required precise…
  • A Low Power ATtiny85 System

    For some years I have wanted to create a low powered Arduino compatible system. The Arduinos themselves do not seem to be suited to this as they do not have the low power features implemented into the Arduino IDE. So, after looking around at alternatives…
  • Digispark ATtiny85 Lowest Power : Does Anyone Know?

    In the past I made a very low power LED flasher circuit using a PIC microcontroller that worked continuously for at least two years on the same set of 2 x AA batteries. I retired before the batteries ran out so I never did find it's maximum life span…
  • Minor Details. aka Oops!

    So, it turns out that the cheap Digispark clones do have a slight difference from the real thing - pin p5 is a "reset" pin by default. Imagine my surprise, when the project I was working on starting doing some seriously strange things when I connected…
  • Empty RGB XMAS Tree

    Merry Boxes & LEDs Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme…
  • Intelligent Hall Light

    Open Arduino Enter Your Project for a chance to win a grand prize for the most innovative use of Arduino or a $200 shopping cart! The Birthday Special: Arduino Projects for Arduino Day! Back to The Project14 homepage Project14 Home Monthly Themes Monthly…
  • Edge Lit signs

    Open Arduino Enter Your Project for a chance to win a grand prize for the most innovative use of Arduino or a $200 shopping cart! The Birthday Special: Arduino Projects for Arduino Day! Back to The Project14 homepage Project14 Home Monthly Themes Monthly…
  • Beer Tap

    This is something done as an extra for the Beyond the Phone Design Challenge. For those interested, it was sponsored by Wurth and my conversations with sleuz was the deciding factor to apply. I had heard that someone was rather interested in beer…
  • ATTiny Fuse Resetter

    The other week I was playing with a Digispark clone, and it turns out that the suppliers have not programmed them correctly. Let me explain When Erik created the Digispark, he wanted to use all 6 pins of the ATTiny85 for I/O. Because there is a bootloader…
  • Pokémon Tamagotchi using Digispark - Help needed

    Hello element14 community, i found an old Gameboy Color in my basement with Pokémon Red in it, and since i am looking for a project for quite a while now, i am willing to sacrifice it for the sake of modding. Since my knowledge of electronics is basic…