Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Nouveau projet à temps très partielle...

    Qtroniks
    Qtroniks
    Voila, j'ai toujours la tête pleine d'idées et l'une des idées qui me trotte depuis trop longtemps est la conception d'un animatronique de creature Scy-Fy...Bien sur j'avais jamais commencé quoi que ce soit puisqu'il me manquait des ressources d'info...
    • 30 Nov 2013
  • Micro-MaTch Connectors

    veronicaluijten
    veronicaluijten
    TE Connectivity’s (TE) Micro-MaTch connectors’ spring connection can extend the life of  your device and offer a unique solution for your high vibration applications by preventing fretting corrosion through a spring-design contact. With a center...
    • 28 Nov 2013
  • How to minimize power consumption?

    e14 Contributor
    e14 Contributor
     Current Sensing resistors are designed for low resistance so as to minimize power consumption.  In order to meet the requirements of the market Panasonic offers a wide range of Current Sensing Resistors in many case sizes (0402 to 2512), ...
    • 28 Nov 2013
  • Linux Tip: Easy way to run Internet Explorer

    fustini
    fustini
    I'm a full-time Linux user so sometimes I run into a site that only works with IE.  Here's an easy way to run Internet Explorer in Linux that I found last night: Ask Ubuntu: How to install Internet Explorer (multiple versions)?http://askubu...
    • 27 Nov 2013
  • My First FPGA!

    mraureliusr
    mraureliusr
    So today I picked up my first FPGA! It was a sample that I got from Atmel, the AT40K40AL. I had no idea that the part was selling for about $85 on some electronic parts suppliers websites!!! The problem is, I can't seem to find any tools to writ...
    • 27 Nov 2013
  • HP LCD screen comes back to life.

    knight_rider1977
    knight_rider1977
    My HP dv9000 fell victim to the known motherboard issue.  It also fell victim to the crummy screen mount clutch.  it has been out of commission for close to a year.  While browsing for Raspberry Pi stuff I came across a lvds driver kit...
    • 26 Nov 2013
  • Rasduino - A Raspberry Pi-Arduino robot programmed with Simulink

    anujaapte
    anujaapte
    How can you make a cool Arduino robotics project even cooler - by adding a Raspberry Pi component to it! This is exactly what we did when preparing for our demo booth at Open Hardware Summit in MIT earlier this year. Raspberry Pi is powerful enough t...
    • 23 Nov 2013
  • How I started programming Arduino with Simulink..

    anujaapte
    anujaapte
    Over last few months I have had a lot of fun working on Arduino projects using Simulink. Honestly, I was a bit apprehensive when I started on my first Arduino project. An engineer turned marketer, I had not worked with hardware in over a decade. I ha...
    • 23 Nov 2013
  • Back to work (Or how to finish your coffee and get back to work)

    cookieglitch
    cookieglitch
    So, short(ish) break over after settling into a new job and focussing on some other projects that require decent weather (Don't know about you, but I'm not a fan of trying to do fibreglassing and similar when your work space is <10C, or as my phon...
    • 23 Nov 2013
  • Stepper motor speed 28BYJ-48

    knight_rider1977
    knight_rider1977
    Well after some playing around with some python code I discovered the max speed I can set a delay between pulses in my 28BYJ-48 stepper motor is .002 MS.  That speed yielded an average of 5.25 seconds for a full rotation.  .003 was at 8 sec...
    • 23 Nov 2013
  • Traveling While Engineering: Why You Should Try Freelancing

    e14 Contributor
    e14 Contributor
    If you’ve read my first post on the topic, then you already know that I am an electrical engineer traveling the world with my wife.  One of the things I do to stay relevant as an engineer is freelance work that I find online.  I believe tha...
    • 20 Nov 2013
  • Augmented Reality BreadBoard circuit building guide

    Stuartsjones
    Stuartsjones
    Spotted this on Reddit just now. In prototype stage, but this could be an excellent teaching tool. www.youtube.com/watch
    • 20 Nov 2013
  • FMCC SOL: Get the Maximum Efficiency of Power System

    schurter
    schurter
    SCHURTER today announced an extension of its FMER SOL DC filter portfolio with a series for applications using 3-phase AC.  The new FMCC SOL high-performance filter series is designed for rated currents from 150A to 2500A which are ideal for inc...
    • 19 Nov 2013
  • Exemption will expire

    gnevison
    gnevison
    The exemption for nickel cadmium batteries in Cordless Power Tools (directive 2006/66/EC) will expire on 31 December 2016.  Find out more EU Batteries Directive information. Register with element14 to be able to receive the latest EU B...
    • 18 Nov 2013
  • Keithley 2450 SMU quick accuracy comparison

    robrenz
    robrenz
    I did some quick accuracy testing against my 8846A and it looks pretty impressive.  I am not a Cal. lab so this is the best I can do.8846A was set for 100NPLC and digital filtering.2450 was set for the max 10NPLC and filtering with 10 readings t...
    • 15 Nov 2013
  • Reading in a 0V - 5V Analogue voltage on the PSOC 4 Pioneer board

    e14 Contributor
    e14 Contributor
    This confused me for a bit so if the following helps anyone then great. Here is my circuit diagram.. The problem I was having was assuming that using a single ended ADC input at 12 bits was going to give me 0 for 0V and 4096 for 5V.However ...
    • 15 Nov 2013
  • How to use a Clamp Meter

    e14 Contributor
    e14 Contributor
     There are several cases when current measurement is necessary. In many of these cases it is practically impossible to break an electrical circuit in order to connect a digital multimeter. Another limitation of using a DMM is that common multime...
    • 14 Nov 2013
  • Traveling While Engineering: An Unexpected Journey

    e14 Contributor
    e14 Contributor
    In May 2013, I graduated with an electrical engineering degree and a fascination with microprocessors and embedded system design.  But instead of going to grad school or getting a job as many of my friends did, I took what a lot of people would ...
    • 13 Nov 2013
  • How I Learned Electronics: A trip down engineering memory lane

    tpcipri
    tpcipri
    As an engineer, I am constantly learning new technologies. Hardly a day goes by where I haven’t learned some new technology or aspect of a technology. In the early 70s when cutting my teeth on electronics, integrated solid state electronics was just ...
    • 11 Nov 2013
  • NF4EB Relay alternative

    e14 Contributor
    e14 Contributor
    The Panasonic / Matsushita NF4EB relays became obsolete at the end of 2012, Cephos now manufactures a replacement relay module - Cephos C-NF4EB. Available in 5, 12 and 24V versions this module has the same dimensions and pinning as the original ...
    • 7 Nov 2013
  • Panasonic offers highly interesting MELF Replacement Solutions

    e14 Contributor
    e14 Contributor
    Currently, the market trend goes from MELF type Resistors to SMD Resistors for several reasons. These reasons are cost reduction, optimization of mounting speed, simplification of mounting equipment (no nuzzle needed) and better solder joint reliabil...
    • 4 Nov 2013
  • c++ coding

    e14 Contributor
    e14 Contributor
    i am writing a c++ code for windows to interact with arduino on com7. i have the code for arduino to take data from com 7. but having difficulty for finding command of c++ for transmitting data on com7. help plz
    • 3 Nov 2013
  • An instant success... Sorta

    funinalaska
    funinalaska
    So this evening on a whim I decided I wanted to try my hand at networking my arduino.So i searched the web for something easy to try my brand spanking new Ethernet Shield with.I ran across this:https://arduino-info.wikispaces.com/ethernet-temp-humidi...
    • 2 Nov 2013
  • Recent Awesome Engineering Podcast Episodes

    fustini
    fustini
    The Amp Hour #169 – An Interview with Vincent Himpe – Escaped Electron Elocutionhttp://www.theamphour.com/169-an-interview-with-vincent-himpe-escaped-electron-elocution/ Hosts Chris Gammell and The specified item was not found. interview Vincent Himp...
    • 1 Nov 2013
  • NEW Tiva C Series TM4C129x MCUs

    e14 Contributor
    e14 Contributor
    Blaze your trail onto the Internet of Things. Check out our new Tiva C Series TM4C129x MCUs, industry’s first ARM Cortex-M4 with Ethernet MAC+PHY, which serves as your gateway to the cloud! http://bit.ly/1bFh3LG
    • 31 Oct 2013
<>