Personal Blogs
  • Community Hub
  • More
Personal Blogs
Douglas Wong's Blog CHIP Computer - they are shipping
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 14 Feb 2016 10:10 AM Date Created
  • Views 1315 views
  • Likes 4 likes
  • Comments 11 comments
Related
Recommended

CHIP Computer - they are shipping

dougw
dougw
14 Feb 2016

This is a quick unboxing and power up of a $9 CHIP computer in case anyone had doubts about the Kickstarter promises....

For some reason I cannot insert a video in a blog since the site upgrade, so you will have to follow this link:

CHIP Computer is Shipping

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago +1
    dougw Thank you for unboxing video. Other than play, do you have project(s) in mind? Can you provide link for vga display? Thanks in advance, Clem
  • clem57
    clem57 over 10 years ago +1
    dougw I was considering the CHIP computer until I realized: They are only providing VGA support at $9. The upcharge for HDMI was about $15. They charged $5 for each computer ordered. Really? The ram is…
  • dougw
    dougw over 10 years ago in reply to clem57 +1
    The Pine looks like a great little computer and there are other interesting modules out there as well. I was looking for the absolute lowest cost way to get a full color VGA display, including LCD. I was…
Parents
  • clem57
    clem57 over 10 years ago

    dougw

         Thank you for unboxing video. Other than play, do you have project(s) in mind? Can you provide link for vga display?

    Thanks in advance,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to clem57

    This little computer has a lot of built-in features and computing power in a tiny form factor, including WiFi and Bluetooth. This makes it a great platform for high performance mobile or wearable devices or small embedded applications, and the hardware is open source. One of the reasons I bought the small display is in anticipation of mobile applications. I don't have specific projects in the works yet - still getting familiar with features and programming environment.

    I got the display on ebay - it is a 5" 800x480 rear-view display for vehicles. There are many to choose from in the $17 range, just make sure to check the resolution. I use a $2 DC-DC module to boost USB voltage to 12 volts for the display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 10 years ago in reply to clem57

    This little computer has a lot of built-in features and computing power in a tiny form factor, including WiFi and Bluetooth. This makes it a great platform for high performance mobile or wearable devices or small embedded applications, and the hardware is open source. One of the reasons I bought the small display is in anticipation of mobile applications. I don't have specific projects in the works yet - still getting familiar with features and programming environment.

    I got the display on ebay - it is a 5" 800x480 rear-view display for vehicles. There are many to choose from in the $17 range, just make sure to check the resolution. I use a $2 DC-DC module to boost USB voltage to 12 volts for the display.