Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog AIS Alarm - PCB Version 0.2
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 7 Feb 2018 4:24 AM Date Created
  • Views 1694 views
  • Likes 9 likes
  • Comments 9 comments
  • daisy
  • smd
  • ais
  • state machine
  • pcb
  • msp430
Related
Recommended

AIS Alarm - PCB Version 0.2

fmilburn
fmilburn
7 Feb 2018

Project Objective: Develop an open source AIS Alarm that alerts sailors that a new marine vessel with AIS is within range

 

Over the weekend I modified the PCB design, submitted it for production, and started thinking about refactoring the firmware.  This post will show the new PCB design and outline some of the thinking that went into it.  A first pass at the state machine will also be introduced.

 

Here is a rendering of the new PCB that is now being manufactured:

image

The main changes are:

  • Removed the LED that was causing interferences with the side of the case completely.  I decided I could convey necessary information with blinks of different length rather than multiple LEDs - remains to be seen how well that will work.  Reduces BOM and cost.  I considered using SMD LEDs very seriously but in the end settled for the 5mm one used here because I wanted maximum brightness.
  • Moved the dAISy on the alarm board directly over the header on the radio.  Bought some short "Dupont" 0.1" headers and will try to connect the two boards that way rather than use ribbon cable.  Will tidy things up and make assembly easier but is a tight fit.  Somewhat more costly since they are non-standard headers.  This is something of an offshoot of the idea Gene suggested in my last post.
  • Moved the buzzer forward to remove interference and placed the programming header behind it.  The microcontroller is now closer to the radio which is undesirable.  Need to check if this materially reduces reception from the radio when the PCB comes back.

 

This is the simplified state machine both as a diagram and a table showing movement from one state to the next.  In the old design there were LEDs for on/off, alarm, and ship detected.  Now it is done with one LED.  This is probably close but I have to keep stopping myself from adding features (KISS).

image

image

The V0.2 board should be back by the end of next week.

 

I found someone who is willing to test it and give feedback when I am comfortable with the prototype.  It is a person who has sailed the Pacific on a small boat and is interested in looking at it.

 

Past Posts from this Project:

AIS Alarm

AIS Alarm - The Process

AIS Alarm - Prototype Hardware

AIS Alarm - Timers and GPIO

AIS Alarm - Prototype Code Outline

AIS Alarm - UART

AIS Alarm - First AIS Messages

AIS Alarm - First FRAM Storage

AIS Alarm - Debouncing Momentary Button Switches

AIS Alarm - FRAM Ring Buffer

AIS Alarm - Schematic

AIS Alarm - PCB Version 0.1

AIS Alarm - PCB Version 0.1 Arrived

 

References and Links:

WEGMATT LLC - dAISy AIS Receiver - low cost AIS receiver

Texas Instruments MSP430FR2xx FRAM Microcontrollers - Post No. 4

TI MSP430FR2111

Maximize the Sound from a Buzzer

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago in reply to gecoz +4
    Hi Fabio, Thanks for examining my work critically - it is appreciated. You have found an omission in the state diagram. Also, I am a self taught enthusiast programmer so my work may not reflect standard…
  • shabaz
    shabaz over 8 years ago +3
    Hi Frank, Nice-looking board design! the entire project is looking really great. As for the board changes, I felt your pain, I too am currently battling with an enclosure, there is never enough room :…
  • gecoz
    gecoz over 8 years ago +2
    Hi Frank, I like this new version of the board, looks very neat. It is great you already found someone willing to test your prototype, I always find on-the-field testing one of the hardest part to cover…
Parents
  • genebren
    genebren over 8 years ago

    Frank,

     

    Looking good!  I could not tell, but it looks like you did not change the footprint on the dual-MOSFETs.  Were you unable to find a different package, or did you just decide to go with what you had?  The state machine design looks good.  On your 'Off' state, are you doing any power saving or sleep modes?

     

    Good luck on your continuing progress on your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Frank,

     

    Looking good!  I could not tell, but it looks like you did not change the footprint on the dual-MOSFETs.  Were you unable to find a different package, or did you just decide to go with what you had?  The state machine design looks good.  On your 'Off' state, are you doing any power saving or sleep modes?

     

    Good luck on your continuing progress on your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 8 years ago in reply to genebren

    Thanks Gene,

    I decided after another trial that I can hand solder these OK.  I modified the footprint on the dual MOSFET a bit - just lengthened the pads although it is hard to tell from the rendering.  But now that you mention it I could lengthen them some more.  I plan to order a template next time and get myself a toaster oven.

     

    Regarding the OFF state - yes, I will use one of the power saving states on the MSP430 that can wake up with a button press.  It is not too critical though as I don't plan to turn off the radio when the alarm is off and the radio is the main power user.  The reason for not turning off the radio is that in an area with heavy traffic the user will want to leave AIS on and monitor on the screen but not hear the alarm continuously beeping.  Kind of like listening to your favorite station on the radio and not hearing the alarm at the same time :-).