Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 3 Oct 2018 6:27 AM Date Created
  • Views 7645 views
  • Likes 9 likes
  • Comments 51 comments
  • current source
  • milliohm measurement
  • op amps
Related
Recommended

Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

fmilburn
fmilburn
3 Oct 2018

Introduction

This is the third post on the development of an inexpensive but reasonably accurate meter for measuring resistance in the milliohm range. In the first post a simple current source was described that created a 10 mA current  across a resistor that allowed the voltage drop to be measured using a multimeter and the resistance calculated.  A number of helpful suggestions were received and I ordered additional components based on that feedback.  In the second post a block diagram for the instrument was introduced and initial measurements were made with a microcontroller using the built-in ADC.  Some, but not all of the ordered parts have been received now and this post will update progress as I don't want John's popcorn to get stale.

 

A Change to the Design Objectives

I originally specified that the current to the DUT would not be greater than 10 mA.  Testing to date has indicated that meeting the desired accuracy will be difficult without amplification of the voltage difference across the DUT which adds some complexity and cost.  Accordingly, the specification is being changed to 100 mA across the DUT.

 

Component Status

First, I have to admit to making a mistake in the orders.  The MCP6N16 instrument amp comes in three versions with different minimum gain.  I wanted the version with minimum gain of 1 and ordered the version that has a minimum gain of 100.  Doh!  Always read the datasheet carefully.  For now I am substituting the MAX9619.  I also ordered a precision LDO voltage source from the TI store which has not been shipped yet.  Usually they are pretty quick. The volt meter I plan to use is still in shipment from China.

 

100 mA Current Source

This is the revised circuit, the only real changes being the addition of a MOSFET to handle the increased current and a new precision 0.1% 10 ohm resistor to set the current.  I am using an inexpensive ANENG multimeter to measure voltage but it does agree well with my bench meter.

image

And here are the results:

image

The tests are being performed the same way as previously using a coil of wire that has been center tapped.  The measured resistance of the full length of wire is 0.092 ohms as seen on top while the measured resistance of half the length is 0.046 ohms - exactly half.

 

Next Steps

The inexpensive voltmeter needs at least 4.5 V to operate so I will probably use either 4 x 1.5 V AAA batteries or USB power and a precision voltage source to set the current.  If I decide to use a microcontroller instead of a voltmeter then a 3V3 LDO will be used to power that.  The parts for Kelvin probes are on order.  Progress depends on the postal service now...

 

Past Posts on this Topic

More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Testing Current Sources for a Kelvin (4-Wire) Milliohm Meter

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Hi Shabaz, An update... I read the datasheet thoroughly and set up the LM334 as a temperature compensated current source as described in the datasheet. A IN4148 was substituted for the diode they used…
  • shabaz
    shabaz over 7 years ago in reply to fmilburn +5
    Hi Frank, That's very interesting! Is it figure 15 in the datasheet? There is a modification suggested here: https://www.electronicdesign.com/analog/what-s-all-lm334-stuff-anyhow that looks like it could…
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Shabaz,, Yes, using the circuit in Figure 15 with 1% resistors and the diode noted above. I am at the limit of the resolution of my multimeter and there was some bouncing back and forth so am not sure…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Frank!

     

    I'm wondering if it is possible to use a dual-stage design, i.e. separate the current source from the final signal output stage, i.e. use an op-amp for the voltage amplification across the load, but perhaps with a lower-current source, since 100mA might make it more difficult, because the reference resistor will get warm and maybe drift. That op-amp you mention (in a min gain of 10 version) could also be used for the second stage.

     

    Any of the current source ideas could be used for the first stage, but I think the LM334 would be attractive (but means your first stage would not be an op-amp, so depends if this is a hard limitation or not : ) because the power in the resistor is really small (since the internal reference inside it is 68mV), i.e. if a 6.8ohm resistor is used, power dissipated in the resistor is 0.68mW.  Then for the desired 1mohm to 10 ohm range, if the meter is 0-2V (as an example) then a gain of 20 is needed (i.e. compatible with the min. gain of 10 version). Or for an op-amp version, it could be the same as the circuit you have now of course (with the reference resistor value changed). These are just some ideas, maybe unnecessary if the resistor won't drift much (or if you find in the end that less than 100mA is fine too, for the particular multimeter you use).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    An update... I read the datasheet thoroughly and set up the LM334 as a temperature compensated current source as described in the datasheet.  A IN4148 was substituted for the diode they used.  I came up with nonstandard resistor values so I put the closest values I had in.  The initial test was about 2% off the desired 10 mA current (not unexpected based on what was in the datasheet) so R1 was adjusted by adding another resistor in parallel until within 1%.  Voltage was varied over the range of interest and here are the results for the full length of test wire:

    image

    Things look good above 2.5V input (the planned instrument will have at least 3V) but notice there is a slight rise in the measured current at 5V.  This may be due to temperature from increased voltage which the datasheet warns of or just increase of temperature as it heats up in time in still air.  I left it on for an hour at 5V and from that point on it was stable although I am unable to make measurements with the resolution I would like.

     

    I added another tap in my test wire at quarter length.  The results are:

    Full Length:  0.092 Ohms

    Half Length: 0.045 Ohms

    Qtr Length:  0.022 Ohms

     

    The accuracy appears to fall off as it nears the bottom of the multimeter range but all is as expected.  I will look into adding amplification next.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    OK thanks - it is getting late :-)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to shabaz

    This is a really good experiment you've done here. I'd vote for you to have your transistor badge for this!

     

    Perhaps you might consider doing it as a separate blog as well (would make it easier for people to bookmark and find again).

     

    If you had asked me what I thought the coefficient was, I'd have said -2.5mV/K. That comes from me learning electronics theory back in the 1970s and never having done serious transistor-level analogue design later on (where, presumably, I would have discovered the difference myself). I've looked in a few old books from that period and several just quote variations of "approximately -2.5mV/K" (one doesn't even mention that it goes off at higher emitter currents).

     

    That figure wasn't wrong back then. One of the books I looked at was published by TI, back when they made transistors, and the author was a real expert on everything to do with the devices.

     

    From what I can make out the theoretical value (for silicon) should be -1.7mv/K but a real transistor doesn't match the simple model that comes from.

    There have been a couple of major changes in the way transistors get made since the 1960s that may account for the change [gold doping to improve recombination and planar construction to allow the use of IC fabrication techniques].

     

    From what you've shown us here, "approximately 2mV/K" would be a better rule of thumb now.

     

    The coefficient moves off towards zero at higher emitter currents (since we're talking about the Vbe, we probably should refer to the emitter current rather than the collector) because of the ohmic properties of the base and emitter (which have a positive coefficient).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jc2048

    Hi Jon!

    Hehe the day off was hopefully productive then : ) I started some DIY, but it was more interesting to do the experiment : )

    That's a good idea, I'll put together a separate blog with the tempco details.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hi Frank,

     

    Sorry I missed mentioning, that's a great idea to have the trim capability. You're right, the '334 possibly isn't the best approach if there will be different current settings : ( That could get very awkward. One possible option is to have a separate circuit per setting (since the '334 is cheap) but that could get tiresome quickly : ) especially if there are many settings, so some other current source method may be preferable for that.

    I tried these settings today, although the test is still running. It's very sensitive to air currents cooling different parts at different speeds perhaps, so I put it on soft packaging foam and a bowl on top to try to seal it up..

    image

    The two resistors are on the proto board:

    image

    They're basically many parallel SMD resistors to get to the values needed. I'm using these settings currently:

    image

    This is the results so far, just running at 5V since the it seems fairly insensitive to reasonable voltage changes. Apologies for poor snapshots from mobile phone:

    image

    So, it shifted about 7uA from the start, but it did stabilise and reach some equilibrium, but it took 16 minutes to get there, and after that it's been sitting at 10.1408mA and unchanging. This is at about 23.8 deg C room temperature (I'm not measuring inside the bowl but outside). I don't know yet what shift there will be when the room temperature changes!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi Shabaz,

    That looks really good and well within the requirements I set out.  I see the measured current is pretty close to the desired current in your spreadsheet.  What are the actual values you are using for R1 and R2?  Also, I am curious about the instrument you are recording the data with.  I am about to start testing again, this time using the 2N3904 as the diode.  My work area is pretty drafty, I may need to cover things up as well.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi Shabaz,

    That looks really good and well within the requirements I set out.  I see the measured current is pretty close to the desired current in your spreadsheet.  What are the actual values you are using for R1 and R2?  Also, I am curious about the instrument you are recording the data with.  I am about to start testing again, this time using the 2N3904 as the diode.  My work area is pretty drafty, I may need to cover things up as well.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hi Frank,

    I'm using:

    R1: three 51 ohm resistors in parallel (this should provide 17.0 ohms)

    R2: four resistors in parallel: 18.2k, 220R, 549R, 549R  (this should give 121.3 ohms)

     

    17.0 and 121.3 are a few tens of mohm lower than the Excel worksheet result, since the breadboard contacts will add a bit.

    I switched on the heating (and have been sitting in 25.2 degrees C - really hot!!) and from what I've seen, I don't believe the drift is any more than 80ppm/degC and might even be half of that. I can't be precise, because the bowl is Pyrex (i.e. heat insulator) so I lifted it for about 5 minutes in the now warmed room (and the readings shot up due to imbalances - so you'll probably find the same thing, that covering it is necessary!) and then put the bowl back on, and the value dropped to slightly lower than the 10.1408mA that I'd recorded at equilibrium before. It is still settling, but the room temperature is changing because I had to turn the heating off, I can't bear 25.2 degrees C any more image

     

    From all that, my best guesstimate is -30 to -80ppm/degC change (i.e. current dropped by about 0.3uA to 0.8uA with 1 degree C increase in temperature), and I believe that is going to be mainly from the resistors, since they were either 100ppm/degC or 50ppm/degC resistors (they were in my box of spare resistors, and I only checked that I picked 1% ones, I didn't look up the ppm).

    They were all normal thick film resistors since this was all I had. All were 0603 sized except the 220R resistor happened to be 0805 sized.

    So, if it gets a reasonably stable supply (a change of -100mV, i.e. down to 4.9V from the 5V that I was testing at, causes a drop of about 0.3uA) then I'm hoping it is definitely stable enough for milliohm measurements, but will be reassured by your findings, in case I made some mistake.

     

    I'm using a new Keithley DMM6500, which I chose for the Bluetooth Unleashed competition. I will write a review of it when I've used it more, right now I really don't know what it does, but the logging is extremely useful, and it looks packed with functionality. I have a very old Keithley model 2015, which I was worried would fail any day, since it is way beyond normal service life by a decade : ), and uncalibrated.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    HI Shabaz,

    That is really good information and I am quite encouraged.  I did not make as much progress as you today but will write it up.  My instruments are not as good as yours so I am thinking about how best to get a read on temperature influence.  When I borrow the Keithley from my friend next week that will help.  I need to start working on amplification as well since I'd like to design a PCB and get it off to a Chinese prototype house next week.

    • Cancel
    • Vote Up +4 Vote Down