Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 3 Oct 2018 6:27 AM Date Created
  • Views 7654 views
  • Likes 9 likes
  • Comments 51 comments
  • current source
  • milliohm measurement
  • op amps
Related
Recommended

Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

fmilburn
fmilburn
3 Oct 2018

Introduction

This is the third post on the development of an inexpensive but reasonably accurate meter for measuring resistance in the milliohm range. In the first post a simple current source was described that created a 10 mA current  across a resistor that allowed the voltage drop to be measured using a multimeter and the resistance calculated.  A number of helpful suggestions were received and I ordered additional components based on that feedback.  In the second post a block diagram for the instrument was introduced and initial measurements were made with a microcontroller using the built-in ADC.  Some, but not all of the ordered parts have been received now and this post will update progress as I don't want John's popcorn to get stale.

 

A Change to the Design Objectives

I originally specified that the current to the DUT would not be greater than 10 mA.  Testing to date has indicated that meeting the desired accuracy will be difficult without amplification of the voltage difference across the DUT which adds some complexity and cost.  Accordingly, the specification is being changed to 100 mA across the DUT.

 

Component Status

First, I have to admit to making a mistake in the orders.  The MCP6N16 instrument amp comes in three versions with different minimum gain.  I wanted the version with minimum gain of 1 and ordered the version that has a minimum gain of 100.  Doh!  Always read the datasheet carefully.  For now I am substituting the MAX9619.  I also ordered a precision LDO voltage source from the TI store which has not been shipped yet.  Usually they are pretty quick. The volt meter I plan to use is still in shipment from China.

 

100 mA Current Source

This is the revised circuit, the only real changes being the addition of a MOSFET to handle the increased current and a new precision 0.1% 10 ohm resistor to set the current.  I am using an inexpensive ANENG multimeter to measure voltage but it does agree well with my bench meter.

image

And here are the results:

image

The tests are being performed the same way as previously using a coil of wire that has been center tapped.  The measured resistance of the full length of wire is 0.092 ohms as seen on top while the measured resistance of half the length is 0.046 ohms - exactly half.

 

Next Steps

The inexpensive voltmeter needs at least 4.5 V to operate so I will probably use either 4 x 1.5 V AAA batteries or USB power and a precision voltage source to set the current.  If I decide to use a microcontroller instead of a voltmeter then a 3V3 LDO will be used to power that.  The parts for Kelvin probes are on order.  Progress depends on the postal service now...

 

Past Posts on this Topic

More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Testing Current Sources for a Kelvin (4-Wire) Milliohm Meter

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Hi Shabaz, An update... I read the datasheet thoroughly and set up the LM334 as a temperature compensated current source as described in the datasheet. A IN4148 was substituted for the diode they used…
  • shabaz
    shabaz over 7 years ago in reply to fmilburn +5
    Hi Frank, That's very interesting! Is it figure 15 in the datasheet? There is a modification suggested here: https://www.electronicdesign.com/analog/what-s-all-lm334-stuff-anyhow that looks like it could…
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Shabaz,, Yes, using the circuit in Figure 15 with 1% resistors and the diode noted above. I am at the limit of the resolution of my multimeter and there was some bouncing back and forth so am not sure…
  • jc2048
    jc2048 over 7 years ago in reply to shabaz

    This is a really good experiment you've done here. I'd vote for you to have your transistor badge for this!

     

    Perhaps you might consider doing it as a separate blog as well (would make it easier for people to bookmark and find again).

     

    If you had asked me what I thought the coefficient was, I'd have said -2.5mV/K. That comes from me learning electronics theory back in the 1970s and never having done serious transistor-level analogue design later on (where, presumably, I would have discovered the difference myself). I've looked in a few old books from that period and several just quote variations of "approximately -2.5mV/K" (one doesn't even mention that it goes off at higher emitter currents).

     

    That figure wasn't wrong back then. One of the books I looked at was published by TI, back when they made transistors, and the author was a real expert on everything to do with the devices.

     

    From what I can make out the theoretical value (for silicon) should be -1.7mv/K but a real transistor doesn't match the simple model that comes from.

    There have been a couple of major changes in the way transistors get made since the 1960s that may account for the change [gold doping to improve recombination and planar construction to allow the use of IC fabrication techniques].

     

    From what you've shown us here, "approximately 2mV/K" would be a better rule of thumb now.

     

    The coefficient moves off towards zero at higher emitter currents (since we're talking about the Vbe, we probably should refer to the emitter current rather than the collector) because of the ohmic properties of the base and emitter (which have a positive coefficient).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    OK thanks - it is getting late :-)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hehe we thought alike. I too wrote a spreadsheet : ) Still, I'm glad we can compare now, because mine had an error, but I've just now corrected it after seeing and testing with the values in your screenshot : )

    image

    The settings I've put in there are the current ones I'm playing with (I chose a tempco and Vf that would hopefully be close enough for either manufacturer 2N3904. I'll locate some resistors and start paralleling them tomorrow, to get as close as I can to these figures.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hi! The TI chart rises as does the data in the table, I think maybe the chart I drew may be confusing things, it was just showing Vf (not tempco) just so we could see how the selected Vf would also change depending on what current setting was used.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    One final post for the night...  I put the numbers into the spreadsheet for the IN4148 - Here is the resulting calculation:

    image

    For R1 I am still using 17.4 Ohms so that is off a bit.  For R2 I took out the 33 Ohm resistor and replaced it with a 100 Ohm trim pot as the datasheet says to vary R2.  Then I fired up the circuit and adjusted R2 until the current was measuring exactly 10.00 mA.  The measured resistance for R2 was 130.5 Ohms and above it was 134 Ohms.  So a 3.5% change in resistance was needed to correct a 1.7% original error in current.  My feeling is that a trim pot is needed to insure better than 1% accuracy.  I am using a cheap trim pot but it seemed fairly stable.  The Newark site is down for me but it looks like you can get a single turn 50 ohm version with 100 ppm / deg C temperature coefficient for less than a dollar which I think would be acceptable.

     

    An observation on flexibility:  With the LM334  it would be difficult to change current settings to measure larger resistors.  It would be more straight forward to switch sensing resistors with a microcontroller if using the op amp approach.

     

    I spoke to my friend today who has all the nice equipment.  He is going to let me borrow his Keithley current meter.  At least it will look good in the pictures :-)

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>