Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Programmable DC Electronic Load - First Look
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 14 Jun 2019 6:56 AM Date Created
  • Views 5355 views
  • Likes 16 likes
  • Comments 20 comments
  • programmable load
  • arduino
  • dc_load
Related
Recommended

Programmable DC Electronic Load - First Look

fmilburn
fmilburn
14 Jun 2019

9 August 19 Update: 

8 July 19 Update:  A protoboard was populated for further testing and described at the bottom of the post

 

I have wanted to build a programmable DC load for some time and have followed both this one by Jan Cumps et. al. and also this one by John Wiltrout.  After lots of thought and no action I decided yesterday to just build something with what was on hand. 

 

Specifications

 

  • Max 15V input and 2.5 Amps
  • Min 1.8V and 0 Amps
  • Resolution 1 mA
  • Deliver 10 mA +/- 1 mA
  • 5V or USB to power
  • User interface:  encoder, buttons, and LCD
  • Simple to build, probably will not have a PCB made
  • Arduino IDE to make it accessible to others

 

Concept Demonstration

 

What was on hand is shown in the following schematic:

image

An Arduino MKR1000 output a voltage using the built-in 10 bit DAC which through an OPA192 op amp and MTP305VL MOSFET control the voltage above the 1 ohm resistor.  One volt output from the MKR1000 equals one amp to the device under test.  In this case the DUT is a 18650 battery hooked up to a boost converter to give roughly 3 Volts.

 

I was surprised at how good the DAC was on the MKR1000.  The MKR1000 ADC had an offset of around 18 mV.  Not shown on the schematic above are digital multimeters measuring the input voltage from the DUT, the output voltage from the DAC, and the voltage across the 1 ohm resistor.  Tests were run at 10 mA, 50 mA, 100 mA, and 1000 mA where it was discovered that the voltage output of the DUT was dropping quickly.

 

Arduino Code

 

[code]
/*
 * Fixed Value Test of DC Electronic Load
 * Tested on MKR1000
 * Frank Milburn
 * June 2019
 * 
 * Released into Public Domain
 * 
*/
const int DAC_PIN = DAC0;     // output to opamp
const int VOLT_PIN = A1;      // input from DUT
const int CURRENT_PIN = A2;   // input from current setting resistor
const int CURRENT = 1000;       // current in mV   WARNING!!! do not set above 3300!!!
void setup() {
  Serial.begin(115200);
  analogWriteResolution(10);
  analogReadResolution(12);
  pinMode(VOLT_PIN, INPUT);
  pinMode(CURRENT_PIN, INPUT);
}
void loop() {
  
  unsigned int dacValue = 0;
  dacValue = map(CURRENT, 0, 3267, 0, 1023);
  analogWrite(DAC_PIN, dacValue);
  Serial.print("Current setting = ");
  Serial.print(CURRENT);
  Serial.println(" mA");
  
  unsigned int inputVoltage;
  inputVoltage = map(analogRead(VOLT_PIN), 0, 4095, 0, 3267);
  Serial.print("Voltage input =   ");
  Serial.print(inputVoltage);
  Serial.println(" mV");
  
  unsigned int currentReading;
  currentReading = map(analogRead(CURRENT_PIN), 0, 4095, 0, 3267);
  Serial.print("Raw = ");
  Serial.print(analogRead(CURRENT_PIN));
  Serial.print("  Current reading =   ");
  Serial.print(currentReading);
  Serial.println(" mV (mA)")
;
  delay(5000);
}
[/code]

 

Results

 

 

10 mA

image

DAC output: 10.9 mA

DUT voltage: 3.295 V

Current: 11 mA

Error: 1 mA

 

50 mA

image

DAC output: 49.1 mV

DUT voltage: 3.289 V

Current: 49.1 mA

Error: 0.9 mA

 

100 mA

image

DAC output: 99.8 mV

DUT voltage: 3.271 V

Current: 99.1 mA

Error: 0.9 mA

 

1000 mA

image

DAC output: 997.5 mV

DUT voltage: 2.89 V

Current: 997.2 mA

Error: 2.8 mA

 

Next Revision

 

Although the full range was not tested, this was a promising beginning especially since there was no tuning.  Here are a couple of areas to work on for the next iteration:

  • 12 bit or more DAC (this one gives ~ 3 mA resolution)
  • move ADC off board
  • Precision resistor (0.98 ohm 3 watt of unknown tempco was used)
  • Replace MTP3055VLMTP3055VL with a more modern part
  • Add overcurrent and reverse polarity protection
  • Add user interface
  • Add heat sinks / cooling fan

 

image

 

8 July 19 Update

 

I soldered a little protoboard to play with before deciding what to do next.  The idea was to make something more reliable mechanically and allow some thermal testing and firmware development.  The design still uses the DAC on the Arduino MKR1000 , OPA192 op amp and the MTP3055VLMTP3055VL MOSFET.  The one ohm resistor was picked up cheap locally and measures 1.003 ohms using the milliohm meter.

image

Female headers were soldered in so that the parts can be easily removed and reused in future.

image

Here it is populated.

image

If you have a 3D printer, then you have to print stuff.  Here it is in a little tray.

image

After fixing a wiring mistake where I confused pin 5 on the op amp with pin 5 on the carrier board (pin 5 on the op amp leads to pin 6 on the carrier) everything was working.  There seems to be an intermittent bad connection between 5V on the MKR1000 and the op amp - one of the main reasons the board was constructed was to avoid this!.  The DAC is accurate in the range tested so far as is A1 which measures the input voltage.  A2 which measures the voltage (and thus current) just above the resistor has about 17 mV offset which seems high but I should consult the datasheet to see if it is in spec.  It can be corrected in firmware.

 

Next Revision

 

It may be a while before I get back to this which is why this interim step is being documented.  Thoughts for the next revision...

 

  • Design a PCB to improve mechanical connections, provide a ground plane, and reduce unwanted capacitance
  • 12 bit or more DAC (MKR1000 has ~ 3 mA resolution with 3A design)
  • move ADC off board (more accuracy, less offset)
  • Precision resistor or at least experiment with tempco of resistor on prototype.
  • Replace MTP3055VLMTP3055VL with a more modern part
  • Add overcurrent and reverse polarity protection
  • Add user interface
  • Add heat sinks / cooling fan
  • Use new Keysight scope with signal generator to investigate issues outlined by Michael Kellett in comments

 

8 Jul 2019:  update progress

9 Jul 2019:  corrected some typos

 

Links

Programmable DC Electronic Load - Follow-up  A follow-up to this post

https://www.element14.com/community/docs/DOC-83867/l/programmable-electronic-load

https://www.element14.com/community/people/jw0752/blog/2018/10/08/a-simple-dc-electronic-load-episode-ii

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 7 years ago +9
    I expect that with some settings and loads your current sink will oscillate. You'll be able to mitigate this with the following changes: about 47R between op amp output and MOSFET gate 4k7 MOSFET source…
  • Andrew J
    Andrew J over 7 years ago +6
    I shall follow this with interest. A DC Load is going to be my next project.
  • fmilburn
    fmilburn over 7 years ago in reply to michaelkellett +4
    Thanks Michael, It sounds like the issues and approach to resolution will be similar to the milliamp meter. I have not constructed a spice model yet but plan to do so. Frank
  • fmilburn
    fmilburn over 6 years ago

    There is an interesting discussion on Hackaday about how Arduino code for reading ADC is incorrect for the SAMD21 which is the microcontroller used in the MKR1000.  Basically it attempts to read the ADC before it is finished and ready.  This may be part of the problem encountered above but I have not investigated it yet.  The Feather M4 uses the SAMD51 and I haven't looked into whether it suffers from the same problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn

    Well, the good news is that the problem is fixable. I've not used pluggable breadboard for a very long time -  so I'm all for soldering.

     

    Good luck.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to michaelkellett

    Feeling like a dull boy... New trials were set up using the microcontroller's internal reference source and capacitance on the input voltage at 66 mV separately and together with slight advantage to adding capacitance.  Then the original setup at 66 mV with no capacitance and the analog reference set to the "default" to try and replicate yesterday's results was set up and almost identical good results were obtained.  In other words, I cannot replicate yesterday's noisy results.

     

    Default analog reference, Capacitance added

    Raw Avg:  90.0

    Raw Median: 90

    Std Dev: 0.9

     

    Internal 2V23 analog reference, no capacitance

    Raw Avg: 90

    Raw Median: 90.0

    Std Dev: 1.3

     

    Internal 2V23 analog reference, with capacitance

    Raw Avg: 90.1

    Raw Median: 90

    Std Dev: 1.0

     

    Repeat original test, Default analog reference, no capacitance

    Raw Avg:  90.3

    Median: 90

    Std Dev: 1.3 (yesterday was 11.5)

     

    Looking back at the photo taken above the differences in the setup are limited to moving the resistor divider to fit the capacitors but something in the original tests gave noisy results at low input voltages that no longer seems to be there.   I am going to move off of the breadboard, solder something up, and repeat the experiments with care over the weekend.  The DAC also needs to be tested for noise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    I think you are right that the internal reference may give better results and have that on my list of things to explore.  I used the Adafruit SAMD51 board as opposed to MKR1000 in these latest experiments because it has a 12 bit DAC and I want 1 mA precision.  I ran the functions listed in the Arduino reference for Arduino SAMD boards, e.g. MKR1000, through the compiler for the Adafruit Feather Express SAMD51 and it appears to support the following for analog references to the ADC:

     

    •   analogReference(AR_DEFAULT);  // This is what I am currently using and is shared with VDD
    •   // analogReference(AR_INTERNAL);   // Not supported on Feather M4 Express
    •   analogReference(AR_INTERNAL1V0);   // Internal 1.0 V reference
    •   analogReference(AR_INTERNAL1V65);  // Internal 1.65 V reference
    •   analogReference(AR_INTERNAL2V23);  // Internal 2.23 V reference
    •   analogReference(AR_EXTERNAL);      // External reference applied to AREF pin

     

    I may have to revert to direct register writes to the microcontroller to get the control necessary which is what I normally do with the TI MSP430 and MSP432 microcontrollers.  I have been using the Arduino IDE because I am not really familiar with Atmel SAMD microcontrollers and wanted to keep things simple.  That is a good idea until it isn't :-).

     

    Edit:  see new comment to Michael above

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to fmilburn

    Does the ADC reference readings agains an internal reference source?  What about the MKR1000?  It's not possible from the code to see how the analog reads are being taken, and this may be a bit of a tangent/red herring, but I found that using the Arduino internal reference source improved accuracy significantly.  Is it possible for you to look at the library code and tell?  If the analogRead is the standard Arduino library code then it may benefit from something like this:

     

    /*
     * Obtain the actual Vcc value of the 4Duino from an internal reference source.
     * The nominal 5V Vin can fluctuate a lot and affect analog read accuracy.
     */
    long readVCC() {
      long result;
      // Read 1.1V reference against AVcc
      ADMUX = _BV(REFS0) | _BV(MUX4) | _BV(MUX3) | _BV(MUX2) | _BV(MUX1);
      delay(2); // Wait for Vref to settle
      ADCSRA |= _BV(ADSC); // Convert
      while (bit_is_set(ADCSRA, ADSC));
      result = ADCL;
      result |= ADCH << 8;
      result = 1126400L / result; // Calculate Vcc (in mV); 1126400 = 1.1*1024*1000
      return result;
    }
    
    /*
      Return an averaged reading from the Analog pin
    */
    float ReadAnalog(int pin) {
      uint8_t i;
      float average;
      float samples[NUMSAMPLES];
    
      for (i = 0; i < NUMSAMPLES; i++) {
        int value = analogRead(pin);
        float supply = readVCC() / 1000.0; // obtain vcc at time of read
        float valueCorrected = supply / 5 * value; // improve the accuracy of the analog reading
        samples[i] = valueCorrected;
        delay(10); // spread readings out otherwise they are likely to be the same value or very close
      }
      average = 0;
      for (i = 0; i < NUMSAMPLES; i++) {
        average += samples[i];
      }
      return average / NUMSAMPLES;
    }

     

    The useful bit is the readVCC() function and lines 27, 28 and 29.  The 'valueCorrected' variable is determined from a 5V range.  I don't think this will eliminate noise (probably just read that more accurately!) but may firm up readings.  I've not tried this on a MKR1000 by the way.

     

    It's an interesting project to follow along.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>