Personal Blogs
  • Community Hub
  • More
Personal Blogs
Hardware Electronic Diet - part 2
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 23 Mar 2018 5:07 AM Date Created
  • Views 2894 views
  • Likes 8 likes
  • Comments 8 comments
  • current consumption
  • battery
  • jumper cable
Related
Recommended

Electronic Diet - part 2

mcb1
mcb1
23 Mar 2018

In my first post Electronic Diet I explained the title

 

Okay so the title is a bit misleading.

I'm not planning on consumming electronics, or removing electronics from my diet (no I don't eat parts)

image

source https://favim.com/image/474959/

 

 

The plan

 

1. Check the current consumption of the unit.

2. Check to see if it can easily be reduced, and by how much.

3. Either fix it or replace it.

 

 

I've managed to find all the information about my fitted alarm unit.

In my digging around I even found the spare in it's box, along with about 4 others I had for repair/modification.

  imageimage

     source 3 minions (me, myself and I)

 

As the photo shows, these are old school with lots of discrete components, some CMOS chips and there is two different versions.

From what I recall both are 49MHz receivers, it's simply that one is much better.

However there does seem to be space for two relays, and I'm guessing that the one on the right might have had the ability to do the central locking without the extra unit.

 

I'm very happy the old unit has withstood the test of time, along flat batteries, massive voltage spikes and whatever else has been thrown at it.

BUT it does need to go on a diet and eat less joules.

 

I've scanned the circuit diagram, and there is lots of options to tweak values.

image

 

 

 

 

As a comparison this is the other unit I'm looking at.

image

     source 3 minions (me, myself and I)

 

It becomes fairly clear that there is very little capacity to reduce this units current consumption.

 

I can make some educated guess'es about the function of the other IC's, without looking underneath.

IC4 is to drive the relays for the integrated central locking.

IC3 is to store the codes or the options selected when you program it.

IC1 looks like a regulator, and the screen printing shows a TO220 style (1A LM7805LM7805 ) but it has a TO-92 fitted ( 100mA 78L0578L05)

 

The board standing up is a 305MHz receiver, and will be using a SAW type filter https://en.wikipedia.org/wiki/Surface_acoustic_wave

 

 

 

 

 

Current Consumption

The purpose of this is not to compare technology that is 20+ years apart, but help stop my battery going flat.

 

I've performed these measurements on the bench, and the first thing is to set the power supply to 12.00 volts.

This represents a figure that the battery may drop to when it's not being charged, and has been sitting for some time.

 

I'm not connecting anything to the inputs because when the doors are closed, the door switch is open.

So any pullup circuitry used on the inputs will be unaffected by not connecting the door switches.

 

Both units flash a LED, and the current consumption will change.

Luckily I was able to Road Test a Keysight  U1282AU1282A back in 2016 RoadTest the Keysight U1282A Digital Multimeter - Review

What wasn't indicated during the testing was the ability to view the max and min values, along with the average.

image

image

 

So despite the display changing, it's easy to get the figures.

 

 

Fitted Alarm

The current consumption is 65 mA in it's idle state.

This was lower than I imagined, but none the less quite high.

Most of the time the alarm isn't set but since it's powering a LED via a 1K resistor it could provide 9 mA when flashing.

 

 

Comparison model

The current consumption is 9.15 mA in it's idle state, rising to 12.48 mA as the LED flashed.

 

 

 

 

Why is the battery going flat?

So there was some questions, suggestions and ideas passed in the last post comments.

I hadn't given all the information about the vehicle, so to be fair these were valid comments about the battery condition.

 

Deep Cycle batteries are rated in AH, that is Amps per Hour, or if you want to swap it around how many hours at x Amps.

Generally the rating is based on a 10H discharge (ie at their rated cell voltage is reached in 10 hours), BUT I've seen some rated at the 20 hour rate, which indicates to me that they are not capable of high discharge rates.

 

Car batteries on the other hand are rated in CCA, or Cold Cranking Amps and usually have a temperature figure (often 20degC)

This figure represents the amount of current available to crank over your car, and has very little bearing on the AH.

 

Looking at a few batteries the CCA is 550-660 and the Reserve Capacity is 90-125.

 

 

So how many hours?

65mA is 0.065A.

90 AH / 0.065 = 1384 hours, which equates to 57.666 days until there is no capacity left.

If you expect to start the vehicle, you need some capacity, so it's not hard to see why this is going flat.

 

 

Solution

Well I now have some of the figures.

I need to do some more checks to see what other current vampires it has, before settling on the solution.

 

Since it's wet outside, this will have to wait until tomorrow and the next blog.

 

Part 3 here Electronic Diet - Engineering a Solution

 

Mark

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    It is like a treasure hunt. Find the leak and get the reward. DAB
  • mcb1
    mcb1 over 8 years ago in reply to genebren +2
    genebren Interesting the 0.065mA could be the culprit, but Current x Time is the issue I had a suspicion that it would be, but I suspect there are a few more mA being drawn as well, meaning it goes down…
  • three-phase
    three-phase over 8 years ago +2
    Depending on the age of the vehicle, I would suspect that there are also some additions to this 65mA such as the radio, clock and engine computer that usually have permanent 12V feeds to them, although…
Parents
  • DAB
    DAB over 8 years ago

    It is like a treasure hunt.

    Find the leak and get the reward.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to DAB

    DAB

    You made the comment in part 1

    You need to understand the problem before you run off an make a lot of changes.

    You are quite right, and sadly we have a big issue at work where they fail to understand the problem, before rushing into applying the first solution that comes into their head.

     

    Engineering a solution is a 4 step process

    1. It is important to fully understand the problem, and ensure the customer understands it OR the impact
    2. Find/Engineer the solutions that will cure the problem.
    3. Decide on the most appropriate solution, and apply it.
    4. Go back and check that it has solved the original problem, and almost as important, ensure it hasn't caused any other problems.

     

    Sadly I've seen far too many decide they have a solution and skip straight into step 3.

     

    If anyone wants some real world examples, I have a good story I can pass on.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to mcb1

    Hi Mark,

     

    Yes, trying to get people to slow down and think is a big problem.

     

    I once worked on a project where I was the IV&V on a 120 Million plus project and went out to the contractor for a status report. They complained that they had a "hardware" glitch in the lab and had spent the last six weeks trying to find it. At the time they were burning about $100,000 a week. After they described the problem, I explained to them that they had a timing problem in the software. Impossible they shouted and proceeded to explain how I did not know what I was doing.

     

    After they ran out of invectives, I calmly went to the white board and slowly walked them through their signal processing code and showed them why they were getting the exact symptoms they saw in the lab. Again, a lot of loud discussions and then we broke for lunch.

     

    After lunch, the head software designer, with is Phd, sheepishly came into the room and admitted that I was probably right. I proposed a couple of simple solutions, but in the end, they weaseled out of the requirement by changing the way they ran the system functions.

     

    Engineering is great, but when the bean counters get involved, you get crazy things happening.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago in reply to mcb1

    Hi Mark,

     

    Yes, trying to get people to slow down and think is a big problem.

     

    I once worked on a project where I was the IV&V on a 120 Million plus project and went out to the contractor for a status report. They complained that they had a "hardware" glitch in the lab and had spent the last six weeks trying to find it. At the time they were burning about $100,000 a week. After they described the problem, I explained to them that they had a timing problem in the software. Impossible they shouted and proceeded to explain how I did not know what I was doing.

     

    After they ran out of invectives, I calmly went to the white board and slowly walked them through their signal processing code and showed them why they were getting the exact symptoms they saw in the lab. Again, a lot of loud discussions and then we broke for lunch.

     

    After lunch, the head software designer, with is Phd, sheepishly came into the room and admitted that I was probably right. I proposed a couple of simple solutions, but in the end, they weaseled out of the requirement by changing the way they ran the system functions.

     

    Engineering is great, but when the bean counters get involved, you get crazy things happening.

     

    DAB