Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog An Extreme Ripple Power Supply Build
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 8 Apr 2019 2:49 AM Date Created
  • Views 2532 views
  • Likes 10 likes
  • Comments 20 comments
  • variac
  • isolation transformer
  • ac bench power supply
Related
Recommended

An Extreme Ripple Power Supply Build

jw0752
jw0752
8 Apr 2019

I usually like to build my projects before I blog about them. This is probably due to the number of times the initial plans do not lead me down the envisioned path. The simplicity of this build along with a good pile of solid resources and the fact that I must wait for my panel meters to arrive has made me decide to blog a preview.

 

In my shop almost never a week goes by with out the need of an AC voltage source. I use the AC source to test motors, lights, power supplies, and circuit boards as well as a substitute for transformers. Since I have built several DC bench supplies and blogged about them over the recent years I decided that it was about time to build an AC power supply suited to my needs. I am currently using a Variac that is plugged into an isolation transformer for my applications but it doesn't monitor the voltage or the current so there is always a lot of patch wires and a couple meters to clutter the bench.

 

Here is my wish list for the new bench AC power supply:

 

0 to 160 volts no load output

2 to 3 Amps capable

Isolated from the mains

Binding post and AC receptacle Output

High Voltage warning light

Meters for indication of Output Volts and Current

 

Initially I found the following items in my parts grave yard:

 

image

This will be the isolation transformer. I can put 115 volts on the primary and it will have 130 volts on the secondary. This will drive the small Variac pictured below.

 

image

 

The case will be from an old Dental Cavitron Scaler. I have used this same style case before to build a Bench Power Supply and a DC Electronic Load.

 

imageimage

 

The Plexiglas blank control panel was cut a couple years ago in anticipation of an application for this case. The case as seen in this picture it still needs a cleaning and a coat of paint.

 

image

 

The case has been painted and I have the tentative control panel layout on the sheet of paper next to the case.

 

image

 

The chassis has had some modifications. The metal that the variac is mounted to was originally part of the chassis deck but it has been cut and folded up to provide additional support for the relatively heavy variac. The cut out on the right side of the chassis came with the original piece of equipment. Anomalies like this often dictate where components and controls need to be placed. In this case it will be the recess needed to allow the mounting of an AC line Output jack on the front panel.

 

I have also produced a tentative Schematic for the power supply. I say tentative as I do not yet have the digital AC panel meters and so I am guessing at their requirements. Nothing ever runs true to plans so I will very likely have to take back a few of the things I told you here when I blog about the completion of the build.  Here is the tentative schematic.

 

image

 

One advantage to giving a preview of what I am building is that I can welcome any advice that anyone is willing to send my way. In the past ideas and advice from my many friends here on element 14 have resulted in renovations and improvements in subsequent builds.

 

Sorry about the title but sometimes it helps to get people in the door when I leave them asking what the heck is he talking about now.

 

Thanks John

 

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +4
    John, This looks like another interesting build. And yes, the title was a little catchy. I can see the use for a good A/C supply, although in my case, I live in such a D/C world. Only recently (my home…
  • Gough Lui
    Gough Lui over 7 years ago +4
    jw0752 - I don't claim to be an expert, but there are a number of notes and suggestions I would make. 1. Consider putting fuses on both primary and secondary sides of the Variac. They are expensive and…
  • jc2048
    jc2048 over 7 years ago +4
    Don't the test meters need their GND connection to be tied to the output neutral? Otherwise the voltmeter measurement is relative to a floating supply. If you'd incorporated a Pi, it could have been a…
Parents
  • jc2048
    jc2048 over 7 years ago

    Don't the test meters need their GND connection to be tied to the output neutral? Otherwise the voltmeter measurement is relative to a floating supply.

     

    If you'd incorporated a Pi, it could have been a 'Raspberry Ripple Power Supply'!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to jc2048

    Hi Jon,

     

    You are correct I have a problem with the electronic logic on my AC voltmeter. I will have to see what I can do about that after the meter arrives. The Ammeter uses a sense coil so that one should stay isolated OK. I may have to put a small one to one isolation transformer on the output and feed its secondary to the meter's sense and ground. I am not sure I want to tie one of the output leads to the meter ground. I will have to think about that and run some empirical tests to satisfy my doubts. I am always happy when you look at the electronic designs that I propose as your experience shines light in the dark corners of what I am trying to do.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 7 years ago in reply to jc2048

    Hi Jon,

     

    You are correct I have a problem with the electronic logic on my AC voltmeter. I will have to see what I can do about that after the meter arrives. The Ammeter uses a sense coil so that one should stay isolated OK. I may have to put a small one to one isolation transformer on the output and feed its secondary to the meter's sense and ground. I am not sure I want to tie one of the output leads to the meter ground. I will have to think about that and run some empirical tests to satisfy my doubts. I am always happy when you look at the electronic designs that I propose as your experience shines light in the dark corners of what I am trying to do.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Gough Lui
    Gough Lui over 7 years ago in reply to jw0752

    My personal feeling was that you really didn't have to have a second isolated output for the panel meters, but if you did, tying one of the legs of the transformer to the Variac to make a common "neutral" reference on the secondary side doesn't seem like a big issue? My main reason for thinking this is that even if you common a leg, the secondary side is still completely isolated from the incoming mains, thus shouldn't present any added danger. In the present configuration that doesn't really work, I also had a feeling that the meter became the "isolation" between two isolated parts which would perhaps be unwise depending on the quality of the insulation on the meter.

     

    If you really must ensure that the meters absolutely could not ever become live, then perhaps it might be worth incorporating a step-down transformer as the isolation and compensate for the step down in the metering configuration. This will have the advantage of having the meter being low voltage and meter input perhaps also low voltage - a wet hand touching the meter shouldn't be unsafe. In the same vein, perhaps rather than relying on an ammeter "shunt" which is still referred directly to the output mains, perhaps you might consider a current transformer (i.e. similar to how a clamp meter works). This would again add insulation between the metering and the output - but perhaps at the cost of accuracy in both cases.

     

    Another thing I thought of, depending on your Variac, perhaps some form of soft-start inrush limiting (NTC?) would be a nice additional feature, along with an input suppression network of sorts (X-caps, Y-caps, choke) which might be good to take out the occasional mains switching spike. If not that, perhaps a MOV would be enough to take out the biggest of surge spikes on the input side - we don't want to see it reflected in the output and frying stuff under test! You might also want to add a switch on the output (assuming US sockets don't have inbuilt switches) so you save plugging/unplugging items from test or arcing at the plug terminals.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Gough Lui

    Hi Gough,

    Thanks for the additional insights. I will incorporate them.

     

    Here is more information on the meters that may indicate that the potential problems we have been discussing may be academic.

     

    image

     

    image

     

    The Ammeter comes with a current transformer. This will still need some modification as the meter - transformer configuration is for 100 A which is much to high for my expected range of 0 to 3 Amps. I figure I can wind 10 loops of the line through the current transformer and that should turn it into a 10 Amp full scale. I will then either move the decimal point or designate the meter as "divide by 10".

     

    After looking more closely at the meters I see that I do not need to produce a DC supply for them either. I haven't decided whether I will use this short cut or not.

     

    It is always an adventure which is all the more enjoyable with insights from my friends and almost nothing to loose with respect to cost.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Gough Lui

    Hi Gough,

     

    I have made changes to the schematic reflecting the improvements that you suggested, including 3 fuses and an MOV. I have also corrected the schematic to indicate the proper wiring of the meters. The jury is still out on whether I use AC or DC to power the meters. Since the meters specs indicate a power supply of 9 to 12V AC or DC I have lowered the meter power supply transformer to a 7.5 Volt secondary if I rectify it. This will yield about 9 volts DC to power the meters. I will run some tests on the meter power circuit to verify that I am in the specified 9 to 12 volt window. I did not add an in-rush varistor as the inductive load should provide its own soft start. I also found an error in the current limit resistor I was using on the power indicator LED and have lowered it from 10K to 680R.

     

    image

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to jw0752

    That looks a bit better. The only reason I bought up soft start was purely because you had so much inductance around, and because I read up on Rod Elliot's pages about Transformers and Inrush, specifically Transformers Part 2 - Beginners' Guide to Electronics  and Inrush Current . Granted, your unit may not be big enough to pose an issue as such, but I suppose it could be a little harsh on your power switch and power supply not to have it, especially if you're turning it on and off frequently and remnant magnetization remains in the core (hence why a switch on the secondary was my suggestion as well).

     

    Regardless, this got me thinking - why didn't I get involved in building a behemoth like this for my experiments? That's because I solved the "issues" a different way - I do my AC experiments on a small 1A Variac connected to a 230V AC pure sine-wave inverter that is powered by an *isolated* switchmode bench-top supply. I basically lopped off the leads and soldered them to banana plugs to go straight into the front panel of a spare 20A switchmode PSU with floating outputs. This way, I get isolation, protection from mains transients and current limiting out of the box. For metering, I'm fortunate to have received a Tektronix PA1000 Power Analyzer, so that goes in-between the variac and the DUT socket with its own switch. Isolation transformers with decent capacity can be fairly expensive, so I had back-to-back 300VA toroidals (which cost me a fortune) but were heavy and bulky - although I still have it, I rarely use it compared to the inverter rig.

     

    The only downsides of my particular arrangement are (of course) the very limited output power, some high frequency noise/harmonic distortion because of the inverters' PWM method of producing a sine wave, the noise of the inverter fan itself and potentially questionable reliability of cheap inverters. For low duty usage, it's probably not too bad. It also doesn't handle largish loads with very poor power factor and might struggle with inrush start-up currents of some larger appliances. It really only works if you use a floating supply for safety and don't touch anything metal while powered - as some inverters do rather stupid things with the Earth connection (some common this to the negative input terminal!).

     

    Food for thought, I guess.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Gough Lui

    Sounds like you have a good system for your needs. It is always a compromise of one type or another. I have on a couple occasions bought a used 600 watt computer power conditioner and modified it to be an isolation transformer. This has worked pretty good and being used it has saved a lot of money on the cost of a large toroidal transformer. Here is the one i have sitting on the shelf awaiting my next need.

     

    image

     

    This is a PowerVAR 6.0.  I have one like it that feeds a mains strip on my bench which I use when needed. One still has to be very careful but at least I don't have to feel quite so threatened by the anti-static strip on the edge of the bench.

     

    John

    • Cancel
    • Vote Up +4 Vote Down