Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Experiment to Test Tandem LM395 IC Darlington Modules
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 24 Nov 2014 2:40 PM Date Created
  • Views 3151 views
  • Likes 2 likes
  • Comments 23 comments
  • lm395
  • darlington
Related
Recommended

Experiment to Test Tandem LM395 IC Darlington Modules

jw0752
jw0752
24 Nov 2014

A few days ago I posed the question of whether I could add a second Darlington Power transistor in parallel to a commercial circuit that was poorly designed. The response from all of my mentors on E-14 was accurate and to the point. Amongst the many replies was one however that has caused me to take this question one step further and investigate an interesting component IC.

 

Don Hersey Wrote:

 

28. Re: Feasability of Adding a Second Parallel Darlington?

image Level 5: Faraday

  Don Hersey Nov 17, 2014 8:06 AM (in response to John Wiltrout)

The pwr on led needs a reversed signal diode in shunt.  LEDs have a reverse breakdown potential of about 6V.  When we parallel bipolars, as an earlier poster stated, we need ballast resistors to minimize current hogging due to the negative tempco of the Qs.

 

Hanging an emitter follower  on the VR produces an output a diode drop below the regulator output.  As a prior poster noted your Q is operating in the linear mode, probably you should embiggen your heatsink.  When one does that (hangs a Q on a VR) he does increase the ampacity of the regulator.  But he loses the thermal shutdown feature.

 

The http://www.ti.com.cn/cn/lit/ds/symlink/lm395.pdf LM195 is the transistor for you.  Even though it is bipolar, they can be paralleled freely as they have thermal feedback control on-board.

 

You can do better than this.  I suggest you read a book or two on operational amplifiers and maybe one on SMPS design

 

 

I bought a couple of the LM395T Transistor substitutes that were mentioned by Don and I set up the following experiment. If you want a better picture of the component in question please use Don's link to pull up a Data Sheet from TI. The LM395T is designed to take the place of a Darlington with the added features of thermal, current, and power limit protection.

 

I used the previous circuit design with a LM317 regulator as the variable driver for a Darlington as the starting point and then I removed the Darlington and substituted (2) LM395T.

 

Here is a schematic:

 

image

 

My plan was to breadboard the circuit and then use the scope to measure the voltage drop across the one Ohm emitter resistors of the LM395s. I would then do a Channel A minus Channel B plot on the Oscilloscope. If the 2 LM395s did actually work together and share the load I should be able to run the output of the LM317 variable regulator from minimum to max with no appreciable change in the A-B Plot. If on the other hand one of the LM395s lagged back and did not share the load we should see a change in A-B with the increase from min to max output.

 

 

Here is the completed test setup with the first oscilloscope scan showing the voltage across R-7 and R-8 and the difference plot in the middle.

 

 

                  imageimage

 

 

Please remember that this is all about learning and any suggestion that you have for how I could have better set up the experiment or made the setting on the scope will be appreciated. In hind sight it may have been better if I had averaged the channel 1 and 2 readings to clean up the difference plot. I looks like I have 96 mV across the R-8 resistor and 104 mV across the R-7 resistor. The 1 Ohm resistors that I used in the circuit had a "J" code and are therefore rated at 5%. This 5% rating of the resistors along with breadboard connections would lead me to believe that at least at this minimal setting the 2 LM395s were sharing the load. This minimum setting can be the most difficult for the components under test. Since nearly all of our 20 Volts is across the LM395s and we are showing a current of 100 mA the LM395s are each required to dissipate approximately 2 Watts of power. As you can see I have them in free air on the breadboard. Not having learned, after 50 plus years in electronics, not to touch hot things I have a minor red mark on the end of my finger in the shape of a TO-220 case.

 

 

The next step is to slowly turn up the voltage of the LM317 and watch the voltages across R-7 and R-8 as well as the difference plot. Here is the final view of the circuit and the oscilloscope plot when the LM317 was at full voltage.

 

 

                imageimage

 

 

I like to use light bulbs to load my test circuits, in most cases, as I have a visual feedback of what is going on. From the point of view of linearity this is of course not the best idea. Bulbs start off with low impedance and then increase as they heat up. The scope indicated that both of the LM395s shared load as the voltage of the LM317 was increased. I did note that the channel 1 which was reading higher than channel 2 at the minimum by 8mV had changed places and was reading 72 mV lower than channel 2 at the max setting. I am not sure what this would indicate, perhaps there is an optimal input voltage cross over point at which the two LM395 would best work together. Throughout this experiment I have talked about turning up the voltage of the LM317 to drive the LM395s. What this has actually been doing is increasing the base currents in the LM395s as they are current controlled devices and I want to make sure I didn't give the impression that they were voltage controlled. Since this test was basically a meet and greet between the LM395 and myself and I have no immediate application for it my curiosity is satisfied at this point that the LM395 can indeed be used in tandem and would work well in the application to which Don Hersey recommended it.

  • Sign in to reply

Top Comments

  • D_Hersey
    D_Hersey over 11 years ago +1
    I'm thrilled that you tried my suggestion! IIRC these were developed by Widlar et al at the same time as other Linear Monolithic devices such as voltage regulators of the day. It uses the same thermal…
  • jw0752
    jw0752 over 11 years ago in reply to mcb1 +1
    Hi Mark, I broke the Old Dog New Trick mode. Today I made a more sensible way to test. See new blog post. John
  • shabaz
    shabaz over 11 years ago in reply to Problemchild +1
    It is like PP3 battery testing Did the creators of the PP3 standard put the connections on one side to make then easier to lick?
Parents
  • DAB
    DAB over 11 years ago

    Excellent post John.

     

    You can also set up a small circuit to better balance the current flow between the devices, but as long as they behave, it looks like you have a good solution.

     

    Also, all of us have a burn scar somewhere on our hands.  We engineers just have to touch stuff, you know!

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to DAB

    Thanks DAB,

    If you have time to give me an example or two of what a balancing circuit would look like it would be of interest to me. No need to put too much time into it but I am curious enough so I would probably set up the circuit again for a little empirical analysis.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago in reply to jw0752

    Hi John

     

    What I thought was to use a comparator across the two outputs.

    You could monitor the output current flow and then introduce feedback to one of the drivers so that it could regulate its gain compared to the other device.

    You could use a couple of resisters to add some hysteresis and moderate the gain adjustment.

     

    You could also set up the comparator to trigger a cutoff signal if the two outputs exceeded a given difference, that way you could tell if one of the drivers died.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago in reply to jw0752

    Hi John

     

    What I thought was to use a comparator across the two outputs.

    You could monitor the output current flow and then introduce feedback to one of the drivers so that it could regulate its gain compared to the other device.

    You could use a couple of resisters to add some hysteresis and moderate the gain adjustment.

     

    You could also set up the comparator to trigger a cutoff signal if the two outputs exceeded a given difference, that way you could tell if one of the drivers died.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 11 years ago in reply to DAB

    You are a good teacher. You have told me what to do and not how to do it. I am taking a break right now from working on some ideas for implementing the comparator control. Schematic on paper in the works.

    Thanks John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to DAB

    Hi DAB, I installed 2 comparators from an LM339 into the circuit. What I learned is that the circuit was very stable already and I could make no improvement with the comparators. I did learn that when I coupled the outputs of the comparators too closely to the LM395 input they made a dandy 1 MHz oscillator. I eventually put the comparator's outputs into LEDs and installed a fine control potentiometer to precisely balance the input voltages to the LM395 chips. I could turn the control one way and one LED would light showing an imbalance to that side, turn the control the other way and the other LED would light. When I got it properly balanced the two LED's both appeared lit though they were in fact bouncing back and forth to quickly for eye resolution. Thanks for encouraging me to investigate a little further as I am even more satisfied now with the performance of the LM395T Chips.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago in reply to jw0752

    I am glad that you had fun with it.

     

    I get weird ideas all the time so I was very happy to see that you actually did the project.

     

    It sounds like your driver transistor are very close in operating parameters.

    If you want some real fun, try using different types of driver transistors to see how much correction they need to keep the circuit stable.

     

    You know me, always thinking.

     

    DAB