Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Experimenting with an Isotek Kelvin Resistor
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 21 Mar 2016 5:55 AM Date Created
  • Views 1121 views
  • Likes 5 likes
  • Comments 12 comments
  • current_sense_resistors
  • kelvin_resistor
Related
Recommended

Experimenting with an Isotek Kelvin Resistor

jw0752
jw0752
21 Mar 2016

Today I salvaged out a circuit board from an ESPE Dental Cure light. To my delight there was Kelvin precision resistor on the board. Specifically it was an Isotek PBV R033 which is a heat sink mounted 10 Watt Kelvin resistor with a value of 0.033 Ohms 1%. Here are front and back photos of the device. I first learned about these resistors a couple years ago from one of the great tutorials posted by Robert Peter Oakes on building power supplies.

 

image

 

image

 

Now in the big scheme of things the arrival of a real 4 terminal Kelvin resistor to my bench must seem pretty trivial but this is my first. Yes in 55 + years of tearing equipment and circuit boards apart this is the first time I have had a Kelvin Resistor to test out. What follows is an exercise in simplicity but it is the type of experiment that must be performed on the occasion when something new shows up. In case you would like more information on this particular resistor here is a link to the company data sheet:

 

http://www.isotekcorp.com/sites/default/files/sites/default/files/pdfs/PBV.pdf

 

I began by producing a new custom symbol for my schematic drawing program. I always like to produce a schematic before an experiment even if it is fairly simple like this one. Here is a copy of the schematic for the test setup:

 

image

 

My plan was to power the circuit at 4 different current levels and take readings of the Current (I), the voltage of the source (Vs), and the voltage across the Kelvin Resistor (Vkr). I would then use my empirical numbers to calculate the resistance (Rk) of the Kelvin Resistor and compare the calculations to the nominal value of 0.033 Ohms 1%. The readings for the voltage of the source would not figure into the calculations but I like to have them for an overview of the system. Keep in mind that perhaps the most accurate instrument in my shop is a Fluke 177 which will be used for DC current readings. Basically none of my equipment qualifies as precision just practical for my level of endeavor. The other equipment that will be used for this experiment are a Mastech power supply which will be the current source and a Radio Shack digital meter that will read the voltage at the test terminals of the Kelvin resistor. The final digit of the Radio Shack meter will read 0.1 mV.  In the chart that follows I have listed the calculated values of (Rk) to several magnitudes of precision past the point justifiable by the precision of the instruments. This was done only to give a better feel for the proximity of the results to the nominal value of (Rk). Ohams Law V = I x R was the basis for the calculations.  Here is the test setup that I used:

 

image

 

The resistor resting on the glass block is a 2 ohm 25 W resistor that is being used as a load. When the circuit was fully powered at 1 Amp the dissipation required was about 2.7 watts. This resistor does not figure into our calculations either.

 

image

 

While not necessary for this experiment, if everything runs smoothly, the Kelvin resistor was stuck to the glass desk top to serve as a heat sink. The Kelvin resistor can dissipate 3 Watts in free air and 10 Watts when properly heat sunk. Since things do not always run smoothly on my bench I try not to take chances hence the heat sinking. Here is the data that was collected from the experiment:

 

image

 

The nominal value of the Kelvin Resistor is 0.033 Ohms with a 1% tolerance. This means that the actual value should lie between 0.03267 and 0.03333 Ohms. I am pleased that my calculated results also fall within that 1 % range. I will now put the new Kelvin resistor aside for use in my next power supply build.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +2
    Excellent blog and demonstration how to use simple equipment to validate the test.
  • shabaz
    shabaz over 10 years ago +2
    Hi John, Nice find and analysis! At first glance I would have mistaken it for a bridge rectifier. Also, what a cool idea to have the labels to make it clear what each meter is being used for. I was looking…
  • clem57
    clem57 over 10 years ago +1
    Nice find! But after reading, the four posts are not clear. I see the outer two you put the load and the inside I see the v=ir with a voltage meter? Clem PS How common are resistors over 1 mega ohm? I…
Parents
  • clem57
    clem57 over 10 years ago

    Nice find! But after reading, the four posts are not clear. I see the outer two you put the load and the inside I see the v=ir with a voltage meter?

    Clem

    PS How common are resistors over 1 mega ohm? I may need a few to many for a project I am working on:

    DIY Capacitive Touch Made Easy | Hack N Mod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57

    A Kelvin resistor at 1MOhm is rather pointless as the whole point is to allow for the removal of the contact resistance and wire resistance to be eliminated from the measurement,  The further you get from single digit Ohms (Going up), you see a diminishing return on the usefulness of them. Going down however see's an ever increasing benefit

     

    The Idea is that you pass a constant current through the resistor using the outer leads but do not measure the volts across the resistor with the same contacts. As this is constant current the resistance of the contacts to the resistor are irrelevant (Its constant current)

    Now using the inner two contacts which are separately connected to the resistor you measure the volts. As the measurement device is high impedance (10Meg Ohms or so) including the leads, then the contact resistance has negligible effect on the measurement as the current flowing through the measurement device is so lowimage

    The diagram is from here, if you want to read more about it Kelvin (4-wire) Resistance Measurement : DC Metering Circuits - Electronics Textbook

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Robert Peter Oakes

    So R subject is the load. Right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to clem57

    Hi Clem,

    No in Peter's drawing there is no load per se. The R subject is the Kelvin Resistor. If you are using a current source then technically you do not need another load to limit it as I did. I put it in to make it a more practical circuit as any practical circuit would have a load that the current would be working through as well as the sense resistor (Kelvin resistor).

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57

    R is the Kelvin Resistor, if you want a load int he circuit then it would be in series with one of the outer loops where it will not interfere with the measurement of the Kelvin Resistor

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57

    R is the Kelvin Resistor, if you want a load int he circuit then it would be in series with one of the outer loops where it will not interfere with the measurement of the Kelvin Resistor