Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Exploring the LT4320  Ideal Diode Bridge Controller
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 1 Feb 2017 7:56 AM Date Created
  • Views 8323 views
  • Likes 9 likes
  • Comments 14 comments
  • lt4320
  • ideal diode bridge
Related
Recommended

Exploring the LT4320  Ideal Diode Bridge Controller

jw0752
jw0752
1 Feb 2017

A while back I heard that a diode full wave bridge could be replaced with MOSFETs that were switched in the proper sequence. The advantage of doing this would be the very low Rds(on) available from the MOSFETs which results in much lower waste heat generation and more power delivered to the load. For this experiment I am going to use the Linear Technologies LT4320 controller and (4) IRLZ34 N channel MOSFETs. I will also set up a conventional diode bridge and compare the readings that I get from each system. Here is a link to the data sheet for the LT4320:

 

http://www.farnell.com/datasheets/1804288.pdf?_ga=1.70622352.1418853850.1451543312

 

Here is a simple schematic from the data sheet for how the LT4320 connects to the MOSFETs

 

image

 

While the LT4320-1 is capable to 600 Hz the chip I am using is the LT4320 and it is rated for up to 60 Hz operation.

 

I will begin by constructing a simple full wave bridge using a common 4 diode package and take some readings. I have also installed a 680 uF capacitor across the output.

 

image

 

The transformer in the picture has been connected to a variac and the output has been dialed to 25.75 Volts AC under load. This may appear a bit arbitrary but when the variac you are using isn't precision you take the first stable value that is close to the desired value. I have loaded the circuit with (4) 12 volt auto tail light bulbs in series. With this load we measure the DC output of the system at 27.97 Volts DC and the current is 390 mA.

 

image

 

The AC ripple on the voltage is 2.68 Volts.

 

image

 

Here is what the wave form across one junction looks like:

 

image

 

The next step in the experiment was to wire up the LT4320 and the (4) MOSFETs. While the schematic looks very simple it turned out to be rather more complicated. In the end I used wire jumpers instead of the more solid staple connectors. It is likely that this will result in a higher connection resistance and will lower the performance difference that I hope to observe. Here are a couple pictures of the circuit:

 

image

 

image

 

The MOSFET circuit performed very nicely. Once again our input voltage under load was 25.75 VAC. The output voltage of the system into the load was 29.5 Volts DC and despite the lighter wiring we had a current of 400 mA. The ripple of the MOSFET system was also 2.68 VAC. Here are shots of the meters and the oscilloscope screens for the ripple and across the drain - source on one MOSFET.

 

image

 

image

 

image

 

In both experimental setups I monitored the temperature of the devices with the finger tip thermometer. The diode bridge got almost hot to the touch while the MOSFETS remained cool. This was not very scientific and may also be explained but the much larger surface area of the MOSFETs compared to the Diode Bridge. Here are the data from the two experiments side by side.

 

                              Diode Bridge                              LT4320 & MOSFETs

 

Input Voltage          25.75 VAC  60 Hz                      25.75 VAC 60 Hz

 

Output Voltage       27.95 V DC                                29.4 V DC

 

Ripple                    2.68 V PP                                   2.68 V PP

 

Load Current          390 mA                                        400 mA

 

The MOSFET Ideal Diode Bridge using the LT4320 controller seems to be a much better system for rectification as it delivers more power to the load and has less heat generated. Keep in mind that the LT4320 and MOSFETs still showed an improvement despite being wired with the higher resistance jumper wires. On the other hand the complexity of the circuit and the magnitude higher cost over the diode bridge will not make this a practical replacement in most applications.

 

John

 

 

 

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +4
    I wasn't very happy with the breadboard of the LT4320 Ideal Bridge circuit. The jumper wires that I used added a resistance variable that did not allow me to get a good comparison with the regular diode…
  • jw0752
    jw0752 over 9 years ago in reply to D_Hersey +1
    Since I don't remember where I first heard about it I have decided it was probably from you. Over the years a lot of inspiration has flowed from Chicago to the Northwoods of WI. Thanks Don John
  • jw0752
    jw0752 over 9 years ago in reply to DAB +1
    Thanks DAB, My projects for the most part are pretty simple. The ones I have really been enjoying are those by jc2048 since they are so well done and have a lot more meat on them than mine do. I see we…
Parents
  • akaad
    akaad over 5 years ago

    The LT4320 ideal bridge is great.

    Energy saving.

    Headache saving.

    But I cannot find the part on the Farnell.NL component search - i.e. they do not stock it.

    How can that be proposed?

    From the innovation a few years back, now several boards have been develooped for these components. That implies the demand should increase.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to akaad

    Hi Albert,

     

    You are right Newark doesn't seem to stock it. When this happens to me I usually go to Octopart and search the part number. They will list the companies that do have the part and the quantity in stock.

     

    https://octopart.com/search?q=LT4320&currency=USD&specs=0

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • akaad
    akaad over 5 years ago in reply to jw0752

    And so I found Mouser, but they charge € 20 for shipping (and that is a flat fee). That is a lot compared to the items; while I have a Farnell account :-) so like to stay 'at home'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to akaad

    Check Ebay as they may have a cheaper source.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 5 years ago in reply to akaad

    Check Ebay as they may have a cheaper source.