Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Learning Circuit Inspires  "The Watch Stand"
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 6 Feb 2019 3:41 PM Date Created
  • Views 1320 views
  • Likes 15 likes
  • Comments 10 comments
  • joule_thief
  • watch_stand
  • battery juicer
Related
Recommended

Learning Circuit Inspires  "The Watch Stand"

jw0752
jw0752
6 Feb 2019

Karen's Learning Circuit Presentation:

 

The Learning Circuit 39: Inductor Project: Battery Juicer

 

got me to playing around with the Battery Juicer Circuit also called the "Joule Thief". You can check out her blog for a schematic and some suggestions. For her build she made a flashlight but I had other ideas for a good use.

 

When I finally crash at night I put my watch next to the bed. Unfortunately it is quite dark in the room so if I wake up and want to know what time it is I have to turn on the light on the table next to the bed. This usually wakes me up more than I want to and it also disturbs the boss. When I saw the nice low level light produced by the LED in Karen's experiment it dawned on me that this would be a perfect night light and watch reading light for the bedroom.

 

A couple hours and about 3 feet of 12 gauge copper wire later I had "The Watch Stand"

 

image

 

The watch stand runs on dead AA batteries that won't even power a wall clock. The circuit is the same simple circuit demonstrated in the Learning Circuit. I used a common mode inductor from a switching power supply, a salvaged NPN transistor from an old CFL light bulb circuit, a single AA holder, and the other electronic components needed to complete the build. A small push latch switch was also installed so the unit could be turned off when not in use. No sense wasting those stolen joules. It looks a bit strange, perhaps a bit like the Lunar lander, but it fits well with my sense of the aesthetic.

 

Here are a few more pictures so you can see it from a few different angles:

 

imageimage

 

imageimage

 

The yellow light diffuser that I have placed over the LED so that I do not get a sharp reflection off the watch crystal is something that was acquired over 50 years ago and has been patiently waiting in my Bulb Sockets box for a practical use.

 

Electronics is fun and inspirations are to be found everywhere we look. Thank you to Karen and the element14 Learning Circuit for a fun project.

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago in reply to shabaz +5
    Hi Shabaz, Thanks, I use a combination of vises and clamps. Since it is heavier gauge copper I have a bit of a problem with it self heat sinking so I pre-tin my target area and then come in hot and quick…
  • jw0752
    jw0752 over 7 years ago +5
    Addendum: I have continued to experiment with the Battery Juicer / Joule Thief circuit to learn more about how it is affected by different transistors and different transformers. Obviously the choice of…
  • rachaelp
    rachaelp over 7 years ago +3
    Excellent work John, it looks really cool and very useful to have to see your watch in the night. Definitely a very nice project! Best Regards, Rachael
Parents
  • shabaz
    shabaz over 7 years ago

    Hi John,

     

    Nice project! How are you holding the shapes together while soldering? You're getting great use out of the round-nose pliers : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    Hi John,

     

    Nice project! How are you holding the shapes together while soldering? You're getting great use out of the round-nose pliers : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 7 years ago in reply to shabaz

    Hi Shabaz,

    Thanks, I use a combination of vises and clamps. Since it is heavier gauge copper I have a bit of a problem with it self heat sinking so I pre-tin my target area and then come in hot and quick. Most of the time perfection isn't necessary as the wire can be adjusted after being soldered to compensate for a slight misalignment.

     

    John

    • Cancel
    • Vote Up +5 Vote Down