Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Playing with an OP 191 Op Amp
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 22 Jan 2016 7:42 AM Date Created
  • Views 2936 views
  • Likes 5 likes
  • Comments 12 comments
  • op191_op_amp
Related
Recommended

Playing with an OP 191 Op Amp

jw0752
jw0752
22 Jan 2016

One of the really great things about the E-14 Web Site is how much one can learn just by reading and paying attention to some of the threads. On Jan 9th michaelkellett posted information on the OP191 and OP192 Op Amps which he likes to use in his designs. Being curious to play with them for myself I marked down the number and ordered some of the OP 191 for my shop. The OP191s that I received were in the SOIC8 package so it was necessary to mount it on an adapter board so that I could conduct some simple experiments on the bread boards. Here is the OP191 after I mounted it on the adapter and turned it into a DIP8.


image


I next built a simple circuit with a gain of 10 and used my wave form generator and my oscilloscope to look at the limits of the chip and how well it performed. Here is the simple circuit.


image


I used a +/- 10 volt supply for the chip and I ran the input level down until I could no longer get good readings on my scope. I was very impressed with how well the OP191 worked. Actually it doesn't take that much to impress me or to cover my needs. I could have taken michaelkellett 's word for it but what would have been the fun in that? The Op Amp did a very good job reproducing sine, square, and ramp inputs.


Here are the readouts of the test equipment during one of the experiments on the Op Amp.


image

 

image

image


Thanks again to MK for the excellent recommendation and all the fun I had tonight playing with the OP191. It will be fun to use it in my next build that requires this level of Rail to Rail Op Amp. If you want to read MK's original post it is in this thread


Power Supply for Home lab?

by mudz


John.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 10 years ago +2
    I'm glad it's working well - I've just finished the design of a board for a client with 9 OPA192s on it - the bare boards should be here on Tuesday so I'll post some pictures (and a some bits of circuit…
  • jc2048
    jc2048 over 10 years ago in reply to jw0752 +2
    I glossed over it in my post, but there are two main effects that roll off the response at higher frequencies. One is the decline in the open loop gain, the other is the slew-rate limitation of the output…
  • jc2048
    jc2048 over 10 years ago in reply to jw0752 +2
    Your roll-off is much earlier than the datasheet would suggest (Figure 15). It's a bit difficult to read, but at a closed-loop gain = -10 their graph shows the actual gain falling by half (-6dB down) at…
Parents
  • jc2048
    jc2048 over 10 years ago

    Very nice part.

     

    TI have a spice model for it, so I thought I'd try your experiment virtually on my computer.

     

    Here's the circuit (inverting amplifier, gain of 10) with +12V and -12V supplies

     

    image


    And here are the waveforms, the input is 100mV peak and the output is 988.55mV peak so it works! A gain of 9.8855, so almost 10.

     

    image


    And here's the frequency response. The roll-off is what you'd expect from the decline in the open-loop gain at higher frequencies, so it looks at first glance like the modelling is quite good and simulation would have some use for experimenting quickly with circuit ideas and configurations.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to jc2048

    Hi Jon,

    I had some time so I used a +/- 12 volt supply and an input voltage of 500 mA. I then varied the frequency from 1 kHz to 500 kHz where I found the gain to be unity. Here is a graph of the output voltage P-P versus the frequency in kHz. I was not able to compare your projected graph to my output easily as yours is in db gain and has a logarithmic scale but they both seem to indicate where the drop out starts to occur. As i mentioned my cables and test equipment are likely to affect the readings as well. Here is a rough graph of what I measured.

     

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to jw0752

    I glossed over it in my post, but there are two main effects that roll off the response at higher frequencies. One is the decline in the open loop gain, the other is the slew-rate limitation of the output. How much the slew-rate affects you depends on the size of the output signal. You should be able to see which is the limiting factor at around 70-80kHz if you look at the shape of the output waveform - if it's still a sine wave it's the gain reducing, if it's triangular it's slew rate (the output not keeping up). You'd also see if you plotted the response for different output amplitudes. If all the curves sit on top of each other it's the gain, if they diverge and take different paths it's the slew rate (that's if you plot the gain rather than the voltage, of course).

     

    For a true comparison you'd need to match my output level (2Vpk/pk) or I'd need to run the simulation with an output of 5Vpk/pk.

     

    As you say, there could be other effects. We also don't know how good the simulation model is - it's reasonable to expect it to be accurate in the area where the chip would normally be operated, less so operating without feedback with just the natural gain of the amplifier.

     

    In a way this is a bit unfair to TI and the amplifier. They really wouldn't expect anyone to actually be operating the part like this.

     

    BTW I'm well outside my comfort zone here even though it's simple op-amp stuff. Most of my career has been working with logic and processsors and the only analogue design I've done along the way is simple sensor conditioning. I'm very rusty on the basics.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 10 years ago in reply to jw0752

    I glossed over it in my post, but there are two main effects that roll off the response at higher frequencies. One is the decline in the open loop gain, the other is the slew-rate limitation of the output. How much the slew-rate affects you depends on the size of the output signal. You should be able to see which is the limiting factor at around 70-80kHz if you look at the shape of the output waveform - if it's still a sine wave it's the gain reducing, if it's triangular it's slew rate (the output not keeping up). You'd also see if you plotted the response for different output amplitudes. If all the curves sit on top of each other it's the gain, if they diverge and take different paths it's the slew rate (that's if you plot the gain rather than the voltage, of course).

     

    For a true comparison you'd need to match my output level (2Vpk/pk) or I'd need to run the simulation with an output of 5Vpk/pk.

     

    As you say, there could be other effects. We also don't know how good the simulation model is - it's reasonable to expect it to be accurate in the area where the chip would normally be operated, less so operating without feedback with just the natural gain of the amplifier.

     

    In a way this is a bit unfair to TI and the amplifier. They really wouldn't expect anyone to actually be operating the part like this.

     

    BTW I'm well outside my comfort zone here even though it's simple op-amp stuff. Most of my career has been working with logic and processsors and the only analogue design I've done along the way is simple sensor conditioning. I'm very rusty on the basics.