Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Unusual Circuit board configuation
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Mar 2017 5:20 AM Date Created
  • Views 1095 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended

Unusual Circuit board configuation

jw0752
jw0752
27 Mar 2017

I was busy salvaging a bunch of Dental electronic equipment for interesting parts when I came across this interesting circuit board construction and I thought you might get a kick out of it.

 

image

 

image

 

image

 

image

 

image

 

This is a driver circuit from a handheld LED composite cure light. It allows the operator to select a timer setting and drives a high power LED that has it's light output towards the blue end of the spectrum. The unit also controls a cooling fan the size of a dime to help cool the LED. In order to fit the needed components into a body witha diameter on the order of a broom handle they had to stack a set of circuit board disks 2.2 cm in diameter.  Pretty cool!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +2
    Interesting stack. We used to use this technique in the old days where we needed to keep circuits in cylindrical devices like missiles and rockets. I would say they expected quite a bit of vibration given…
  • COMPACT
    COMPACT over 9 years ago +1
    Some of those PCBs are rather thick!
  • mcb1
    mcb1 over 9 years ago +1
    I had a feeling it was inside a housing, that had limited size.
Parents
  • COMPACT
    COMPACT over 9 years ago

    Are you sure it's not because the thick PCBs are multilayered as the top PCB is substantially thinner?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 9 years ago

    Are you sure it's not because the thick PCBs are multilayered as the top PCB is substantially thinner?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 9 years ago in reply to COMPACT

    Hi Compact,

    The three boards in the middle have components on both sides while the end pieces have components on only one side. I would be surprised if the thicker boards are more than just double sided but I do not know. I used a magnifier to see if I could detect more than two layers but there was no indication and I doubt that the circuit is complicated enough to need this. In any case your guess is as good as anyone else's. Thanks for your insight.

    John