Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog Fast Test Amplifier - Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 10 Aug 2018 5:04 PM Date Created
  • Views 1336 views
  • Likes 10 likes
  • Comments 9 comments
  • test amplifier
Related
Recommended

Fast Test Amplifier - Part 1

michaelkellett
michaelkellett
10 Aug 2018

A while ago (July 5th) in the discussion

 

https://www.element14.com/community/message/241748/l/programmable-frequency-generator#241748

 

I suggested an approach to building a low cost high frequency power amplifier.

The idea was to keep the design as simple as possible and base it on the classic 1970s bipolar transistor based HiFi power amplifier.

 

I've taken the idea a bit further and designed some boards, and finally got round to putting the parts on one and doing a bit of testing today.

 

The final schematic looks like this:

 

image

And the board looks like this:

 

image

 

I've been testing it cautiously using +/- 12V supplies (should be OK up to +/-18) and a 20 ohm load.

So far it looks quite good, small signal bandwidth is up to 10MHz but it can't do anything like full power at that frequency.

All the tests below were 12V pk-pk into 20 ohms:

 

Sine wave at 1MHz:

image

 

And the spectrum of the same:

 

image

 

Square wave at 500kHz:

 

image

 

And a close up to look at the slew rate:

 

image

 

So far it doesn't look too bad - quite a bit more testing to do and almost certainly some tweaking. I'm hopeful of meeting my target spec of 10W into 8 ohm load up to 2 MHz.

 

If anyone wants to build one I'll be posting the BOM and will put the Gerber files on Dropbox or similar.

 

MK

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +3
    Hi Michael, That's really neat, it could have science applications, or working with transducers. I'd be interested to replicate at some stage when you get the info posted. I've been busy on a DDS project…
  • DAB
    DAB over 8 years ago +3
    Nice update. Are you going to show the bandwidth response? DAB
  • three-phase
    three-phase over 8 years ago +3
    Looks like a very neatly laid out PCB. Kind regards
Parents
  • jc2048
    jc2048 over 8 years ago

    Good stuff. Effectively, it's a high-power op amp, which I suppose is where those amplifier designers were getting some of their ideas from.

     

    Look forward to seeing if you can make the thermal side work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 8 years ago

    Good stuff. Effectively, it's a high-power op amp, which I suppose is where those amplifier designers were getting some of their ideas from.

     

    Look forward to seeing if you can make the thermal side work.