Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: The Lab: Found More Test Equipment: SMD Rework Station 853D
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 5 Feb 2021 11:31 PM Date Created
  • Views 1264 views
  • Likes 5 likes
  • Comments 2 comments
  • flight simulator
  • nexgen
  • smd hot air station
  • my lab
  • yihua 853d
Related
Recommended

NexGen: The Lab: Found More Test Equipment: SMD Rework Station 853D

phoenixcomm
phoenixcomm
5 Feb 2021

This unit is most likely made by YIHUA.  The 853D is broken down into three functional blocks.image

  1. SMD Rework Wand. This has a digital temperature control and has interchangeable tips. image
  2. Solder Station Wand. This has a digital temperature control and it is removable via a 5-pin Din Plug. (I intend to buy a solder removal gun with vacuum)
  3. Power Supply (0-15vdc) with Digital Voltage Readout but set with a potentiometer. It also has an analog current meter.
  4. The Test Switch has two positions:
    1. The Test position is a  misnomer as in the Test position you can now use it as a DVM (volts only).
    2. Normal Power Supply output.

 

 

 

imageimage

Pinouts on ProsKit 33-331 Gun

between pins

1 & 2

500 ohms @
  room temp.

Heating Element

3 & 4

25 ohms @

  room temp.

Trigger

5 & 6

0 ohms

Trigger ON

Shaking Gun

7 & 2

0 ohms

Shaking Gun

 

image

 

 

 

Armed with this info it looks like the adapter will be cake.

 

I will also relocate the main power switch from the rear to the front.

 

Coupler for Gun to 853D Description
853DSS-332Adapter / Stand
Thermocouple +11n/a
Thermocouple -22

n/a

Heater33

Solid State Relay

Heater Pass through

Heater44
Ground2n/a
Trigger5

Triggers SS relay

normal relay for Vacuum.

Trigger6
Shaking7turn on/off SS Relay
Shaking2

 

 

 

 

 

 

 

Note the picture of the ProsKit Gun and the Rework Station are images from the net.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +1
    I am just not set up for working with these ity-bity components. DAB
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB +1
    DAB Dab, Me neither but I have a stereo 10x inspection microscope without a stand its nice for hand-holding. but when I get some more money I will get the unsoldering gun and that's what I really will…
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB

    DAB Dab, Me neither but I have a stereo 10x inspection microscope without a stand its nice for hand-holding. but when I get some more money I will get the unsoldering gun and that's what I really will use this for. Plus removal and soldering SMD components.  Its a pain to use the plunger thing to unsolder multi-layer boards. I have used the PACE system before and it is really nice but lots of $$$$$. And I can always use the hot air wand for heat shrink tubing. image This saves me from breaking out my Big Red Heat Gun.

    image

    ~~Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    I am just not set up for working with these ity-bity components.

     

    DAB