This is a copy of Scotts article that I found the picture of so called good soldering technique published in Import Tuner:
I then wrote scott this letter (email):
Scott - I was writing a page in my blog on element 14 entitled Soldering School and I was looking for some images demonstrating good technique. And that my friend is when I came across this picture:
1) When working with wires, you want a tip that is about as wide as the wire you will be working on. A little bigger or smaller is fine, but too small and you will have trouble heating up the wire quickly or at all. This in fact is bad advice, The tip should alway be smaller than your work you should never use a bigger tip. The tip should not control the heat of the iron, and if your iron is too hot with a large tip your solder will flow over the work but not envelope each strand, plus you might also melt the wire's insulation. 2) One more point shrink tubing is a good thing but only when It covers a good joint. 3) In between making connections and immediately after turning off the soldering iron, coat the tip with solder to protect it. Coating prevents the tip's protective metal coating from oxidizing and cracking or wearing away. Are you kidding me!! LOL. How in the world is a clean tip going to oxidize?? You should always have a tip cleaner around for removing the slick on the tip. I used to have a old school Ungar Imperial that I had since the 70's and still have most of the original tips! Let me see thats 40 years and the tips haven't oxidized away yet. 4) If you see the coating of solder on the tip discolouring and turning dull grey, add more solder to re-tin the tip. Nope not even close. First clean the tip with your sponge or tip cleaner, then you can apply fresh solder to the tip, and then wipe it off with the sponge. And then use a clean iron. 5) Clean up the solder with isopropyl alcohol or denatured alcohol to remove used flux when done soldering. Alcohol evaporates and dries quickly, does not leave impurities behind Ok, for the most part, yes, but no. The only way to clean the flux off the board or connection is to use a "flux remover" and a very stiff brush such and use the alcohol to remove any residues. BTW the irons that you show in this photo: Should be avoided like the plague. You can not control this irons temperature at the tip, as its only held in place with a screw, nor do you know about temperature recovery when you are done. You should keep them for your wood burning projects, or cut the chord off and toss the iron. And all metals discolours when you heat it..
|
NEW::= I just left a comment on his blog as it is restricted to 1024 I am enclosing the copy of my comment to him as well
|








Top Comments
-
anniel747
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
phoenixcomm
in reply to anniel747
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
phoenixcomm
in reply to anniel747
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children