Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Soldering School - part 1: an open letter to Scott Tsuneishi of Import Tuner
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 6 Mar 2013 5:57 AM Date Created
  • Views 933 views
  • Likes 5 likes
  • Comments 5 comments
  • soldering_iron
  • solder_wire
  • flight_simulation
  • soldering_tools
  • soldering_terminals
  • diy_cockpit
  • feature_tutorial
  • flux_removal
Related
Recommended

Soldering School - part 1: an open letter to Scott Tsuneishi of Import Tuner

phoenixcomm
phoenixcomm
6 Mar 2013

This is a copy of Scotts article that I found the picture of so called good soldering technique published in Import Tuner:

 

The most fundamental skill needed to assemble any electronic project is that of soldering. Basic soldering is a skill that's easy to learn and not too hard to master but misconceptions on the proper procedures also include many individuals having no clue on where to start.  Soldering is accomplished by quickly heating a metal or metallic alloy to join metallic surfaces together. A good soldering job can be rewarding while a poor job can lead to electrical failures and frustration. These steps will help improve soldering skills along with teaching you the basics and importance on how to perfect your soldering skills. Doing the job right the first time eliminates the need for costly rework.

image

 

1. Always use a quality soldering iron. We recommend an iron with a ceramic element core. Keep in mind that total power or wattage of the iron is less important than its thermal recovery ability. Thermal recovery is the ability of the iron to "recover" to proper temperatures immediately after soldering. Ceramic elements have been known to be better at maintaining proper temps. Although they are designed using lower wattage, they tend to heat much faster. A "cheap" soldering iron is usually constructed with a wire coil element. Wire coil units typically lose heat when used and are slow to recover from the initial temperature drop delaying usage. We recommend also refraining from using butane torch/battery-type soldering irons unless portability is crucial.

 

2. Proper solder tip sizes and shapes are very important in getting a good solder connection. When soldering wires, we prefer using the flat-tipped ones (sometimes called "spade tips"). Avoid the rounded conical tips, which are primarily used to repair or solder very small IC chips on PC boards.

When working with wires, you want a tip that is about as wide as the wire you will be working on. A little bigger or smaller is fine, but too small and you will have trouble heating up the wire quickly or at all.

 

3. Always use quality type/brand solder. For electronics, solder is traditionally comprised of a mixture of tin and lead.
Although 60/40-tin/lead solder is most commonly found on the market, we prefer 63/37 eutectic solder, which solidifies almost instantly. A 60/40 solder typically cools inconsistently as areas remain soft or semisolid once applied until fully cooled.image

 

4. Pre-tinning the wires or components (coat with a thin layer of solder) or fills the wires or connector contacts with solder so you can easily melt them together. It also prevents the need to hold heat to components for too long. Pre-tinning is accomplished by applying a thin layer of solder to the individual parts before fusing the wires together. When tinning wire, you want to make sure the solder flows all the way to the center, from the end of the wire to the edge of the insulation where you stripped it back.

 

5.image Use the right amount of solder; do not glob it on. More doesn't necessarily mean better. On the flip side, not using enough solder is just as bad, which can make the connection physically weak. A good solder joint will be smooth and shiny. If the joint is dull and crinkly, the wire probably moved during soldering and might require a do-over.

6. Keep your iron tip clean by wiping it off regularly with a damp sponge or rag both before and after making connections. A dirty tip can prevent your solder from making proper contact with the parts and can slow down heat transfer to components.

 

7. In between making connections and immediately after turning off the soldering iron, coat the tip with solder to protect it. The coating prevents the tip's protective metal coating from oxidizing and cracking or wearing away. If you see the coating of solder on the tip discoloring and turning dull gray, add more solder to re-tin the tip, or turn off the soldering iron if you will not be using it very soon (a discolored tip with a rainbow color pattern means the tip is too hot).

 

8. Clean up the solder with isopropyl alcohol or denatured alcohol to remove used flux when done soldering. Alcohol evaporates and dries quickly, does not leave impurities behind, will not corrode metal, and will not hurt electronics; whereas water can take days to dry and can corrode parts or leave impurities behind.

 

9. Lastly, use heat-shrink tubing to complete the soldering process to protect the wires.

image

 

I then wrote scott this letter (email):

 

Scott - I was writing a page in my blog on element 14 entitled Soldering School and I was looking for some images demonstrating good technique. And that my friend is when I came across this picture:  image
Your intention of writing the article might have been good... But my friend you should not try to talk about a subject that you know little or nothing about. If you look at the photo you can clearly see that the solder is touching the soldering iron:  That is a failure in good technique. The solder should never touch the iron when soldering the connection. The only time this is permissible is when you tin your iron, and then you must wipe it off in a damp sponge!
Here is a link you my blog article:  http://www.element14.com/community/people/phoenixcomm/blog/2013/02/25/soldering-school. You also made several other blunders:

 

1)  When working with wires, you want a tip that is about as wide as the wire you will be working on. A little bigger or smaller is fine, but too small and you will have trouble heating up the wire quickly or at all.

This in fact is bad advice, The tip should alway be smaller than your work you should never use a bigger tip. The tip should not control the heat of the iron, and if your iron is too hot with a large tip your solder will flow over the work but not envelope each strand, plus you might also melt the wire's insulation.

2)  One more point shrink tubing is a good thing but only when It covers a good joint.

3)  In between making connections and immediately after turning off the soldering iron, coat the tip with solder to protect it. Coating prevents the tip's protective metal coating from oxidizing and cracking or wearing away.

Are you kidding me!! LOL. How in the world is a clean tip going to oxidize?? You should always have a tip cleaner around for removing the slick on the tip. I used to have a old school Ungar Imperial that I had since the 70's and still have most of the original tips! Let me see thats 40 years and the tips haven't oxidized away yet.

4)  If you see the coating of solder on the tip discolouring and turning dull grey, add more solder to re-tin the tip.

Nope not even close. First clean the tip with your sponge or tip cleaner, then you can apply fresh solder to the tip, and then wipe it off with the sponge. And then use a clean iron.

5)  Clean up the solder with isopropyl alcohol or denatured alcohol to remove used flux when done soldering. Alcohol evaporates and dries quickly, does not leave impurities behind

Ok, for the most part, yes, but no. The only way to clean the flux off the board or connection is to use a "flux remover" and a very stiff brush such and use the alcohol to remove any residues.

image

BTW the irons that you show in this photo:  Should be avoided like the plague. You can not control this irons temperature at the tip, as its only held in place with a screw, nor do you know about temperature recovery when you are done. You should keep them for your wood burning projects, or cut the chord off and toss the iron. And all metals discolours when you heat it..

imageimage


Regards,
Cris Harrison
Fort Worth, Tx.

 

NEW::=  I just left a comment on his blog as it is restricted to 1024 I am enclosing the copy of my comment to him as well

phoenixcomm
3/7/2013 at 1:47 AM

Scott I wrote you an email with an open letter to you. This letter can be read at my Blog: http://www.element14.com/community/people/phoenixcomm/blog/2013/03/06/soldering-school-an-open-letter-to-scott-tsuneishi-of-import-tuner. This article was full of good intentions and just bad advice and really bad technique. The reason for this is the picture of the soldering iron and the wire as an example of "good technique" but it shows  a lack of understanding of what is happing. If you look at the picture you will see that the solder is in fact touching the iron. Major no-no. There where also other silly to almost stupid remarks in your article. Before you cry foul you should read the first blog of Soldering School and read the course work.
Regards
Cris Harrison, BSEE, BSCS
Phoenix Aerospace
Ret Air Force Crew Chief

  • Sign in to reply

Top Comments

  • DAB
    DAB over 13 years ago +1
    Hi Chris, Good update. As I stated before, good soldering skills are a must. Learn good techniques early and use them often. A sloppy soldering job is NEVER acceptable. Just my opinion, DAB
Parents
  • anniel747
    anniel747 over 1 year ago

    phoenixcomm First observation: his tentative at a Wrap Splice is not so good to start with and is twisted as a lefty.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to anniel747

     Anniel747, yes but that type of splice is not approved anymore!  Please see 

    Soldering School - part 3: The Cable Multi-Purpose Color Display (F/A-18C/D MPCD) This was not grade A work, but I did this just before leaving to Cockpit Fest!

    The solder splices are very inexpensive! The Chinese ones are too long so I cut them down. Certified  $7 - 10 EACH! :) there is a video so watch it! Never, Never use a lighter or torch of some Ilk! As the flame will burn and melt the PVC!!!Just use an approved heat gun. Go one of my websites www.electronics-workbench.com look at the tools section. ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to phoenixcomm

    phoenixcomm It is still approved in revision D (02/06/2024).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • anniel747
    anniel747 over 1 year ago in reply to phoenixcomm

    phoenixcomm It is still approved in revision D (02/06/2024).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to anniel747

     anniel747 It may be still approved but NOT recommended for harsh environments! ie Cars, Trucks, Heavy Equipment, Aircraft & boats. 

    here is the link from TE 

    *Meets performance requirements of SAE-AS83519 (formerly MIL-S-83519) and NAS 1747, supplied with BiAlloy temperature indicator. **Qualified to SAE-AS83519 (formerly MIL-S-83519), supplied with thermochromic temperature indicator. ***Meets performance requirements of SAE-AS83519 (formerly MIL-S-83519) and NAS 1747, supplied with thermochromic temperature indicator. ****Meets performance requirements of SAE-AS83519 (formerly MIL-S-83519), supplied with BiAlloy temperature indicator. Note: Cadmium-free option (B-152 series) is available for operating temperature of 125˚C [257˚F]. Consult TE for details.