Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Learning to 3D Print
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 29 Oct 2022 1:05 AM Date Created
  • Views 2658 views
  • Likes 11 likes
  • Comments 14 comments
  • 3d printer
  • Creality
  • Ender 3-Pro
  • filament
Related
Recommended

Learning to 3D Print

ntewinkel
ntewinkel
29 Oct 2022

I've had my 3D printer, a Creality Ender 3-Pro (from element14/Newark here), for a while, and I've printed random things like project cases, coins, and fun things with it.

The prints usually came out alright. especially when printing with the Creality PLA for which the Creality slicer has its own special settings.

When I first got the printer, I also picked up some ABS filament locally, second hand but still in air-tight wrap, but I was never able to get great prints with them. Usually they were ok, but never great. The Creality slicer has a "Generic ABS" setting I was using for it.
Fun side note: the ABS settings are hot enough to melt the magnetic mat that comes with the Ender 3-Pro! Let it cool down before trying to remove the print. So I have a new mat now Smile oops.

Then recently I was able to add a few extra colours to my filament collection, through a shopping cart prize here at element14. Those are all Multicomp brand PLA.

However; when I went to print with them I was unable to get anything even close to decent on my printer! That's when I realized that, even though they are all PLA, the temperature ratings are very different than the Creality version. Where my Creality filament is rated for 180-215, the Multicomp black is rated for 205-225 degrees C. No wonder it didn't work well!

So I realized that I need to take a step back and figure out what settings will work for me for each of these new filaments, before I try to print anything else with them. I watched a lot of videos on the subject too, and it seems that this is a highly recommended step anytime we get a new roll of filament, regardless of experience! Good to know.

Last night I posted a question in the 3D printing section (thank you for the help!).  Gough Lui and rsjawale24 shared some excellent knowledge and gave me some extra pointers on how to proceed.

I decided to blog my ongoing experimenting here, in case my journey might be helpful for others in the future. And also maybe something I might need to refer back to Slight smile

Re-Starting my 3D Printing Journey

I thought I'd start with the very first step again: printing the lucky cat that came pre-installed (in g-code format) on the SD card that came with the printer. When I first got the printer, I recall that cat printed out amazingly well - very clean, very detailed.

I printed it with the white Creality PLA (Print temp is marked as 180-215).
During printing the display says it's printing at 200 degrees, with bed at 45 degrees C, and FR (feed rate, I assume?) at 100%.

Ender 3Pro display for cat print

Room temperature by the printer is about 20 degrees.

And the print came out perfect! All the fine details too.
I don't know what kind of magic they are using, but I've never had any of my prints come out like that, even with the same material while specifically choosing "Creality PLA" on the Creality Slicer.

Creality Ender 3 Pro Lucky Cat 3D print

It did take almost 6 hours to print, and it's only 7cm tall.

ps, that PLA has always just been stored in a drawer - not in any airtight bag with desiccant. The art studio does tend to have generally nice dry humidity levels though.

Next Steps...

I'll try printing some little calibration cubes next, to see how that goes. Starting with Creality white as above, and then I'll try the new Multicomp black PLA.

Edit: turns out my problems were due to a cracked plastic extruder lever on my Creality Ender 3 Pro.

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 3 years ago in reply to rsjawale24 +1
    I'll give the Ultimaker one a try, thanks for the suggestion It looks like the MacOS Creality Slicer is Cura based (the old Windows one is very different) for the UI and g-code generator, but hopefully…
Parents
  • robogary
    robogary over 3 years ago

    Glad to see you have good luck with your first prints.  My 3D printer was like gold on its first print, with great success with the example code provided. Mine was a small elephant. The first few prints did OK for me, then continually downgraded to the point where the 3D printer stays in a closet now. I havent found a good  simple freeware modeling tool , and I cant get the prints to stick to the plate or layer nicely anymore, no matter what I've tried. Cleaning the extruder helped, but didnt solve the not sticking to the bed. I wonder how to evaluate when a nozzle is worn out, or if the filament is the root cause. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to robogary

    I feel your pain! None of this was in the brochure!

    My first ever print went horribly wrong because I had no idea that I had to clean the build plate with alcohol first Face palm There was zero quick-start getting-started information provided. You'd think they would at least give some newbie step-by-step instructions on how to print the provided sample.

    >I havent found a good  simple freeware modeling tool
    I haven't really done any modelling - I mostly just find things on Thingiverse. Luckily there are others needing enclosures for boards that I use!
    That's a whole other learning curve I don't think I'm ready for yet.
    I did modify a jar lid once. I think I used Tinkercad to cut and paste pieces around.

    Have you tried printing the starter elephant again?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 3 years ago in reply to ntewinkel

    Tinkercad is a good training tool. I'd done a couple designs there which are useful on my projects. I always search Thingiverse first for a solution or a starting place. Im amazed at the talent and patience of the folks that can build the models. Engineers make a good career of building cad models , so for sure its a highly skilled talent that takes alot of practice. 

    I havent retried printing the elephant. :-) The 3d printer is magic.....when it works. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 3 years ago in reply to ntewinkel

    Tinkercad is a good training tool. I'd done a couple designs there which are useful on my projects. I always search Thingiverse first for a solution or a starting place. Im amazed at the talent and patience of the folks that can build the models. Engineers make a good career of building cad models , so for sure its a highly skilled talent that takes alot of practice. 

    I havent retried printing the elephant. :-) The 3d printer is magic.....when it works.