Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Pump Monitoring Win
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 14 Aug 2018 10:20 PM Date Created
  • Views 1410 views
  • Likes 13 likes
  • Comments 10 comments
  • monitor
  • wemos d1
  • pump
  • iot
Related
Recommended

Pump Monitoring Win

ntewinkel
ntewinkel
14 Aug 2018

The good news is: My little Wemos D1 based pump monitor works!

 

The bad news is: The anomaly detected by my pump monitor was real and required physical labour to correct image

 

 

In a nutshell - You might recall that I had a WiFi temperature sensor set up for my hummingbird feeder during the winter. It is based on an ESP-01 module, and I used it to take regular temperature readings and send it to my server. From there I could then see the graph of the temperature.

 

Earlier in the year we had a pump station failure, in that the pump stayed on too long. Luckily we were outside near the tank when it happened and we heard the gurgling of the pump running dry. We had to dig it out and jiggle the sensor (it's a depth sensor, but they said it can get gummed up with stuff stuck on it), and it worked again. I raised it up an inch to give some clear space under it.

 

I realized that in all failure cases the pump stays on too long. In this case the depth sensor was reporting deeper than real liquid levels and so the control panel failed to turn the pump off = on too long. In the case where the pump itself fails the control panel would provide it power but it would not pump out enough to hit the off level = on too long. Log files showed that before the previous pump failure (and tank alarm) the pump had intermittently run longer than was usual.

 

So I used the different parts that make up the WiFi temperature sensor, and modified it slightly to become a pump monitor instead.

 

This is what it looks like (it's in my basement/crawlspace) - I soldered on a resistor and a light sensor on a long lead (cat-5 wires).

imageimage

And this is how I placed the sensor above the LED on the panel:

image

 

I had a WeMos D1 available, so I used that - it's much easier to use than the ESP-01, as it has a micro-USB port on it that I can use to program it, and I can also use it to provide power from a small 5v USB iPhone charger cube.

Instead of a temperature sensor I instead used a light sensor, which I placed near the little red LED "pump on" light on the control panel.

The scripts on the server are also very similar to the temperature one - it logs the readings "on" and "off" into a simple file, and the server adds timestamps.

 

Because I also wanted to know how long the pump runs each time, the Arduino program counts the number of seconds between the light sensor detecting light and then detecting that the light is off again.

This also gets sent to the server.

 

To make monitoring more real-time, I added a piece to the script that sends me a text message for each event (using the email-to-text feature my cell provider includes in my package).

 

I quickly noticed that the pump is always on for about 2:07 (minutes:seconds), give or take 5 seconds. So I added some code for the WeMos to send warning updates to the server if the pump stays on for longer than 5 minutes (I will be reducing that down to 3 minutes soon).

 

So I've been happily receiving comforting text messages for the last handful of months since that first incident, until this weekend - of course while I was away on a mini-vacation.

 

This is what I usually see. Very comforting:

image

 

And here is when I knew the pump controller needed attention, not comforting at all! but good to know it works:

image

 

You'll noticed the top few are 02:04 and 02:08, which is very much along the lines of what I've been getting since I set that up... but then uh-oh!

The pump stayed on for over 10 minutes! EEEP! Luckily it turned off by itself or I would have needed to drive home to deal with it (we were staying overnight on the mountain - about 40 minutes away).

 

When we got back later that day the pump did a proper run again, but then hiccuped again the next day.

 

So today we dug it out again (luckily the lid is only a few inches under dirt) - and this time I pulled the sensor out of the tank completely and cleaned it up to where the panel reported it properly as 0.0 inches again. And I raised it up a few more inches just in case the tank gets too much sediment and gums it up again.

Turns out the sensor was reporting the level as 12" when in reality it was down to about 3 or 4".

I'm not very happy with this expensive control panel the plumber installed 4 years ago - it was supposed to be much more reliable, but it turns out to be the opposite! I kinda think this sensor issue caused the previous pump to fail after only 3 years (just after warranty - boo!). The good old fashioned float switches don't care about a bit of goo on them.

If it comes time to replace it, I'll definitely go back to float switches! With my little DIY IoT monitor as a safety backup image

So now we're running some laundry to get the liquid level in the tank up to above the sensor, to make sure that the sensor does report proper numbers and that the pump controller does properly pump out the tank again. The bright side of that is that I don't have to do more shovelling until that part is proven image

 

So, while it was a lot of effort to clear things up again, we realized that without my little IoT monitor we would not even have known about this issue! It might have caused us yet another premature pump failure from constantly running it dry!

 

So a definite Win for the DIY tech here!

And my wife no longer makes fun of me receiving text messages from my septic pump image

 

I'll probably add a redundant low-level float switch, which the control panel has room for, so in the future it at least won't run dry.

The panel tech support guy also suggested I could expand my little DIY device to use a relay to emulate the redundant low-level float! Great idea - seeing as it already counts the minutes I could quite easily have it send the 3 minute warning while at the same time shutting off the pump.

 

Cheers,

-Nico

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +5
    The nice thing about self engineered devices is that you can usually go right to the problem and fix them. The bad thing about self engineered devices is that you may be the only person who can fix them…
  • ntewinkel
    ntewinkel over 8 years ago in reply to jw0752 +4
    Thanks John! As I recall, you had a similar win with your automatic water shut-off and alarm, right? > The bad thing about self engineered devices is that you may be the only person who can fix them. In…
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1 +4
    Ours is a sewer lift station - we have city sewer at the edge of the property, but it's higher than the ground level by the house. > Looks like you now need the ability to remotely turn it off as well…
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    Ours is a sewer lift station - we have city sewer at the edge of the property, but it's higher than the ground level by the house.

     

    >Looks like you now need the ability to remotely turn it off as well.

    Yep! I realized that as I was up on the mountain looking at the text messages image

    I'm home 99.9% of the time, but Murphy's law got me again!

     

    Luckily, I did already have a remote power switch available, which I can control from my phone from anywhere, so I've added that to the control panel plugin.

    Hopefully I won't need it! But in the meantime it'll track how much power that control panel is using image

     

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    Looking at the manual and other info, it seems the sensor uses pressure to determine the tank level.

    http://www.sjerhombus.com/wp-content/uploads/2018/06/EZ-Connect-User-Guide.pdf

    https://www.sjerhombus.com/products/c-level-sensor/

     

    The fact it can be thrown off by debris would suggest that it needs a fine filter around it to prevent it from being blocked.

    The instruction suggests placement 1 inch above the bottom OR sludge. The sludge level could build up and eventually make it fail again.

     

     

    You could use a standard water filter to allow the fluid to be filtered before the actual level (and pressure) acts on the sensor.

    The bottom should be sealed and the top sealed around the sensor body.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    Nice work.

    Looks like you now need the ability to remotely turn it off as well.

     

    Our septic system uses a float switch in the final chamber to pump out the fully processed liquid to the disposal field.

     

    The irrigation controllers here tend to use a float switch down the well to detect there is water, and then a phase detection system to detect the loading on the submersible pump, or alternatively a pressure switch to ensure the pump is actually pumping water (otherwise they overheat).

     

    I wonder if you can add a pressure switch?

    I'd tend to use a bladder so that the switch is not on contact with the liquid.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to jw0752

    Thanks John! As I recall, you had a similar win with your automatic water shut-off and alarm, right?

     

    >The bad thing about self engineered devices is that you may be the only person who can fix them.

    In this case the part that needed fixing/cleaning was the control panel's liquid level sensor in the tank, unfortunately. I kinda wished it was a silly edge case in my own device!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago

    The nice thing about self engineered devices is that you can usually go right to the problem and fix them. The bad thing about self engineered devices is that you may be the only person who can fix them. Thanks for sharing your adventure with us,

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<