element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • About Us
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Remote Desktop for Avnet SmartEdge IIoT
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 20 Feb 2021 3:39 AM Date Created
  • Views 1030 views
  • Likes 2 likes
  • Comments 3 comments
  • iiot
  • avnet
  • gui
  • smartedge
  • ssh
  • raspberry pi
  • remote desktop
  • gateway
Related
Recommended

Remote Desktop for Avnet SmartEdge IIoT

ntewinkel
ntewinkel
20 Feb 2021

Note: this is still a work in progress...

At this point, I'm still only seeing a black screen when I connect using Remote Desktop.

I also tried the RealVNC player: https://help.realvnc.com/hc/en-us/articles/360002249917-VNC-Connect-and-Raspberry-Pi#setting-up-your-raspberry-pi-0-0

 

The other issue I'm running into is that my mouse/keyboard doesn't work when I start the GUI (using startx).

 

Edit: Feb 23 update: I have decided to re-flash the firmware and start over. NOTE that Avnet has just released the new version 1.3 firmware, so I recommend going straight to that.

 

My Avnet SmartEdge IIoT has just been sitting on my desk since my initial evaluation of it, and I thought it was about time I put it to good use.

 

Given that at its heart this unit is a Raspberry Pi, my plan is to use it for things I've been using an older Raspberry Pi for, like my OpenSprinklerPi controller, as well as for some new things I would like to try out, which includes things like receiving and storing data from various WiFi sensors around the house and displaying them graphically in a browser.

 

Being an industrial Gateway, this unit didn't have to fit the tight budget of a regular Raspberry Pi and seems to be a much better overall build.

It has a nice solid design with what appears to be a good stable power supply as well as a sizeable heatsink.

It also uses eMMC flash rather than an SD card, and all of it is enclosed in a professional looking case.

I expect it will be a more reliable setup than a regular Raspberry Pi.

 

But to get there, I first need to get things set up to where I can comfortably work with it.

For me, that includes setting it up with the GUI environment and Remote Desktop.

 

I'll try to summarize the steps I took here.

I'm writing this after the fact, so I may be missing details, but it should serve as a guide in case I or someone else needs to do this in the future.

 

For many of these steps, you will find what you need right here on element14: SmartEdge Industrial IoT Gateway Solution - Connects to Innovate

 

1. Update to the newest Avnet firmware.

Jan Cumps has created a great tutorial for this: AVNET SmartEdge IIOT Gateway: the 2020 Linux Image and IoTConnect Scripts

These steps will update the SmartEdge from the original firmware to a more stable version, and also allow for recovery in case things stop working.

Note: Make sure you add the ssh file as per his suggestion.

 

Edit Feb 23:

Note Also: Use the latest firmware, v1.3 as of Feb, 2021. Without this you won't be able to provision the SmartEdge.

 

Edit Feb 23:

Remember to use the Avnet IoTConnect App to provision the SmartEdge!

This seems to be required to be able to use SSH.

 

-> At this point, I was using a monitor and keyboard connected to the Avnet for the first few steps. That's a bit of a hardware juggle pain for me, so it's best to get an ssh connection ASAP.

Part of the problem was that I had either forgotten to add the ssh file, or ran into some issues trying to do that.

For that case:

 

1.5: Enable SSH

Start the SmartEdge with monitor and keyboard.

Remember that the default username is avnet, with password avnet.

Now add the ssh file into the boot folder:

cd /boot

sudo touch ssh

For the following steps, I used an old article I wrote back in 2015 as a guide. Most of the steps still apply.

Connecting to a Remote Desktop on the Raspberry Pi

 

2. Find the IP address of the SmartEdge.

ifconfig

Then restart:  (I'm pretty sure this is required for ssh to start up, but I could be wrong)

sudo shutdown -r now

note: it looks like you can now also simply use

sudo reboot

and to shutdown:

sudo poweroff

But I've found "sudo reboot" to take much longer than the shutdown command.

 

--> After restart you should be able to ssh to the SmartEdge. From my Mac that looks like:

ssh avnet@192.168.2.2

but use the IP address you found by using ifconfig.

Then login and you can comfortably work with your regular keyboard and monitor in a Terminal window.

 

3. Give the SmartEdge a new name (default is RaspberryPi)

To check the existing name:

hostname

Edit the file to update the name:

sudo nano /etc/hostname

I renamed mine to be "smartedge"

 

4. Update the Raspberry Pi system

For the rest of the updates, the system needs the usual Raspberry Pi updates. So let's run that now:

The SmartEdge manual, on page 27, includes the steps for installing the desktop GUI.

See: https://www.element14.com/community/servlet/JiveServlet/previewBody/93279-102-2-385720/Avnet%20SmartEdge%20IIoT%20Gatewa…

 

It says to set certain system files on hold, but that seems to already be in place with the new firmware, as the apt-mark hold commands all return the message "xxx was already set on hold."

sudo apt update

sudo apt upgrade

sudo apt dist-upgrade

ps, Note the use of "apt" instead of "apt-get" - from what I've read, these commands do the same thing but the newer "apt" makes things more "pleasant" - I've noticed the progress bar is nice to have, for example.

 

5. Add Bonjour to allow access using the hostname in the form of smartedge.local instead of the IP address

sudo apt install avahi-daemon

 

6. Install the desktop GUI

sudo apt install --no-install-recommends xserver-xorg xinit

sudo apt install raspberrypi-ui-mods

I didn't install the Chrome browser, and because I'm not using a directly connected monitor I don't want to boot to GUI at startup, so I skipped those steps.

 

I already had Microsoft Remote Access installed on my Mac (you can reference my 2015 article if you need that), so at this point I added the SmartEdge to the list.

For the settings, I set the PC name to "smartedge.local", making use of the name provided by the Bonjour service, to avoid issues with the dynamic IP address given to it by the router.

If you set the username (avnet) and password (avnet) right away, it will automatically login when you open a session.

For the display I tend to just set it to 1920x1080 and "fit session to window" because I have a 4k monitor, but you can choose whatever works best for you.

 

At this point you can clean up unused packages:

sudo apt clean

 

7. Turn off boot-to-GUI

Since I plan to use this SmartEdge via Remote Desktop, it doesn't make sense to start it up into the GUI.

Use raspi-config to turn that off:

sudo raspi-config

 

Set it to log in to the command line (not autologin).

Exiting raspi-config, say yes to "reboot now".

 

8. Enable VNC using raspi-config

sudo raspi-config

Then choose Interfacing Options and VNC

 

9. Install xrdp

sudo apt install xrdp

10. Re-install vnc4server again to avoid interference with RealVNC

sudo apt install vnc4server

 

Maybe reboot one last time...

 

Now we should be able to ssh to the SmartEdge, and we should also be able to use Remote Desktop to access it with a GUI interface.

 

Happy Computering,

-Nico

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 4 years ago +1
    The ssh file in the boot root is in case you prepare the OS and there is no keyboard and screen to connect. You typically do that right after flashing the OS, before first startup. When the disks are still…
  • ntewinkel
    ntewinkel over 4 years ago in reply to Jan Cumps +1
    ah ok, that's easier than the manual method. I might re-flash the SmartEdge and start over again. I'm not even sure if I need GUI and/or Remote Desktop. Maybe I'll try on a regular RPi first to rule out…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to ntewinkel +1
    I always use headless, on Pi, BB and other Linux small devices. They can run a desktop, and there are some reasons to use it (E.g.: when you build an end user interface with the HDMI). But however you…
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    The ssh file in the boot root is in case you prepare the OS and there is no keyboard and screen to connect.

    You typically do that right after flashing the OS, before first startup. When the disks are still available on the host pc you used for flashing.

    SSH will then be available at first boot.

     

    In the other case, when you have a keyboard and screen attached when starting up the box first time, you can directly use raspi-config to enable ssh.

    It's one of the menu options.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago

    The ssh file in the boot root is in case you prepare the OS and there is no keyboard and screen to connect.

    You typically do that right after flashing the OS, before first startup. When the disks are still available on the host pc you used for flashing.

    SSH will then be available at first boot.

     

    In the other case, when you have a keyboard and screen attached when starting up the box first time, you can directly use raspi-config to enable ssh.

    It's one of the menu options.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 4 years ago in reply to Jan Cumps

    ah ok, that's easier than the manual method.

     

    I might re-flash the SmartEdge and start over again. I'm not even sure if I need GUI and/or Remote Desktop.

    Maybe I'll try on a regular RPi first to rule out any issues due to specific differences.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to ntewinkel

    I always use headless, on Pi, BB and other Linux small devices.

    They can run a desktop, and there are some reasons to use it (E.g.: when you build an end user interface with the HDMI).

    But however you toss and turn it, they are not powerful enough to be a desktop PC or graphical development system. They aren't sized for that.

     

    I've always aimed to build good graphical development environments on more powerful devices (laptops, PCs) to do the development. And to learn how to cross-compile and debug.

     

    The Pis and SmartEdges are strong enough to serve sophisticated services, such as Node-RED, databases, REST, ....

    But as a core development system with an IDE they fall flat on the belly. Even as plain build system they lack the oomph.

     

    My approach is that when one of my children complains their laptop is too slow and they need a better one, they have to give the old one back to me.

    I install Linux on them (laptops, not children) and they serve as development and build hubs (and one as a blockchain testbed) for many more years. With a desktop.

    • Cancel
    • Vote Up +1 Vote Down
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.