Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog JQ6500 MP3 Player
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 26 Sep 2021 6:54 PM Date Created
  • Views 21165 views
  • Likes 1 like
  • Comments 13 comments
  • seeeduino xiao expansion board
  • seeeduino xiao
  • jr6001
  • jq6500
  • mp3 player
Related
Recommended

JQ6500 MP3 Player

ralphjy
ralphjy
26 Sep 2021

I recently saw a discussion by Sean Conway about an MP3 Player that he was attempting to control: Looking for member insight into the JR6001 Serial MP3 Custom Programmable Sound Recorder Module .

 

That inspired me to try out a similar module - the JQ6500 https://www.amazon.com/gp/product/B01N47M1V2/ref=ppx_yo_dt_b_asin_title_o00_s00?ie=UTF8&psc=1 .  I'll have to admit that I chose this one because it was available on Amazon Prime and I could get it in a couple of days.  These are much cheaper if you source them from China, but I don't have the patience to save a few dollars image.  And there is also a contributed Arduino library for the module.

 

These modules have their sound files loaded into flash over USB and they are configured and controlled via serial UART.  There is a built in power amplifier that can drive a speaker directly.  The other feature of this particular module is that there are 5 dedicated pins that can be used to select 1 of 5 sound files just by pulling the pin low.  Seems like something that would be useful to add sound to projects.

 

image

 

image

 

image

 

Pin Type

Pin Description

K1

Playback of Audio 1

K2

Playback of Audio 2

K3

Playback of Audio 3

K4

Playback of Audio 4

K5

Playback of Audio 5

SGND

Ground

ADKEY

AD port

BUSY

Play Indicator

RX

UART serial Data input

TX

UART serial data output

GND

Ground

VCC

5V power supply

ADC_R

Headphones/Amplifier(Right Channel)

ADC_L

Headphones/Amplifier(Left Channel)

SPK-

Speaker -

SPK+

Speaker +

I just received my modules from Amazon today.  I've decided that since they are controlled via UART that I would use a Xiao with and expansion board to make the hookup easy.  I'll also probably use the display sometime in the future.

Here's a picture of my setup - the JQ6500 is on the breadboard at the bottom:

image

 

Electronics from China frequently have issues and these modules were no exception.  I connected a module to the USB port and discovered that it was not flashed.

image

 

Of course, no mention of this possibility or how to fix it in the documentation.  Luckily, this is apparently a common issue and I found a tutorial on how to flash the unit: JQ6500, recover a broken / unreadable module .  A little time and a small amount of pain later, I had flashed both of my modules and had access to the file loader over USB.

image

image

 

My first attempt to load MP3 files failed because the module only has 4 MB of flash for storage and most of the MP3 files I have around are larger than that.  I downloaded a free "Ukulele" music file from bensound.com and loaded that (about 2 minutes duration - 2 MB).

 

The module has 5 dedicated pins that allow you to play the first 5 stored tracks just by pulling the pin low or to Ground.  I tried grounding the K1 pin and was rewarded with music image.

 

To use the UART control, I'm using an Arduino library by James Sleeman: https://github.com/sleemanj/JQ6500_Serial .  I modified the Full Demo example to run on the Xiao.  I am using the hardware Serial1 port as the UART to the module.

 

Xiao_JQ6500_FullDemo.ino

/** Full demo of MP3 Controls, after uploading, open your Serial Monitor and enter commands.
 * 
 * Allows you to test all the various controls of the JQ6500 module.
 *
 * @author James Sleeman,  http://sparks.gogo.co.nz/
 * @license MIT License
 * @file
 * 
 * Modified by Ralph Yamamoto for Xiao plus expansion board
 * 
 */

#include <Arduino.h>
#include <JQ6500_Serial.h>
#include <SPI.h>
#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>

#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 64 // OLED display height, in pixels

// Declaration for an SSD1306 display connected to I2C (SDA, SCL pins)
#define OLED_RESET     -1 // Reset pin # (or -1 if sharing Arduino reset pin)
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, OLED_RESET);

// Create the mp3 module object, 
//   Use Serial1

JQ6500_Serial mp3(Serial1);

void setup() {
  // put your setup code here, to run once:
  Serial.begin(9600);
  Serial1.begin(9600);

  display.begin(SSD1306_SWITCHCAPVCC, 0x3C);
  display.clearDisplay();
  display.display();
    
  mp3.reset();
  statusAndHelpOutput();
}

void loop() {
  
    byte b;
    if(Serial.available())
    {
      b = Serial.read();

      switch(b)
      {
        case 'p': Serial.println("Play");   mp3.play();     return;
        case 'r': Serial.println("Restart"); mp3.restart(); return;
        case ' ': Serial.println("Pause"); mp3.pause();     return;
        case '>': Serial.println("Next");  mp3.next();      return;
        case '<': Serial.println("Prev");  mp3.prev();      return;
        
        case ']': Serial.println("Next Folder");  mp3.nextFolder(); return;
        case '[': Serial.println("Prev Folder");  mp3.prevFolder(); return;
    
        case '+': Serial.println("Vol +"); mp3.volumeUp(); return;
        case '-': Serial.println("Vol -"); mp3.volumeDn(); return;
        case 'm': Serial.println("Vol 0"); mp3.setVolume(0); return;
        
        case 'v': 
        {
          char volBuff[10]; 
          memset(volBuff, 0, sizeof(volBuff));          
          Serial.readBytesUntil('\n',volBuff, sizeof(volBuff)-1);
          mp3.setVolume(max(0,min(30, atoi(volBuff))));
          
          Serial.print("Vol ");
          Serial.println(max(0,min(30, atoi(volBuff))));                    
        }
        return;

        case 'e':
        {
          do
          {
            while(!Serial.available()); // Wait
            b = Serial.read();
            if(b != ' ') break; // Allow "e N" or "eN" etc...
          } while(1);
          
          Serial.print("Equalizer ");
          switch(b)
          {
            case 'N': Serial.println("Normal");  mp3.setEqualizer(MP3_EQ_NORMAL);  break;
            case 'P': Serial.println("Pop");     mp3.setEqualizer(MP3_EQ_POP);     break;
            case 'R': Serial.println("Rock");    mp3.setEqualizer(MP3_EQ_ROCK);    break;
            case 'J': Serial.println("Jazz");    mp3.setEqualizer(MP3_EQ_JAZZ);    break;
            case 'C': Serial.println("Classic"); mp3.setEqualizer(MP3_EQ_CLASSIC); break;
            case 'B': Serial.println("Bass");    mp3.setEqualizer(MP3_EQ_BASS);    break;
          }
        }
        return;

        case 'l':
        {
          do
          {
            while(!Serial.available()); // Wait
            b = Serial.read();
            if(b != ' ') break; // Allow "e N" or "eN" etc...
          } while(1);
          
          Serial.print("Loop ");
          switch(b)
          {
            case 'A': Serial.println("All"); mp3.setLoopMode(MP3_LOOP_ALL);      break;  // Plays the tracks one after another and repeats 
            case 'F': Serial.println("Folder"); mp3.setLoopMode(MP3_LOOP_FOLDER);       break; // Loop within folder
            case 'O': Serial.println("One (repeat playing same file)"); mp3.setLoopMode(MP3_LOOP_ONE);       break; // | These seem to do the same, repeat the same track over and over
            case 'R': Serial.println("??? - Don't know what it means exactly, in the datasheet it is \"RAM\""); mp3.setLoopMode(MP3_LOOP_RAM);       break; //- 
            case 'N': 
            case 'S': Serial.println("None (play file and stop)"); mp3.setLoopMode(MP3_LOOP_ONE_STOP); break;  // Default, plays track and stops
          }
        }
        return;

        case 's':
        {
          do
          {
            while(!Serial.available()); // Wait
            b = Serial.read();
            if(b != ' ') break; // Allow "e N" or "eN" etc...
          } while(1);
          
          Serial.print("Source ");
          switch(b)
          {
            case 'S': Serial.println("SD Card (if available)."); mp3.setSource(MP3_SRC_SDCARD);      break;
            case 'B': Serial.println("on board memory.");mp3.setSource(MP3_SRC_BUILTIN);   break;            
          }
        }
        return;

        case 'f':
        {
          char fnumBuff[10]; 
          memset(fnumBuff, 0, sizeof(fnumBuff));          
          Serial.readBytesUntil('\n',fnumBuff, sizeof(fnumBuff)-1);
          unsigned int fnum = strtoul(fnumBuff, NULL, 10);

          Serial.println();
          Serial.print("Play file #");
          Serial.print(fnum);
          Serial.println(F(" (if it exists)."));
          mp3.playFileByIndexNumber(fnum); // 48 == ord('0')   
          return;
          
        }
        return;
        
        case 'F':
        {
          char fnumBuff[10]; 
          memset(fnumBuff, 0, sizeof(fnumBuff));          
          Serial.readBytesUntil('/',fnumBuff, sizeof(fnumBuff)-1);
          unsigned int folnum = strtoul(fnumBuff, NULL, 10);
          
          memset(fnumBuff, 0, sizeof(fnumBuff));          
          Serial.readBytesUntil('\n',fnumBuff, sizeof(fnumBuff)-1);
          unsigned int fnum = strtoul(fnumBuff, NULL, 10);
          
          fnum   = max(1,min(fnum, 999));
          folnum = max(1,min(folnum, 99));
          
          Serial.print("Play "); 
            if(folnum < 10) Serial.print('0');
          Serial.print(folnum);
          Serial.print('/');
            if(fnum < 10) Serial.print("00");
            else if(fnum < 10) Serial.print('0');
          Serial.print(fnum);
          Serial.println(".mp3 (if it exists).");
          mp3.playFileNumberInFolderNumber(folnum, fnum); // 48 == ord('0')   
        }
        return;
                  
        case '?': statusAndHelpOutput(); return;
        
        case 'S': Serial.println("Sleep"); mp3.sleep(); return;
        case 'z': Serial.println("Reset"); mp3.reset(); return;
        
      }
      
    }
    
    static unsigned long m = millis();
    
    if(millis() > 1000 && m < (millis() - 1000))
    {
      if((mp3.getStatus() == MP3_STATUS_PLAYING))
      {
        Serial.print(F("Playing, Current Position: "));
        Serial.print(mp3.currentFilePositionInSeconds());
        Serial.print(F("s / "));
        Serial.print(mp3.currentFileLengthInSeconds());       
        Serial.println('s');
      }
      m = millis();
    }  
}

void statusAndHelpOutput()
{
   Serial.println();
   Serial.println(F("JQ6500 MP3 Player Demo"));
   Serial.println(F("~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~"));
   
   Serial.print(F("Status           : "));
   switch(mp3.getStatus())
   {
     case MP3_STATUS_STOPPED: Serial.println(F("Stopped")); break;
     case MP3_STATUS_PLAYING: Serial.println(F("Playing")); break;
     case MP3_STATUS_PAUSED:  Serial.println(F("Paused"));  break;
   }
   
   Serial.print(F("Volume (0-30)    : "));
   Serial.println(mp3.getVolume());
  
   Serial.print(F("Equalizer        : "));
   switch(mp3.getEqualizer())
   {
     case MP3_EQ_NORMAL:     Serial.println(F("Normal"));  break;
     case MP3_EQ_POP:        Serial.println(F("Pop"));     break;
     case MP3_EQ_ROCK:       Serial.println(F("Rock"));    break;
     case MP3_EQ_JAZZ:       Serial.println(F("Jazz"));    break;
     case MP3_EQ_CLASSIC:    Serial.println(F("Classic")); break;
     case MP3_EQ_BASS:       Serial.println(F("Bass"));    break;     
   }
   
   Serial.print(F("Loop Mode        : "));
   switch(mp3.getLoopMode())
   {
     case MP3_LOOP_ALL:      Serial.println(F("Play all tracks, then repeat."));  break;
     case MP3_LOOP_FOLDER:   Serial.println(F("Play all tracks in folder, then repeat."));     break;
     case MP3_LOOP_ONE:      Serial.println(F("Play one track then repeat (loop track)."));    break;
     case MP3_LOOP_RAM:      Serial.println(F("Unknown function exactly, seems to play one track then repeat?"));    break;
     case MP3_LOOP_ONE_STOP: Serial.println(F("Play one track then stop."));    break;          
   }
   Serial.println();
    
   Serial.print(F("# of On Board Memory Files    : "));
   Serial.println(mp3.countFiles(MP3_SRC_BUILTIN));
       
   Serial.print(F("\"Current\" On Board Memory File Index: "));
   Serial.println(mp3.currentFileIndexNumber(MP3_SRC_BUILTIN));
   Serial.println();
   
   Serial.print(F("# of SD Card Files    : "));
   Serial.println(mp3.countFiles(MP3_SRC_SDCARD));
   
   Serial.print(F("# of SD Card Folders  : "));
   Serial.println(mp3.countFolders(MP3_SRC_SDCARD));
   
   Serial.print(F("\"Current\" SD Card File Index: "));
   Serial.println(mp3.currentFileIndexNumber(MP3_SRC_SDCARD));
   
   Serial.print(F("\"Current\" SD Card File Name : "));   
   char buff[120];
   mp3.currentFileName(buff, sizeof(buff));
   Serial.println(buff);
   
   Serial.println();
   Serial.println(F("Controls (type in serial monitor and hit send): "));
   Serial.println(F("~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~"));
   Serial.println(F("? Display this menu.\n"));
   
   Serial.println(F("p Play\t\t> Next\t\t< Prev\n[space] Pause\tr Restart from start of file\n] Next folder\t[ Prev folder\n"));
   
   Serial.println(F("f[1-65534]      Play file by (FAT table) index number\nF[01-99]/[001-999].mp3 Play [001-999].mp3 in folder [01-99]\n"));
   
   Serial.println(F("+ Vol up\t- Vol down\tm Mute\nv[0-30] Set volume\n\ne[N/P/R/J/C/B] Equalizer (N)ormal, (P)op, (R)ock, (J)azz, (C)lassic, (B)ass\nl[A/F/O/R/N]   Loop (A)ll, (F)older, (O)ne, (R)???, (N)o Loop\ns[S/B]         Switch to (S)D Card/(B)uilt In Memory\n\n"));
}

 

Here's a short list of the most commonly used commands:

        case 'p': Serial.println("Play");   mp3.play();     return;

        case 'r': Serial.println("Restart"); mp3.restart(); return;

        case ' ': Serial.println("Pause"); mp3.pause();     return;

        case '>': Serial.println("Next");  mp3.next();      return;

        case '<': Serial.println("Prev");  mp3.prev();      return;

   

        case ']': Serial.println("Next Folder");  mp3.nextFolder(); return;

        case '[': Serial.println("Prev Folder");  mp3.prevFolder(); return;

 

        case '+': Serial.println("Vol +"); mp3.volumeUp(); return;

        case '-': Serial.println("Vol -"); mp3.volumeDn(); return;

        case 'm': Serial.println("Vol 0"); mp3.setVolume(0); return;

 

The program output is displayed on the Serial Monitor and commands are entered into the Serial monitor and relayed to the module through the UART.

 

Here's a demo playing the "Ukulele" song:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

When I have time later, I'll add a keypad (or pushbuttons) and display functions.  I think for some of my projects I'll just use it preconfigured and standalone, just using the pins to play individual files.

 

Sean was trying to use his modules by issuing control sequences directly over the UART without the benefit of a library.  I think that might be a fun thing to try with a serial terminal...

 

 

Update 09/27/2021

I forgot to include this link to the components101 website that has a detailed module description and a link to the PDF spec that I'm using.  Just in case others have not found it yet.

https://components101.com/modules/jq6500-mp3-player-module-pinout-features-datasheet-working-application-alternative

  • Sign in to reply
Parents
  • fmilburn
    fmilburn over 5 years ago

    Hi Ralph,

     

    Thanks for posting.  I checked to see if 2MB was enough for the little animatronics I'm doing and it looks sufficient.  For example, Bender has 1.3MB of sound files.  I ordered two JQ6500 modules today to try out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to fmilburn

    Don't forget to check out that repair link as you'll probably have to flash your modules.  I did it exactly as he described using a VM.

     

    I didn't actually try to test the maximum capacity, so I'm not actually sure how much of that 4 MB is available. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 5 years ago in reply to fmilburn

    Don't forget to check out that repair link as you'll probably have to flash your modules.  I did it exactly as he described using a VM.

     

    I didn't actually try to test the maximum capacity, so I'm not actually sure how much of that 4 MB is available. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 5 years ago in reply to ralphjy

    I tried installing it twice and it fails with the same message:

    image

    I've checked to make sure it is pointing at the .iso and I also tried using Rufus to put it on a USB stick but Rufus said it didn't recognize the format of the iso.  So maybe I am using the wrong file?

     

    The .iso file I am using is located here: JQ6500-rescue-tool/ISO at master · NikolaiRadke/JQ6500-rescue-tool · GitHub

     

    I notice it has a slightly different name than what is shown in the video.  Is that the same one you are using and did you have to install anything else besides VMware and point to the .iso file?  I'm bound to be doing something wrong...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to fmilburn

    Hi Frank,

     

    Yes, I am using the file jq6500-rescue-linux.iso (the older file was called jq6500-rescue-tool.iso).  I believe either file should work, but the newer one does not ask you to select the flash memory size.

     

    I followed the directions in this blog - http://www.lucadentella.it/en/2018/04/11/recuperiamo-un-modulo-jq6500/ .   I think I may have linked the YouTube video that was in Italian instead of English (sorry, but I think you figured it out).

     

    The blog was a bit dated so he used the old filename and was using VMware Workstation 14, but the rest of the instructions applied in terms of getting the iso to run.  The toolkit menu he used was for the old file.

     

    It seems that you may have set up your VM incorrectly, so you should check that you used the steps in the blog.

     

    Here are my VM settings.  You can see that the CD/DVD uses the ISO image.

    image

     

    And the menu when the VM powers on.

    image

     

    I didn't do anything extra that I can recall.  Maybe you should try downloading your ISO again.  Your VM seems to be complaining about no OS.

     

    Here are the two files that I downloaded.

    image

     

    I did not try using Rufus or a live CD.

     

     

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to ralphjy

    Thanks Ralph,

     

    That is really helpful.  It will probably be tomorrow evening before I can get back to this but will post how it comes out then.  If I can figure out where I went wrong I will post that also as a trap to avoid for others.

     

    Frank

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to ralphjy

    Thanks Ralph,

     

    Got it working.  I downloaded a new copy of the ISO and left it in my download folder (before I moved it to a new more permanent folder) when using VMware.  Everything worked fine after that.  I noticed you left it in your download folder as well. It seems like I've moved ISO files around before on my hard drive without issue, but maybe not.  Always best to follow the directions exactly when you don't know what you are doing :-)

     

    Frank

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to fmilburn

    Glad that you got it working.  The file must have gotten corrupted when you moved it.  I hadn’t moved it out of laziness I suppose...  I imagine I should get better organized in case I buy more of these.  Of course, if I wait too long they won’t be available anymore image.

     

    Ralph