Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Preparing to add a laser to my CNC router
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Nov 2019 4:38 PM Date Created
  • Views 2797 views
  • Likes 9 likes
  • Comments 5 comments
  • genmitsu cnc 3018-pro
  • laser engraving
Related
Recommended

Preparing to add a laser to my CNC router

ralphjy
ralphjy
7 Nov 2019

Earlier this year I got a low cost CNC router to complement my 3D printing capabilty.  The Genmitsu 3018 Pro is a great low cost router with a working volume of 300mm x 180mm x45mm and it also has the option on its controller board to use a PWM output to control a laser module (actually has 2 connector ports).  The diameter of the spindle clamp would allow it to use common 30mm x 30mm laser modules without any modification.  So, with the addition of a laser module and LaserGRBL software I could do laser engraving and cutting,  I'm thinking that will be my Christmas present from Santa this year.

image

 

I had an exchange of messages with shabaz and Fred27  about laser safety and decided that before I get my laser module that I should get some safety equipment.  Here's what I decided to get.

 

Safety Equipment

  1. Protective eyewear
  2. Fire extinguisher
  3. Remote monitor

 

Protective eyewear

I took Shabaz's recommendation and got the LS02 Safety Glasses from Edmund Optical.  I am going to get a laser in the 450 - 500nm range and these glasses are rated with an Optical Density >7 @ 180 - 532nm.

image

 

This particular model fits over my prescription glasses.  I like that the working range is marked on the front of the lens.

image

image

image

Link:  https://www.edmundoptics.com/p/arg-lasershield-safety-glasses/41399/

 

 

Fire extinguisher

I'm still looking for a small CO2 extinguisher because the dry chemical ones make too much of a mess.  I'll probably need to find an industrial supplier.

 

 

Remote monitor

I decided to mount a Pan/Tilt IP camera on the ceiling so that I could monitor the laser from the adjacent room on a computer or mobile device.  The pan and tilt capability also lets me monitor other activity in the workroom like when I am using the 3D printer.  I put presets in the camera for a wide view and also zoomed in views of the CNC router and the 3D printer.

image

A short video showing the preset views:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Warning light?

The other feature that I've considered is a warning light outside the door of the workroom to indicate that the laser is in operation.  That may be overkill for a home setup

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +4
    Very nice. This is really safety first, buying the safety equipment before Santa deliveries your gift.
  • dubbie
    dubbie over 6 years ago +4
    It is good to see safety being seriously considered with lasers as it only takes one mistake. Eyes don't heal well after a lasering. An alternative approach would be to put the laser cutter inside a box…
  • shabaz
    shabaz over 6 years ago +3
    Hi Ralph, Nice reminder about the extingusher, I need to get one too. The camera set-up is very cool! That style of glasses fits really well, I could not tell that there are prescription glasses behind…
Parents
  • dubbie
    dubbie over 6 years ago

    It is good to see safety being seriously considered with lasers as it only takes one mistake. Eyes don't heal well after a lasering. An alternative approach would be to put the laser cutter inside a box, possibly with a camera inside, or a protective glass view area. This also has the advantage of providing better control over the fume extraction as it is better to get a laminar flow of air away from the cutting point. Otherwise the fumes can re-condense back onto the surface and cause unsightly marks, especially when cutting plastics. The fumes can also be toxic so you have to get rid of those safely as well.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    That’s a good point about ventilation.  I’m planning to see how well the solder fume extractor I have will work (it has a filtering system).  If it gets overwhelmed, I may need to add some active venting.  The unit is about 10 feet from a window.

     

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    That’s a good point about ventilation.  I’m planning to see how well the solder fume extractor I have will work (it has a filtering system).  If it gets overwhelmed, I may need to add some active venting.  The unit is about 10 feet from a window.

     

    Ralph