Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Raspberry Pi Zero 2 W - MotionEyeOS
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 22 Nov 2021 4:44 PM Date Created
  • Views 45653 views
  • Likes 5 likes
  • Comments 13 comments
  • rpi camera v2.1
  • raspberry pi zero 2 w
  • video streaming
  • MotionEyeOS
  • motion eye
Related
Recommended

Raspberry Pi Zero 2 W - MotionEyeOS

ralphjy
ralphjy
22 Nov 2021

This is my first post on the new site, a follow-up to I've Got To Get Me One Of These!

I'll have to admit that navigating the new site software and structure has been challenging, so it will be interesting if this works out...

I naively had thought that I could swap Raspbian OS SD cards between a RPi Zero W and Zero 2W - and that does work if you start with a recent version of the OS that knows what a Zero 2W is.  Of course, I was trying an SD card from an older Zero W - so that did not work.

I also wanted to try the MotionEyeOS on the Zero 2W since I've used that with the Zero W.  Unfortunately, the latest released image version is from last year - 20200606 - and that did not work.  I had hoped to see if I could get about the same performance as an RPi 3.

There's a lot of info on how to build your own update to MotionEyeOS, but I wasn't up to the challenge.  There was also the suggestion to install MotionEye (non-OS on the RaspbianOS, but luckily I found that "jawsper" had built a version of MotionEyeOS that would run on the Zero 2W: MotionEyeOS_RPi_Zero_2W.   For my inaugural blog, I'm going to try that out.

Here is the Zero 2W with the camera in the official Raspi case.  I 3D printed a clip so that I could tripod mount it.  The power to the microUSB is from a power adapter, but I think I'll use a USB power bank to make it portable.

image

This is the MotionEye Console with the image preview and the video settings below that.  I set the resolution to 800x600 and the framerate to 15 FPS.

image

image

And a short video streaming to a different browser window - there is a slight bit of lag.  

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I'll post this and hope that the video converted ok.

  • Sign in to reply
Parents
  • steviep
    steviep over 4 years ago

    Thank you for sharing I've have it up and running with record video only 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • steviep
    steviep over 4 years ago

    Thank you for sharing I've have it up and running with record video only