Documents elf14 presents - The Test and Measurement Tool Bundle Giveaway
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 18 Nov 2020 3:44 PM Date Created
  • Last Updated Last Updated: 26 Jan 2021 9:28 AM
  • Views 10568 views
  • Likes 20 likes
  • Comments 194 comments
Related
Recommended

elf14 presents - The Test and Measurement Tool Bundle Giveaway

image
The Test and Measurement Tool Bundle Giveaway!

Engineer and Maker Wishlist | Circuit Assembly Tools Giveaway! | Test and Measurement Giveaway! | Ultimate Raspberry Pi Giveaway! | Project14 Holiday Special

 

 

Unsupported video URL format.

 

Welcome to the elf14 element14 Community!

 

It's the season of gift-giving, so the element14 Community has prepared the Best Test and Measurement Tool Bundle to giveaway!

 

The below kit will be awarded to the element14 members that add a comment and let us know:

 

What was your first test or measurement tool?

Why that tool? How did it help you, what project did you use it on? Do you still have it in your collection or on your bench, or has it since been replaced?

 

Contest Opens: 27th November 2020

Contest Closes: 30th December 2020

Winners Announced: After 11th January 2021

 

 

What We Gave Away!

 

Product NameManufacturerQuantityBuy KitBuy Kit
Handheld Digital OscilloscopeMulticomp Pro1Buy NowBuy Now
Handheld Digital MultimeterMulticomp Pro1Buy NowBuy Now
Humidity MeterMulticomp Pro1Buy NowBuy Now
Test Lead, 4mm Banana Plug, Stackable, Alligator Clip, 60 VDC, 10 A, Black, 304.8 mmMulticomp Pro1Buy NowBuy Now
Test Lead, 4mm Banana Plug, Stackable, Alligator Clip, 60 VDC, 10 A, Red, 304.8 mmMulticomp Pro1Buy NowBuy Now
Test Lead, Alligator Clip, Alligator Clip, 60 VDC, 10 A, Black, 304.8 mmMulticomp Pro1Buy NowBuy Now
Test Lead, Alligator Clip, Alligator Clip, 60 VDC, 10 A, Red, 304.8 mmMulticomp Pro1Buy NowBuy Now
TEST LEAD KIT, 12 PIECEMulticomp Pro1Buy NowBuy Now
TEST LEAD KIT, 10 PIECEMulticomp Pro1Buy NowBuy Now

 

Congratulations to the Winner!

 

nathandumont has been chosen, and they have managed to get in touch!

 

It would have been unfair to deny the prize due to technical problems, thank you to everyone for entering!

 

Terms and Conditions apply.

  • elf14 presents
  • holiday season 2020
  • holiday season
  • elf14presents_wishlist
  • giveaway
  • test and measurement tool bundle giveaway
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 5 years ago +12
    I remember when I was just starting in college I decided that I was building enough electronics that I needed a Volt-Ohm-Milliammeter (VOM) of my own and I bought a Knight Kit from Allied Electronics and…
  • dubbie
    dubbie over 5 years ago +10
    When I started with electronics I was probably only 16 or 17 and managed for several years without any test equipment at all. Obviously, not much of my stuff worked as I had no method of finding faults…
  • genebren
    genebren over 5 years ago +10
    I was always in a hurry to grow up and get a 'real job'. I completed High School in three years and college in three years. While in High School, I spent nearly half of my time in the Electronics Lab …
Parents
  • hugohu
    hugohu over 5 years ago

    My first instrument was a Commercial Electric multimeter. It's pretty low cost, it has a rugged case. My parents got it for me 2 years ago. It's right next to me- I use it whenever I need to poke some leads around. For my current purposes it's fine, even though it's not the most advanced.

     

    Oscillscope? No, I don't have one hehe, but I do plan on getting one if I need it.

     

    Back to the question. What did I use it on? Well, I used it then mostly to detect if a wire was soldered correctly(I was terrble at soldering then), and uesd it to make some small blinky lights. NOt the most effective nor the most practical use case but it did work.

     

    Currently? I'm still using it to detect traces, but now it's for fine pitch SMD components! I used it just the other day with my 1 Meter Of Pi project, when I thought my HAT wasn't receiving power.

     

    Why a multimeter? Well, my parents told me, "this is going to be very useful". And useful it was. It could detect voltages, it could detect current, etc. It's also extremely helpful for loose resistors.

     

    The question doesn't ask, but I'm just going to answer a question of what I would do with this.

     

    For the multimeter- I'd replace my current. It probably doesn't have a significant level of enhanced features, not the most advanced, but it does have bluetooth which would be probably able to connect to my phone, or other bluetooth enabled device. This allows me to potentially monitor readings without being in front of the device.

     

    For the oscilloscope- if I am the lucky winner, that would save me money. I would really appreciate an oscillscope with good features and bandwidth being added to my toolkit- there would be a lot of possibilities opened up with such a powerful device. And it's also a portable one that's smaller, which is suitable for my rather messy desk.

     

    Humidity meter:I frankly don't have too much use for this at the moment but I suppose I could put it near my workbench to monitor readings.

     

    While the chances of me being picked are extremely slim, if I am the lucky winner that would be extremely beneficial to myself and my projects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hugohu
    hugohu over 5 years ago

    My first instrument was a Commercial Electric multimeter. It's pretty low cost, it has a rugged case. My parents got it for me 2 years ago. It's right next to me- I use it whenever I need to poke some leads around. For my current purposes it's fine, even though it's not the most advanced.

     

    Oscillscope? No, I don't have one hehe, but I do plan on getting one if I need it.

     

    Back to the question. What did I use it on? Well, I used it then mostly to detect if a wire was soldered correctly(I was terrble at soldering then), and uesd it to make some small blinky lights. NOt the most effective nor the most practical use case but it did work.

     

    Currently? I'm still using it to detect traces, but now it's for fine pitch SMD components! I used it just the other day with my 1 Meter Of Pi project, when I thought my HAT wasn't receiving power.

     

    Why a multimeter? Well, my parents told me, "this is going to be very useful". And useful it was. It could detect voltages, it could detect current, etc. It's also extremely helpful for loose resistors.

     

    The question doesn't ask, but I'm just going to answer a question of what I would do with this.

     

    For the multimeter- I'd replace my current. It probably doesn't have a significant level of enhanced features, not the most advanced, but it does have bluetooth which would be probably able to connect to my phone, or other bluetooth enabled device. This allows me to potentially monitor readings without being in front of the device.

     

    For the oscilloscope- if I am the lucky winner, that would save me money. I would really appreciate an oscillscope with good features and bandwidth being added to my toolkit- there would be a lot of possibilities opened up with such a powerful device. And it's also a portable one that's smaller, which is suitable for my rather messy desk.

     

    Humidity meter:I frankly don't have too much use for this at the moment but I suppose I could put it near my workbench to monitor readings.

     

    While the chances of me being picked are extremely slim, if I am the lucky winner that would be extremely beneficial to myself and my projects.