Polls What do you think is the best Single board Computer in the market?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 31 Mar 2016 8:12 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 2370 views
  • Likes 1 like
  • Comments 40 comments
Related
Recommended

What do you think is the best Single board Computer in the market?

There are too many options to choose from now. There is no right or wrong answer here. Please tell us why in the comments section below.

 

I have created this document so that we can compare all the SBCs in one place. Please edit it and add information on the SBCs you know about for the benefit of the community.

 

Comparison of SBCs in the market.

  • rasberry pi
  • single board
  • best
  • computers
  • beagle bone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +5
    Reference: http://wiki.pine64.org/index.php/Main_Page For USD 39.00 + shipping, the Pine A64+ (see details at reference) + 2GB DDR3 RAM, WiFi, 10/100/1000 Mbps Ethernet RJ45, and Bluetooth. No GPS built…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rsc +3
    Yo Scott! I hear ya. I have been assembling Mini-ITX systems for folks since their inception; small is beautiful. I am still running a Zotac IONITX-F-E (Dual-core Intel Atom 1.6GHz + Nvidia ION graphics…
  • rachaelp
    rachaelp over 10 years ago +3
    There are so many options and the "best" really does depend on what your project requirements are. For the same person the best may well change a lot depending on the design requirements for what they…
Parents
  • rachaelp
    rachaelp over 10 years ago

    There are so many options and the "best" really does depend on what your project requirements are. For the same person the best may well change a lot depending on the design requirements for what they are working on at the time.

     

    A really nice tiny embedded ARM board running Linux that I came across a little while ago is the Arietta G25 by ACME Systems: Arietta G25 - Low cost Linux embedded module

     

    It has a 400MHz ARM9 and it's the tiny form factor and pure stripped back to the bare minimum that I like about this. I have a project I am working on where this will be ideal for my initial prototypes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    rachaelp - What is the nature of the project?  Given the G25 specs, I would guess an engineering or science interfacing application.  Which O/S distro are you going to use or are you going to bootstrap an app on your own?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to e14 Contributor

    Hi Richard,

     

    It's a networked monitoring / control application and it needs to interface to other cards in the system via a LIN bus which was another reason for looking at that processor. This particular board will only be used for a lab based prototype but to get me going quickly and evaluate the processor, the final design will have the processor designed into the main board and will give me access to the Ethernet port. I'll just run the linux distro I can download from them for the prototype but will likely do something completely stripped back and customised for the final design, I've not looked too much into that yet.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rachaelp
    rachaelp over 10 years ago in reply to e14 Contributor

    Hi Richard,

     

    It's a networked monitoring / control application and it needs to interface to other cards in the system via a LIN bus which was another reason for looking at that processor. This particular board will only be used for a lab based prototype but to get me going quickly and evaluate the processor, the final design will have the processor designed into the main board and will give me access to the Ethernet port. I'll just run the linux distro I can download from them for the prototype but will likely do something completely stripped back and customised for the final design, I've not looked too much into that yet.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    My reading assignment: https://en.wikipedia.org/wiki/Local_Interconnect_Network#LIN_protocol

     

    That articlereminded me of the 1970s Bisynchronous 3270 multi-drop (master/slave polling) protocol with one-byte frame identifiers that was so common back then.  Even the max speed (20 kbit/sec) is about the same as the old days.  Of course, the hardware today is more reliable and less expensive.

     

    So, this is an automobile network application?  Do you work for a manufacturer or a 3rd party?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    Not to beat this subject into the ground but I just saw a working Arduino-based application as a LIN protocol analyzer:

     

         Master === Arduino === Slave 1 === Slave 2 .....

     

    See https://github.com/zapta/linbus

    Arduino would be an excellent low-cost tool for the job.