Polls What do you think is the best Single board Computer in the market?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 31 Mar 2016 8:12 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 2370 views
  • Likes 1 like
  • Comments 40 comments
Related
Recommended

What do you think is the best Single board Computer in the market?

There are too many options to choose from now. There is no right or wrong answer here. Please tell us why in the comments section below.

 

I have created this document so that we can compare all the SBCs in one place. Please edit it and add information on the SBCs you know about for the benefit of the community.

 

Comparison of SBCs in the market.

  • rasberry pi
  • single board
  • best
  • computers
  • beagle bone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +5
    Reference: http://wiki.pine64.org/index.php/Main_Page For USD 39.00 + shipping, the Pine A64+ (see details at reference) + 2GB DDR3 RAM, WiFi, 10/100/1000 Mbps Ethernet RJ45, and Bluetooth. No GPS built…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rsc +3
    Yo Scott! I hear ya. I have been assembling Mini-ITX systems for folks since their inception; small is beautiful. I am still running a Zotac IONITX-F-E (Dual-core Intel Atom 1.6GHz + Nvidia ION graphics…
  • rachaelp
    rachaelp over 10 years ago +3
    There are so many options and the "best" really does depend on what your project requirements are. For the same person the best may well change a lot depending on the design requirements for what they…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    My reading assignment: https://en.wikipedia.org/wiki/Local_Interconnect_Network#LIN_protocol

     

    That articlereminded me of the 1970s Bisynchronous 3270 multi-drop (master/slave polling) protocol with one-byte frame identifiers that was so common back then.  Even the max speed (20 kbit/sec) is about the same as the old days.  Of course, the hardware today is more reliable and less expensive.

     

    So, this is an automobile network application?  Do you work for a manufacturer or a 3rd party?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonyboubady
    tonyboubady over 10 years ago

    For me, i want to try every one of that and use according to my spec needs for various projects...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to e14 Contributor

    Hi Richard,

     

    It's a networked monitoring / control application and it needs to interface to other cards in the system via a LIN bus which was another reason for looking at that processor. This particular board will only be used for a lab based prototype but to get me going quickly and evaluate the processor, the final design will have the processor designed into the main board and will give me access to the Ethernet port. I'll just run the linux distro I can download from them for the prototype but will likely do something completely stripped back and customised for the final design, I've not looked too much into that yet.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    P.S. If you are ever going into a conventional build project such as ATX, Micro-ATX, Mini-ITX, or Mini-STX and you can specify an application (E.g. one of workstation, file server, or HTPC), then I would be able to make some recommendations for you.

     

    In general:

    • File servers typically need wired Ethernet connections, minimal graphics, and probably no audio.  What (eSATA/EIDE/USB) storage will be used?
    • Workstations need graphics and audio.  What level of quality is desired for both?
    • HTPCs also need graphics and audio.  HDMI to a high definition TV is normally used for Video.  Audio too or will audio pipe into a separate device like a sound system of some sort?

     

    I should stop there.  There are a lot of personal preference and usage questions to answer regardless of the application.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    There will never be a better, best or greatest.

     

    The technology is changing too fast and everyone's requirements determine which is most appropriate for the project.

     

    I learned many decades ago, that you can use just about any MCU on a project if you know how to use it properly.

    Timing issues aside, you can always create a system using any MCU that will do the project.

    Consider it like you would a hammer.  You have many different types to use, but as long as you are just pounding nails, they all pretty much do the job.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    You said above that Mini-ITX is too large for your purposes.  Look up.

     

    Most folks at this site would be bored with a blog on selecting the best Mini-ITX as they are understandably into very small footprints (very different from 17 × 17 cm form factor) or they are already experts with more traditional computer assembly.  However, which Mini-ITX (or any other mobo/SBC) you need depends on your purpose.  One type does not fit all.  It is very personal.

     

    There are many DIY guides/forums on-line for DIYers like Tom's Hardware (http://www.tomshardware.com/ ) and AnandTech (AnandTech: Hardware News and Tech Reviews Since 1997 ).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rachaelp

    rachaelp - What is the nature of the project?  Given the G25 specs, I would guess an engineering or science interfacing application.  Which O/S distro are you going to use or are you going to bootstrap an app on your own?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks a lot. This is the kind of information only experienced users can help us out with.

     

    It would be helpful if you can write an article on selecting the best mini ITX for your application for a noob like me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    ooh. I've seen these. But these are too large for my applications. I'll go for them at a later time when required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    One word of warning about Intel "Cedar Trail" GMA mobos (https://en.wikipedia.org/wiki/Intel_GMA) like the Intel ATOM MUD and MUD2 boards: Intel, the graphics supplier, Imagination Technologies (PowerVR), and the various Linux distro communities  do not support Linux on them.  Hence, one has to settle for a buggy form of vanilla VGA graphics.

     

    An example of one of these non-Linux mobos is the "Intel D2700 MUD".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>