Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog A simple DIY Oscilloscope with Arduino Uno and Mega
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Dec 2014 11:05 AM Date Created
  • Views 39400 views
  • Likes 20 likes
  • Comments 79 comments
  • mega
  • ardbeginner
  • tft
  • oscilloscope
  • uno
  • arduino
Related
Recommended

A simple DIY Oscilloscope with Arduino Uno and Mega

e14 Contributor
e14 Contributor
26 Dec 2014

My DIY Oscilloscope, how i got my signal image

 

Content :

- Description

- Screenshots

- Video

- Credits and links

 

Descriptions

 

I am experimenting with RF and IR signals in various frequencies and had some trouble with the receivers and needed to see what kind of signal i was receiving.

I cannot afford a real oscilloscope but i knew about the older Arduino oscilloscopes.

 

After trying many different versions of code and tutorials, I was unable to get a single one to work, and all the tutorials and guides around was 2-3 years old.
Not sure if it is the IDE or the actual hardware that has changed in such a way that it didn't work anymore.

 

I finally found a working oscilloscope from a Japanese website, (linked below) and a working TFT screen library,

meaning i could read the various signals received.

 

Clearly the limitations are 0-5v but that is fine, what i needed to know is either wave type and frequency, and this is sufficient.
It also gives me an indication of the amplitude which is just a nice bonus.

 

But what I'm most happy with, is the two channel feature, i often use the second channel as a reference point to be able to

differentiate the main channel on the screen.

 

 

Some screenshots..

This is the .96" OLD test, single wave test imageimage

 

 

 

imageimageimage

2.4" TFT screen on the Uno,    two right images same screen on a Mega.

 

 

A youTube vidoe i made on the experience.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Credits and Links :

 

My compilation of the Oscilloscope and TFT library  ( what you see on the video and images ) :

https://dl.dropboxusercontent.com/u/19761809/arduino/Vaupell-Oscilloscope.zip

 

 

Original Oscilloscope link (code by : Noriaki Mitsunaga ) :

http://n.mtng.org/ele/arduino/oscillo-j.html

 

 

Original TFT display link ( TFT shield library source ) :

http://www.smokeandwires.co.nz/blog/a-2-4-tft-touchscreen-shield-for-arduino/

 

TFT library :

Library : https://github.com/Smoke-And-Wires/TFT-Shield-Example-Code

Attachments:
Vaupell-Oscilloscope.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to 4ringfan +2
    True, I highly recomened if using ribbon cable, buy a roll, and add the ends yourself, much much cheaper. I usually buy them home in 10 meters at a time. But, I try to use cable as little as possible,…
  • 4ringfan
    4ringfan over 11 years ago +1
    I just received a LCD TFT shield that I had ordered for no particular reason. Now I'm going to have to play with it. Thanks for the incentive!
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    Nope just one of them. The problem was the Screen it took up all my pins on the arduino uno. You could do a messy workaround, either by soldering something onto the SD pins (since were not using them anyway…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    Thank you for the info, I will compile as you pointed out and see how it goes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago

    It is a really good work. Well done with great results!

     

    if I can give you an advice, I suggest that you hosts - at least - the sources on GitHub (now that gitorious has died) so the other users has no problem to download the stuff in the format they prefer, browse it before and many other advantages than using the dropbox.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Mike,

     

    to be sure beyond any doubt you should check - excluding the comment lines - if the two .h files are the same. Then, if they are, it is very probable that the two libraries are the same.

     

    Best.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    This is kind of a basic question but I too the .ino file provided in the .zip file and compiled it, it says that there are couple of missing files/libraries, I have to include them separately right?

     

    By the way the library TFTLCD.h is the same as Adafruit_TFTLCD.h right?

     

    Thx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 11 years ago in reply to niq_ro

    niq_ro as dmaruska said

    Try a DIFFERENT zip/UNzip software....

    I used peazip - free to download.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>