Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Arduino Nano RP2040 Connect - MQTT
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 12 Jun 2021 7:17 PM Date Created
  • Views 9989 views
  • Likes 8 likes
  • Comments 10 comments
  • mqtt
  • arduino nano rp2040 connect
  • u-blox nina 102 module
  • mbed
  • rp2040
Related
Recommended

Arduino Nano RP2040 Connect - MQTT

ralphjy
ralphjy
12 Jun 2021

I wanted to test connecting the Nano RP2040 Connect to my RPi4 MQTT server by publishing temperature and humidity data from a BME280 sensor.  I figured that this should be fairly easy since I've already used the BME280 with another RP2040 board - the SparkFun Pro Micro RP2040 and I've used my MQTT server with multiple ESP32 devices.

 

Of course, the devil is in the details...

 

I stayed within the confines of the Arduino IDE hoping that it would makes things simpler, and it did, but new board variants are coming out an incredible pace so things are still a mess.

 

The Nano RP2040 Connect is supported as arduino mbed_nano hardware and the Pro Micro RP2040 is supported as rp2040 hardware using the board library contributed by Earle Philhower.

 

The first problem I ran into was with the Wire library.  I was using functions to set the I2C pins that are not included in the mbed Wire library (Wire.setSDA(I2C_SDA), Wire.setSCL(I2C_SCL)).  I had used these functions to designate the QWIIC connector pins on the Pro Micro RP2040.  In mbed you need to instead do that as part of the interface declaration MbedI2C I2C(I2C_SDA, I2C_SCL).  Since I'm not using a connector this time, I just used the default I2C pins (i.e. removed the function calls).

 

The second problem that I ran into is that the Pro Micro uses the WiFi library and the Nano RP2040 Connect uses the WiFiNINA library.  I was setting up a static IP addr using the WiFi.config function and the WiFiNINA version of that function uses a different parameter order.  And the WiFiNINA function is also a Void rather than Bool (i.e. doesn't return a value).

 

For the WiFi library the function is WiFi.config(ip, gateway, subnet, dns).

For WiFiNINA library the function is WiFi.config(ip, dns, gateway, subnet).

 

The final problem was that I am using the dtostrf function to convert integers to strings for MQTT and I couldn't figure out what to include for mbed (it is supposed to be "mbed/dtostrf.h").  After struggling for a while, I took the easy way out and just added the function code to the sketch.

 

After fixing all that, it is working...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Nano_RP2040_Connct_BME280_MQTT.ino

/*
 *  Created on: 06.11.2021
 *  
 * the arduino_secrets.h file:
 * #define SECRET_SSID ""    // network name
 * #define SECRET_PASS ""    // network password
 * #define SECRET_MQTT_USER "public" // broker username
 * #define SECRET_MQTT_PASS "public" // broker password 
 *  
 *
 */

#include <Arduino.h>
#include <stdio.h>
//#include "mbed/dtostrf.h"
#include <WiFiNINA.h>
#include <PubSubClient.h>
#include "arduino_secrets.h"
#include <Wire.h>
#include "Adafruit_Sensor.h"
#include <Adafruit_BME280.h>

#define USE_SERIAL Serial

// LED Pin
const int ledPin = LED_BUILTIN;

// Add your MQTT Broker IP address, example:
//const char* mqtt_server = "192.168.1.144";
const char* mqtt_server = "10.0.0.234";

// Set your Static IP address
IPAddress local_IP(10, 0, 0, 207);
// Set your Gateway IP address
IPAddress gateway(10, 0, 0, 1);

IPAddress subnet(255, 255, 255, 0);
IPAddress primaryDNS(8, 8, 8, 8);   //optional
IPAddress secondaryDNS(8, 8, 4, 4); //optional

WiFiClient rp2040Client;
PubSubClient client(rp2040Client);
long lastMsg = 0;
char msg[50];
int value = 0;

Adafruit_BME280 bme;

float tempBME = 0.0;
float humBME = 0.0;

char *dtostrf (double val, signed char width, unsigned char prec, char *sout) {
  char fmt[20];
  sprintf(fmt, "%%%d.%df", width, prec);
  sprintf(sout, fmt, val);
  return sout;
}

void setup() {
    USE_SERIAL.begin(115200);
//    while(!USE_SERIAL);
    delay(500);

    USE_SERIAL.println();
    USE_SERIAL.println();
    USE_SERIAL.println();
    
    if (!bme.begin(0x76)){  
        USE_SERIAL.println("Could not find a valid BME280 sensor, check wiring!");
        while (1);
    }    

    setup_wifi();
    client.setServer(mqtt_server, 1883);
    client.setCallback(callback);
  
    pinMode(ledPin, OUTPUT);
    digitalWrite(ledPin, LOW);
}

void setup_wifi() {
  delay(10);
  // We start by connecting to a WiFi network
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(SECRET_SSID);

  WiFi.config(local_IP);

  WiFi.begin(SECRET_SSID, SECRET_PASS);

  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }

  Serial.println("");
  Serial.println("WiFi connected");
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());
}

void callback(char* topic, byte* message, unsigned int length) {
  Serial.print("Message arrived on topic: ");
  Serial.print(topic);
  Serial.print(". Message: ");
  String messageTemp;
  
  for (int i = 0; i < length; i++) {
    Serial.print((char)message[i]);
    messageTemp += (char)message[i];
  }
  Serial.println();

  // Feel free to add more if statements to control more GPIOs with MQTT

  // If a message is received on the topic floor2/output, you check if the message is either "on" or "off". 
  // Changes the output state according to the message
  if (String(topic) == "rp2040connect/output") {
    Serial.print("Changing output to ");
    if(messageTemp == "on"){
      Serial.println("on");
      digitalWrite(ledPin, HIGH);
    }
    else if(messageTemp == "off"){
      Serial.println("off");
      digitalWrite(ledPin, LOW);
    }
  }
}

void reconnect() {
  // Loop until we're reconnected
  while (!client.connected()) {
    Serial.print("Attempting MQTT connection...");
    // Attempt to connect
    if (client.connect("RP2040Client")) {
      Serial.println("connected");
      // Subscribe
      client.subscribe("rp2040connect/output");
    } else {
      Serial.print("failed, rc=");
      Serial.print(client.state());
      Serial.println(" try again in 5 seconds");
      // Wait 5 seconds before retrying
      delay(5000);
    }
  }
}

void loop() {
    if (!client.connected()) {
      reconnect();
    }
    client.loop();
  
    long now = millis();
    if (now - lastMsg > 30000) {
      lastMsg = now;
    
      tempBME = bme.readTemperature()*1.8 + 32 - 5;
      humBME = bme.readHumidity() + 7;
  
      // Convert the value to a char array
      char tempString[8];
      dtostrf(tempBME, 1, 2, tempString);
      Serial.print("Temperature: ");
      Serial.println(tempString);
      client.publish("rp2040connect/temperature", tempString);
  
      // Convert the value to a char array
      char humString[8];
      dtostrf(humBME, 1, 2, humString);
      Serial.print("Humidity: ");
      Serial.println(humString);
      client.publish("rp2040connect/humidity", humString);
    }
        
    delay(1000);
}

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 5 years ago in reply to ralphjy +2
    From what I read (at so many places I couldn't keep track), dtostrf() is an AVR specific library (Atmel 328 etc.), and avr/dtostrf is a work-around for the M0, M4 chips. And then we get to these mbed boards…
  • cstanton
    cstanton over 5 years ago in reply to ralphjy +2
    Feedback and Support is for problems with the site. Experts would be a better place to post
  • mp2100
    mp2100 over 5 years ago +1
    I appreciate the reviews of these new boards. And: good coding tip. I was using dtostrf on my lora board and it’s not supported everywhere, and I got stuck. Your programming skills are better than mine…
Parents
  • mp2100
    mp2100 over 5 years ago

    I appreciate the reviews of these new boards.  And: good coding tip.  I was using dtostrf on my lora board and it’s not supported everywhere, and I got stuck.  Your programming skills are better than mine, I will bookmark your code.

    (dtostrf function to convert integers to strings)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to mp2100

    Thanks for the compliment, but I literally just copied the library code.  I just haven't figured out what file I need to include to pick up that function.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to ralphjy

    So, I dug a little deeper and in the bowels of the mbed_nano installation I found a reference to a deprecated function:

     

    C:\Users\Ralph\AppData\Local\Arduino15\packages\arduino\hardware\mbed_nano\2.1.0\cores\arduino\api\deprecated-avr-comp\avr\dtostrf.h(28): char *dtostrf(double val, signed char width, unsigned char prec, char *sout);

     

    I added the following include and can now pick up the function. 

     

    #include <avr/dtostrf.h>

     

    I guess I could play around and figure out how to reference it in the mbed_nano path, but why bother.  I'm not sure why this is deprecated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mp2100
    mp2100 over 5 years ago in reply to ralphjy

    From what I read (at so many places I couldn't keep track), dtostrf() is an AVR specific library (Atmel 328 etc.), and avr/dtostrf is a work-around for the M0, M4 chips.  And then we get to these mbed boards, and things stop working (until you create your own function).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mp2100
    mp2100 over 5 years ago in reply to ralphjy

    From what I read (at so many places I couldn't keep track), dtostrf() is an AVR specific library (Atmel 328 etc.), and avr/dtostrf is a work-around for the M0, M4 chips.  And then we get to these mbed boards, and things stop working (until you create your own function).