Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Using H450 (Toshiba TB67H450) Motor Driver Boards with Arduino
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 6 May 2023 11:33 PM Date Created
  • Views 11558 views
  • Likes 11 likes
  • Comments 25 comments
  • TB67H450
  • H450
  • A4950
  • TB67H450FNG
  • motor
  • motor and motion control
Related
Recommended

Using H450 (Toshiba TB67H450) Motor Driver Boards with Arduino

shabaz
shabaz
6 May 2023

Table of Contents

  • Introduction
  • Module Description
  • Motor Voltage (Power Source)
  • Motor Current Limit
  • Using the Module
  • Complete Circuit
  • Software
  • Summary


Introduction

Sean colporteur  was recently looking for motor driver modules to replace older modules that had a few problems. The older modules were getting damaged. Part of the problem is that a lot of hobby motor driver boards employ the L298 integrated circuit, which is many decades old and does not offer built-in protection like modern circuits. Under certain scenarios, the L298 boards cannot be used without additional circuitry and still may not be suitable if the software or the connected motor or supplies or wiring are subject to change. For more information on those scenarios, see the following blog post and comments: Raising the Bridge...Automation with Arduino: Failure reconciliation  

I had a look around, and the H450 module looked interesting; it is very low-cost and specified as suitable for 4.5-44V motors up to 2A. Each module can drive up to two normal DC motors (also known as permanent magnet DC motors or brushed DC motors) or one stepper motor. This blog post discusses how to use the modules to drive normal DC motors.

image

Note that the information here may also be compatible with A4950 boards too, but I don't know for sure. If you want to be entirely sure that the information here will help you, then carefully examine the photos further below in the blog post (in the Module Description section) and order an identical board (some may have subtle differences). The information here is also compatible with the DC Motor 6 Click Board  as javagoza discusses in the comments below.

This blog post shows an Arduino board being used with the module, but it will work fine with the Pi Pico too (and any board with 3.3V or 5V logic, provided pins can be configured for PWM output, if speed control is desired).

Module Description

The module contains two Toshiba TB67H450FNG motor driver ICs. Each IC contains a single H-bridge circuit and logic/driver circuitry for it.

image

The board contains two of the chips and the bare minimum needed to use them:

image

The board has an electrolytic capacitor on the underside. If you’re not using pin sockets to plug the board, then the capacitor will need to be bent outwards. It’s a weird board design : )

image

The screenshot below shows the particular board that I used, although others might be compatible, I have not tried any others:

image

Motor Voltage (Power Source)

The module accepts a single 4.5 to 44V supply, labeled VM. The H-bridge will switch that voltage to the motors.

Motor Current Limit

There is a VREF pin, labeled VCC on the boards. That voltage must be 5V or lower. It determines the maximum current that the motors require. If the current demand goes higher, then the chip will switch off the H-bridge, protecting the motors and the chip itself.

The formula is: Imax = (VREF/10)/R where R is 0.25. This can be simplified to: Imax = VREF * 0.4. So, if VREF is set to 5V, then the maximum current is 2A. That’s the maximum value (VREF must not be set higher than 5V). If your motors only require 1A max, then VREF would be set to 2.5V.

The great thing about the current limit is that it can protect both the motor and the circuit, so it is worthwhile taking some time to find the best value, and a variable resistor can help, as discussed further below.

Using the Module

The circuit diagram below shows the minimal connections needed to use the board.

image

Note that it is a good idea to improve the circuit a little bit. The diagram below shows a more ideal circuit. Use an 18V Zener diode if the motor power supply is up to 12V, and it will provide a bit of protection from transient voltages caused by wire inductances. The suggested 18V Zener diode is 1N5355 .

image

This improved circuit uses a trimmer resistor to set the current limit per motor to between 0 and 2A. If you don’t need that and just want the maximum current, then the trimmer resistor is not needed, and the 1k resistor R1 can be wired to a 5V supply.

My constructed circuit is shown below; the only extra addition is a 78L05 voltage regulator circuit so that the 5V supply for the current setting trimmer resistor is generated locally from the motor power supply. It saves having to connect the 5V supply from the Arduino. The output from the 78L05 just goes to the trimmer resistor and nowhere else.

image

It is also good to be nice to radio users by placing a capacitor or two directly across each motor. Otherwise, users of wireless remote control circuits may experience limited range, and you won’t get great music reception on radios either, while using the circuit.

The suggested capacitors are 100nF  and 10nF    

image

It is also good to add a ferrite core to the motor wiring. You could either use a single ferrite core or one in each wire connected to the motor. Loop the wire through the ferrite several times. The photo above shows quite large ferrite cores because that was all I had. You could use smaller ones if you don’t have space, but the larger ones are usually more effective.

A suggested ferrite core is Fair-Rite 2631540202  

A clip-on ferrite could be used too.

The DC to 50 MHz spectrum below shows that quite a noticeable improvement is made with the capacitors and ferrites.

image

Complete Circuit

The circuit diagram here shows a 78L05 voltage regulator  added (it saves having to wire 5V from the Arduino or whichever microcontroller board is being used). 

The circuit here has some 'Do Not Fit' components for flexibility. With R1 being a wire link, the current limit is set to 2A. R1 and R2 could be replaced with resistors if a different maximum current is needed.

image

The KiCad 7 project is on GitHub. Here is what the board looks like:

image

The 2-pin connectors for the motors and the power supply are screw terminals, and the holes are large enough to accept 3.5mm or 3.81mm pitch connectors for those. Alternatively, wires could be directly soldered.

The Gerber files are in a zip file called h450_motor_board_gerber_files.zip in that GitHub location.

Here is what the board may look like assembled:

image

I have not built this board, so there may be issues with it.

Software

Using the module with Arduino code is extremely easy. Firstly, make sure that the control pins (AIN1, AIN2, and [if you’re driving two motors] BIN1, BIN2) are connected to PWM-capable pins on whichever Arduino you are using, and make sure that the 0V (GND) connection is also made.

For my test, I connected just a single motor and used PWM pins 9 and 10.

The Arduino .ino file is available on GitHub. 

It is easy to follow along. Lines 5-59 contain the driver code, but you only need to examine just a handful of lines, lines 12-18 for the purposes of this blog post. Ordinarily, this code would be in a downloadable library, but since a lot of newcomers to C/C++ do not know how to create their own library, I thought it was worthwhile to keep this driver code in the main .ino file for now, so that they can see what goes inside a library. As can be seen, there’s not a lot of code!

Lines 12 to 18 describe the entire library; there are just three functions listed there! The first one is actually the “constructor” (this is C++ terminology) called Motor. It accepts two parameters, which are the pin numbers.

The only other two functions are called run and stop.

image

Here is how it would be used.

If a motor is connected to the PWM pins 9 and 10, then an instance of the Motor class is created by typing:

Motor mymotor(9,10);

To run the motor in a clockwise direction at a speed of 128 (the range is 0-255), type:

mymotor.run(DIR_CW, 128);

To run it in the other direction at top speed:

mymotor.run(DIR_CCW, 255);

To stop the motor:

mymotor.stop();

There’s a hard braking capability too, if that is desired:

mymotor.stop(HARD_BRAKE);

To use the motors with your own Arduino code, you could just copy-paste lines 5-59 into your .ino file and then make use of it, as shown in the example. Or you could just copy the entire example .ino file and edit it to suit your needs.

If you prefer an installable library (which is the correct way of doing things), that is an exercise for the reader. Hopefully, others can help with that if required (it is straightforward to do), but as mentioned, it is not essential, and it is a good learning exercise to be able to see the code for now.

Summary

The H450 modules are approximately just as cheap as L298 boards but the H450 ones are far better for motor control. This blog post describes how to make use of the boards, both in terms of hardware and software. I think they are very easy to use and are more likely to survive hardware and software issues.

If you have tried the H450 modules or any others, and have feedback, positive or negative, it would be great to hear.

Thanks for reading!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago in reply to colporteur +1
    Hi Sean, These DC-DC converter modules are very good, they will accept 7-28V and output 5V at 500mA, and they are quite low-cost. I've placed the KiCad symbol and footprint for that on GitHub here if…
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur

    "...I have to figure out all the stuff I need before the plaster goes up..."

    Given that it is a mining scene, can't you just chip into the plaster as required ? Slight smile

    Just watch out for the water pipes though... don't want to flood the mine. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to colporteur

    Hi Sean,

    Thanks! I figured since I'd already drawn the schematic, it was a quick thing to create the PCB.

    Sure, it will be great to hear about the mining cutaway project. I'd be happy to help (and I'm sure others would be too) wherever possible!

    Regarding KiCad 7, I had a look, and the software doesn't allow me to save in the older KiCad 6 format unfortunately, so it would require KiCad 7. However on the plus side, versions 6 and 7 are very similar, so you'll be right at home with version 7.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to shabaz

    image

    I will assume from this error message the files are KiCAD 7. I only started using the software in September of 22. I guess I will need to upgrade.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to shabaz

    WTF, in a positive way. I went through the scout achievement badges and have nominated you for the Scout Engineer badge.

    image

    There were a lot of positive with the Scout program until it got over shadowed by the undisclosed sexual abuse.

    Here I was going to sharpen my KiCAD skills and bang out a PCB. You keep this up my engineering friend and you will president of this community:)

    I could really use your skills on the model railroad layout. Looking at designing a mining operation. Cutaway view on the side of a wall. I have to figure out all the stuff I need before the plaster goes up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to colporteur

    Hi Sean,

    I've added the regulator circuit to the blog post, in the section titled "Complete Circuit". 

    I've uploaded the KiCad 7 schematic to GitHub, as well as the PCB and Gerber files, so if you like, you could either directly order the board using the zip Gerber files, or alternatively the board could be edited with KiCad. The board is slightly larger than it needs to be, but that's because I was trying to place the drill holes such that an Arduino could be stacked on top or underneath, since I'm hoping the holes will align if I've got that right! : )

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>