Arduino
  • Products & Partners
  • More
Arduino
Blog [Christmas Tree] Internet of Holiday Lights - Finished Build
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 21 Jan 2015 9:17 PM Date Created
  • Views 864 views
  • Likes 3 likes
  • Comments 2 comments
  • infineon
  • mqtt
  • yun
  • openhab
  • classic_modern_tree
  • iot_holidaylights
  • led
  • arduino
Related
Recommended

[Christmas Tree] Internet of Holiday Lights - Finished Build

fvan
fvan
21 Jan 2015

Previous posts in this project:

  • [Christmas Tree] Internet of Holiday Lights - Project Description
  • [Christmas Tree] Internet of Holiday Lights - Getting Started
  • [Christmas Tree] Internet of Holiday Lights - Control from openHAB
  • [Christmas Tree] Internet of Holiday Lights - Special Feature
  • [Christmas Tree] Internet of Holiday Lights - Song-based Lighting

 

  • Introduction
  • Building the Tree
  • Conclusion

 

Introduction

 

OK, this will be the final post for the Internet of Holiday Lights RoadTest Plus. It's been fun, frustrating, collaborative, etc ...

  • Fun, because I really enjoyed working with the Yun. I love Arduinos and the Yun's wireless programming and network connectivity just make it even better!
  • Frustrating, because I didn't get to where I wanted to be, due to unforeseen difficulties with the build.
  • Collaborative, because of the sharing and teaming up for special features.

 

Get ready for some picture overload! (the gallery function would've come in handy image)

 

Building the Tree

 

The biggest (and hardest as turned out) part of this project was the build. I wanted to make a Christmas tree with both classic and modern elements.

 

The idea was to hollow a log and stuff the electronics inside. Unfortunately, hollowing the log did not work as planned, and my tools were not suited for this kind of work. I ended up going for an alternative with a plastic cylinder for the base after having wasted too much time on the log.


imageimageimage

The tree itself was easier. Using threaded rods cuts in different lengths, I created a tree structure with branches. The expectation was to have a long LED strip go from branch to branch in a spiral shape. This lead to the next problem with the build: the strip was not rigid enough to keep the spiral shape and would just hang loosely. To solve that issue, I came up with the idea to use some fence wire to which the LED strip would be attached. That worked.

imageimageimage

Finally, all the wires needed to be guided to the base of the tree and hidden as wel as possible. Zip ties came in extremely handy!

The tree is ready! It's not late for Christmas 2014, it's just ready a bit early for Christmas 2015 image

imageimageimage

Now, where do I store this until Christmas ... ?

 

Conclusion

 

We are now the proud owners of a digital Christmas tree which can be controlled either manually using our smartphone or tablet or automatically depending on the Christmas song that is currently playing.

 

Oh ... I almost forgot. It also tells me when other fellow e14 members' project is online!

 

This was fun building, I hope you had fun reading!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +1
    Nice tree. I was wondering why the threaded rod until I saw the 3D printed connector.... In lieu of cable ties, fishing line works well, and is transparent. I use it for the illuminated signs, but it does…
  • fvan
    fvan over 11 years ago in reply to mcb1

    The threaded rods were what I had available to work with in the garage, and it made it easy to keep the connectors in place by screwing them on.

     

    Good idea on the fishing lines. Guess I'll have to find a spool and keep it handy. It indeed has the advantage of being very subtle and difficult to see. Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Nice tree.

    I was wondering why the threaded rod until I saw the 3D printed connector....image

     

    In lieu of cable ties, fishing line works well, and is transparent.

    I use it for the illuminated signs, but it does give your fingers a hard time..

     

    Mark