Arduino Forum Different result if connecting 9V?
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
  • Replies 15 replies
  • Subscribers 405 subscribers
  • Views 1569 views
  • Users 0 members are here
  • tmp 36
  • problem
  • power supply
  • arduino
  • sensor
Related

Different result if connecting 9V?

Former Member
Former Member over 9 years ago

I have done the project in Jeremy Blum "Explorign Arduino" related to the three color LED changing with the temperature. It works right when connected with USB, but it is always red if connected to 9V.

Did I do anything wrong? is it normal? how can I solve it?

The sensor is a TMP-36image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    To learn, you need to read the datasheet on the sensor and think what changes with the switch from USB to 9 volt battery. Clem
  • Former Member
    Former Member over 9 years ago +1
    Per John's comment, I'm assuming you're using a 9V barrel adapter. A couple of points: 1. You have to get enough power for the Arduino, the LED, the TMP36, etc. I never use carbon-zinc batteries or cells…
  • clem57
    clem57 over 9 years ago in reply to Former Member +1
    Sensors are very dependant on the voltage provided. Change the voltage, they need to be recalibrated. Try a separate independent power source on the rail to the sensor that is 5V. repeat the experiment…
Parents
  • Former Member
    Former Member over 9 years ago

    Per John's comment, I'm assuming you're using a 9V barrel adapter.

    A couple of points:

    1.     You have to get enough power for the Arduino, the LED, the TMP36, etc.  I never use carbon-zinc batteries or cells (usually labeled "Heavy-Duty").  I prefer Lithium batteries or cells as they can output high current, when needed; but alkaline batteries/cells should be OK.  Check the battery: not just the voltage, but how much current it can output.  Preferably use a new battery.

    2.     The type of problem you're seeing is almost always due to insufficient power.

    3.     Since it's working properly with USB power (original USB 2.0 specifies 5V at 500mA) that should tell you what you need to replicate for total max power.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago

    Per John's comment, I'm assuming you're using a 9V barrel adapter.

    A couple of points:

    1.     You have to get enough power for the Arduino, the LED, the TMP36, etc.  I never use carbon-zinc batteries or cells (usually labeled "Heavy-Duty").  I prefer Lithium batteries or cells as they can output high current, when needed; but alkaline batteries/cells should be OK.  Check the battery: not just the voltage, but how much current it can output.  Preferably use a new battery.

    2.     The type of problem you're seeing is almost always due to insufficient power.

    3.     Since it's working properly with USB power (original USB 2.0 specifies 5V at 500mA) that should tell you what you need to replicate for total max power.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 9 years ago in reply to Former Member

    Hi Brian,

    I have also found that even with batteries it is usually a good idea to have a decoupling capacitor across the power feed.

    John