Arduino Forum Different result if connecting 9V?
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
  • Replies 15 replies
  • Subscribers 405 subscribers
  • Views 1565 views
  • Users 0 members are here
  • tmp 36
  • problem
  • power supply
  • arduino
  • sensor
Related

Different result if connecting 9V?

Former Member
Former Member over 9 years ago

I have done the project in Jeremy Blum "Explorign Arduino" related to the three color LED changing with the temperature. It works right when connected with USB, but it is always red if connected to 9V.

Did I do anything wrong? is it normal? how can I solve it?

The sensor is a TMP-36image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    To learn, you need to read the datasheet on the sensor and think what changes with the switch from USB to 9 volt battery. Clem
  • Former Member
    Former Member over 9 years ago +1
    Per John's comment, I'm assuming you're using a 9V barrel adapter. A couple of points: 1. You have to get enough power for the Arduino, the LED, the TMP36, etc. I never use carbon-zinc batteries or cells…
  • clem57
    clem57 over 9 years ago in reply to Former Member +1
    Sensors are very dependant on the voltage provided. Change the voltage, they need to be recalibrated. Try a separate independent power source on the rail to the sensor that is 5V. repeat the experiment…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Jose,

    Your hookup looks good. As Brian has pointed out there is no reason why it will not work if the power source is solid and hooked to the DC input jack or to the Ground and Vin terminals of the Arduino header. I would also put a 0.1 uF cap across the 9 Volts near the Arduino. That book by Jeremy is excellent and I had a lot of fun working through it a while back.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    Thank you for the answer. I have checked with another board with a LCD and a DTH 11 sensor and the difference is 2 degrees centigrade between USB and 9v. What I can't understand is why. I thought the board provided 5v when connected to either 9V or USB.  I have checked the battery and it is providing 6.54v.

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    Thank you for the answer. I have checked with another board with a LCD and a DTH 11 sensor and the difference is 2 degrees centigrade between USB and 9v. What I can't understand is why. I thought the board provided 5v when connected to either 9V or USB.  I have checked the battery and it is providing 6.54v.

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 9 years ago in reply to Former Member

    Sensors are very dependant on the voltage provided. Change the voltage, they need to be recalibrated. Try a separate independent power source on the rail to the sensor that is 5V. repeat the experiment and report back the results.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to clem57

    I think you'll find that the 5v line is less than 5v while being powered from USB.

     

    Clem is correct that it will need recalibrating.

    I tend to always use a Dallas One Wire DS18B20 (or similar) to avoid this.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to Former Member

    Do you have a reasonably accurate DMM - if so try measuring some voltages around you circuit and you will be able to work out what is changing and affecting the result - it might then be simple to deal with the problem. If you post the circuit you have I can suggest places to measure.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to Former Member

    The answer may be simpler as far as sensing things

     

    The voltage reference by default in Arduino Uno / Mega and the like is set to be VCC

     

    USB rarely gives exactly 5V, more like 4.7 ish but can vary based on load and a number of other factors

     

    When you connect via the barrel jack with in your case 9V, then the on-board voltage regulator kicks in and is way better than 1% accurate typically and very close to the nominal 5V

     

    So in each case the VREF to the ADC will be different and therefor for the same input to the ADC pins, you will get a lower reading when running with the higher VREF voltage