Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4677 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer is "Yes", then buy ceramic resistors of the value required, but with at least a 2 watt rating.....they will still get warm though and may need some cooling if enclosed.

     

    The Arduino should be able to pulse the output pin and use a PWM method to control the brightness and to actually reduce the power needed to go through the LED.

     

    To learm more look here:- http://arduino.cc/it/Tutorial/PWM

     

    This may or not be appropiate for your application of course, only you know that.

     

    regards

     

    Andy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to e14 Contributor

    Do you mean that i could drive the ir led with  ..say..50mA , which would mean that the voltage drop is going to be about 3.6V, given the 180mW of the LED,wont that hurt the LED?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Depending on your needs, but you don't always have to power your LEDs with the max amount of current specified in the sheet - just don't go over.

     

    For example I have several projects that I use 2K 1/8 watt resistors on my power indicator LEDs simply because using the calculated resistor of 680 ohm 1/2 watt makes the LED way to bright. Plus I like to consume as little power as possible, allowing me to use smaller wattage resistors.

    Like a mentioned earlier, try a 100 ohm or even a 500 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Depending on your needs, but you don't always have to power your LEDs with the max amount of current specified in the sheet - just don't go over.

     

    For example I have several projects that I use 2K 1/8 watt resistors on my power indicator LEDs simply because using the calculated resistor of 680 ohm 1/2 watt makes the LED way to bright. Plus I like to consume as little power as possible, allowing me to use smaller wattage resistors.

    Like a mentioned earlier, try a 100 ohm or even a 500 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    well if I use a 120ohm resistor the current going trought the LED will be about 20mA , right?

    then .25mW resistors are perfect?